Functions#
This section provides a reference to the ECDH Crypto API functions.
Functions#
To compute the ECDH point addition vector.
To compute the ECDH point subtraction vector.
To compute the ECDH point multiplication vector.
To compute the ECDH point double vector.
To compute the ECDH point affinity vector.
Function Documentation#
sl_si91x_ecdh_point_addition#
sl_status_t sl_si91x_ecdh_point_addition (sl_si91x_ecdh_mode_t ecdh_mode, const uint8_t * sx, const uint8_t * sy, const uint8_t * sz, const uint8_t * tx, const uint8_t * ty, const uint8_t * tz, uint8_t * rx, uint8_t * ry, uint8_t * rz)
To compute the ECDH point addition vector.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_si91x_ecdh_mode_t | [in] | ecdh_mode | ECDH mode of type sl_si91x_ecdh_mode_t. |
| const uint8_t * | [in] | sx | Pointer to the x coordinate of the first point to be added. |
| const uint8_t * | [in] | sy | Pointer to the y coordinate of the first point to be added. |
| const uint8_t * | [in] | sz | Pointer to the z coordinate of the first point to be added. |
| const uint8_t * | [in] | tx | Pointer to the x coordinate of the second point to be added. |
| const uint8_t * | [in] | ty | Pointer to the y coordinate of the second point to be added. |
| const uint8_t * | [in] | tz | Pointer to the z coordinate of the second point to be added. |
| uint8_t * | [out] | rx | Pointer to the x coordinate of the result point. |
| uint8_t * | [out] | ry | Pointer to the y coordinate of the result point. |
| uint8_t * | [out] | rz | Pointer to the z coordinate of the result point. |
This is a blocking API. Returns
sl_status_t. For more information on status codes, refer to SL STATUS DOCUMENTATION.
sl_si91x_ecdh_point_subtraction#
sl_status_t sl_si91x_ecdh_point_subtraction (sl_si91x_ecdh_mode_t ecdh_mode, const uint8_t * sx, const uint8_t * sy, const uint8_t * sz, const uint8_t * tx, const uint8_t * ty, const uint8_t * tz, uint8_t * rx, uint8_t * ry, uint8_t * rz)
To compute the ECDH point subtraction vector.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_si91x_ecdh_mode_t | [in] | ecdh_mode | ECDH mode of type sl_si91x_ecdh_mode_t. |
| const uint8_t * | [in] | sx | Pointer to the x coordinate of the first point to be subtracted. |
| const uint8_t * | [in] | sy | Pointer to the y coordinate of the first point to be subtracted. |
| const uint8_t * | [in] | sz | Pointer to the z coordinate of the first point to be subtracted. |
| const uint8_t * | [in] | tx | Pointer to the x coordinate of the second point to be subtracted. |
| const uint8_t * | [in] | ty | Pointer to the y coordinate of the second point to be subtracted. |
| const uint8_t * | [in] | tz | Pointer to the z coordinate of the second point to be subtracted. |
| uint8_t * | [out] | rx | Pointer to the x coordinate of the result point. |
| uint8_t * | [out] | ry | Pointer to the y coordinate of the result point. |
| uint8_t * | [out] | rz | Pointer to the z coordinate of the result point. |
This is a blocking API. Returns
sl_status_t. For more information on status codes, refer to SL STATUS DOCUMENTATION.
sl_si91x_ecdh_point_multiplication#
sl_status_t sl_si91x_ecdh_point_multiplication (sl_si91x_ecdh_mode_t ecdh_mode, const uint8_t * d, const uint8_t * sx, const uint8_t * sy, const uint8_t * sz, uint32_t affinity, uint8_t * rx, uint8_t * ry, uint8_t * rz, uint8_t reverse)
To compute the ECDH point multiplication vector.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_si91x_ecdh_mode_t | [in] | ecdh_mode | ECDH mode of type sl_si91x_ecdh_mode_t. |
| const uint8_t * | [in] | d |
|
| const uint8_t * | [in] | sx |
|
| const uint8_t * | [in] | sy |
|
| const uint8_t * | [in] | sz |
|
| uint32_t | [in] | affinity | Affinity mode:
|
| uint8_t * | [out] | rx |
|
| uint8_t * | [out] | ry |
|
| uint8_t * | [out] | rz |
|
| uint8_t | [in] | reverse |
|
This is a blocking API. Returns
sl_status_t. For more information on status codes, refer to SL STATUS DOCUMENTATION.
sl_si91x_ecdh_point_double#
sl_status_t sl_si91x_ecdh_point_double (sl_si91x_ecdh_mode_t ecdh_mode, const uint8_t * sx, const uint8_t * sy, const uint8_t * sz, uint8_t * rx, uint8_t * ry, uint8_t * rz)
To compute the ECDH point double vector.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_si91x_ecdh_mode_t | [in] | ecdh_mode | ECDH mode of type sl_si91x_ecdh_mode_t. |
| const uint8_t * | [in] | sx | Pointer to the x coordinate of the point to be doubled. |
| const uint8_t * | [in] | sy | Pointer to the y coordinate of the point to be doubled. |
| const uint8_t * | [in] | sz | Pointer to the z coordinate of the point to be doubled. |
| uint8_t * | [out] | rx | Pointer to the x coordinate of the result point. |
| uint8_t * | [out] | ry | Pointer to the y coordinate of the result point. |
| uint8_t * | [out] | rz | Pointer to the z coordinate of the result point. |
This is a blocking API. Returns
sl_status_t. For more information on status codes, refer to SL STATUS DOCUMENTATION.
sl_si91x_ecdh_point_affine#
sl_status_t sl_si91x_ecdh_point_affine (sl_si91x_ecdh_mode_t ecdh_mode, const uint8_t * sx, const uint8_t * sy, const uint8_t * sz, uint8_t * rx, uint8_t * ry, uint8_t * rz)
To compute the ECDH point affinity vector.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_si91x_ecdh_mode_t | [in] | ecdh_mode | ECDH mode of type sl_si91x_ecdh_mode_t. |
| const uint8_t * | [in] | sx | Pointer to the x coordinate of the point. |
| const uint8_t * | [in] | sy | Pointer to the y coordinate of the point. |
| const uint8_t * | [in] | sz | Pointer to the z coordinate of the point. |
| uint8_t * | [out] | rx | Pointer to the x coordinate of the result point. |
| uint8_t * | [out] | ry | Pointer to the y coordinate of the result point. |
| uint8_t * | [out] | rz | Pointer to the z coordinate of the result point. |
This is a blocking API. Returns
sl_status_t. For more information on status codes, refer to SL STATUS DOCUMENTATION.