Constants#
This section provides a reference to the ECDSA Crypto API constants.
Enumerations#
Enumeration defining ECDSA private and public key sizes.
Enumeration defining ECDSA operations.
Enumeration defining ECDSA signature sizes supported by the SI91X device.
Enumeration defining ECC curve types supported by the SI91X device.
Enumeration defining the SHA modes supported by the ECDSA algorithm on the SI91X device.
Enumeration Documentation#
sl_si91x_ecdsa_key_size_t#
sl_si91x_ecdsa_key_size_t
Enumeration defining ECDSA private and public key sizes.
This enumeration defines the key sizes for private and public keys supported by the ECDSA algorithm on the SI91X device.
| Enumerator | |
|---|---|
| SL_SI91X_ECDSA_PRIV_KEY_SIZE_224 | Private key size of 224 bits. |
| SL_SI91X_ECDSA_PRIV_KEY_SIZE_256 | Private key size of 256 bits. |
| SL_SI91X_ECDSA_PUB_KEY_SIZE_224 | Public key size of 57 bytes. |
| SL_SI91X_ECDSA_PUB_KEY_SIZE_256 | Public key size of 65 bytes. |
sl_si91x_crypto_ecdsa_mode_t#
sl_si91x_crypto_ecdsa_mode_t
Enumeration defining ECDSA operations.
This enumeration defines the types of ECDSA operations supported, including generating ECC key pairs, generating signatures, and verifying signatures.
| Enumerator | |
|---|---|
| SL_SI91X_GENERATE_ECC_KEY_PAIR | Generate ECC private-public key pair. |
| SL_SI91X_ECDSA_GENERATE_SIGN | Generate signature. |
| SL_SI91X_ECDSA_VERIFY_SIGN | Verify signature. |
sl_si91x_ecdsa_signature_size_t#
sl_si91x_ecdsa_signature_size_t
Enumeration defining ECDSA signature sizes supported by the SI91X device.
This enumeration defines the signature sizes supported by the ECDSA algorithm on the SI91X device, including 224-bit and 256-bit sizes.
| Enumerator | |
|---|---|
| SL_SI91X_ECDSA_SIGN_HALF_SIZE_P224R1 | Signature size of 224 bits divided by 2. |
| SL_SI91X_ECDSA_SIGN_HALF_SIZE_P256R1 | Signature size of 256 bits divided by 2. |
| SL_SI91X_ECDSA_SIGN_MAX_SIZE | Maximum signature size supported. |
sl_si91x_crypto_ecc_curve_t#
sl_si91x_crypto_ecc_curve_t
Enumeration defining ECC curve types supported by the SI91X device.
This enumeration defines the ECC curves supported by the ECDSA algorithm on the SI91X device, which includes ECC_SECP224R1, and ECC_SECP256R1.
| Enumerator | |
|---|---|
| SL_SI91X_ECC_SECP224R1 | Values as provided by firmware. |
| SL_SI91X_ECC_SECP256R1 | |
sl_si91x_crypto_ecdsa_sha_mode_t#
sl_si91x_crypto_ecdsa_sha_mode_t
Enumeration defining the SHA modes supported by the ECDSA algorithm on the SI91X device.
This enumeration defines the SHA modes supported for the ECDSA algorithm on the SI91X device, which includes SHA256, SHA384, and SHA512.
| Enumerator | |
|---|---|
| SL_SI91X_ECDSA_SHA_256 | |
| SL_SI91X_ECDSA_SHA_384 | |
| SL_SI91X_ECDSA_SHA_512 | |