Functions#
This section provides a reference to the SHA Crypto API functions.
Functions#
sl_status_t
sl_si91x_sha(uint8_t sha_mode, const uint8_t *msg, uint16_t msg_length, uint8_t *digest)
To provide the SHA output for the given configuration.
Function Documentation#
sl_si91x_sha#
sl_status_t sl_si91x_sha (uint8_t sha_mode, const uint8_t * msg, uint16_t msg_length, uint8_t * digest)
To provide the SHA output for the given configuration.
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | sha_mode | 1 – For SHA1 2 – For SHA256 3 – For SHA384 4 – For SHA512 5 – For SHA224 |
| const uint8_t * | [in] | msg | Pointer to the message. |
| uint16_t | [in] | msg_length | Total message length. |
| uint8_t * | [out] | digest | Buffer to store the output. |
This is a blocking API. Returns
sl_status_t. For more information on status codes, see SL STATUS DOCUMENTATION.