Button
Introduction#
The SI91x button driver is a platform-level software module designed to manage button initialization and reading. It provides a wide range of functions for handling button operations, such as initialization, state monitoring, and callback management for state changes. The driver supports flexible interrupt configurations, allowing detection based on button state, edge transitions, or a combination of both. All button functions are accessed via the generic driver, which internally calls specific functions for the corresponding button.
Configuration#
All button instances are configured using the sl_button_t struct. This struct along with a function definition for initializing Button is automatically generated when an Button is set up using Simplicity Studio's wizard. This struct sl_button_t struct is automatically generated into the following files sl_si91x_button_instances.h and sl_si91x_button_instances.c. The samples below are for a single instance called "btn0".
// sl_si91x_button_instances.c
#include "sl_si91x_button_pin_config.h"
#include "sl_si91x_button_instances.h"
#include "sl_si91x_button_btn0_config.h"
sl_button_t const button_btn0 = {
.port = SL_BUTTON_BTN0_PORT,
.pin = SL_BUTTON_BTN0_PIN,
.button_number = SL_BUTTON_BTN0_NUMBER,
#ifdef SL_BUTTON_BTN0_PAD
.pad = SL_BUTTON_BTN0_PAD,
#endif
.interrupt_config = SL_BUTTON_CONFIG_BTN0_INTR
};
void button_init_instances(void)
{
sl_si91x_button_init(&button_btn0);
}
Note
The sl_si91x_button_instances.c file is shown with only one instance, but if more were in use they would all appear in this .c file.
// sl_si91x_button_instances.h
#ifndef SL_SI91X_BUTTON_INSTANCES_H
#define SL_SI91X_BUTTON_INSTANCES_H
#include "sl_si91x_button.h"
extern const sl_button_t button_btn0;
void button_init_instances(void);
void sl_simple_button_init_instances(void);
#endif // BUTTON_INSTANCES_H
Note
The sl_si91x_button_instances.h file is shown with only one instance, but if more were in use they would all appear in this .h file.
For more information on configuring available parameters, see the respective peripheral example readme document and Peripheral Configuration.
Usage#
After the button structures are defined, button functions can be called by passing an instance of sl_button_t, which will internally redirect to the type-specific version of the function. The commonly used functions include the following:
To initialize the button: sl_si91x_button_init
To return the current state (pressed or released) of the pin associated with a button: sl_si91x_button_state
To toggle the value of a local variable associated with the state of button: sl_si91x_button_toggle_state
A callback that user can modify for the application: sl_si91x_button_isr
The sl_si91x_button_init function is automatically invoked when the application starts.
The button driver supports interrupt mode, with or without debounce functionality.The application can implement sl_si91x_button_state to determine the current state of the button when needed. Additionally, sl_si91x_button_toggle_state can be implemented by the application to toggle the "soft" state, enabling interrupts and their callbacks. The sl_si91x_button_isr is a callback function triggered by a change in the button's state, and the application can implement this function to define the desired actions upon a state change.
Modules#
Macros#
A set of numerical macros for use with the button APIs.
To configure or to trigger the interrupt based on logic levels (LOW, HIGH, or both) or edge changes (rising, falling, or both).
Interrupt on level low/pressed button state can be configured.
Interrupt on level low/pressed and high/released button state can be configured.
Interrupt on level rising edge of the button press.
Interrupt on level falling edge of the button press.
Interrupt on level rising edge and falling edge of the button press.
Button state is pressed.
Button state is released.
Button state is invalid.
Functions#
To initialize the specified button with the given configuration.
Deinitialize the specified button and release associated resources.
To handle the interrupt when a button changes its state.
To get the current state (pressed or released) of a button.
To return the current state (pressed or released) of the pin associated with a button.
To toggle the value of a local variable associated with the state of a button.
To set the state (pressed or released) of the pin associated with a button.
Older API - Not recommended to use.
Older API - Not recommended to use.
Older API - Not recommended to use.
Older API - Not recommended to use.
Macros Documentation#
Function Documentation#
sl_si91x_button_init
void sl_si91x_button_init (const sl_button_t * handle)
To initialize the specified button with the given configuration.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const sl_button_t * | [in] | handle | Pointer to an sl_button_t button configuration structure containing the specific button details. |
This function configures the GPIO settings and interrupt configurations for the specified button. It handles different configurations based on the board version and button number. For UULP (Ultra-Low Power) and M4 (High-Performance) GPIOs, it sets the pin direction, pin mode, and interrupt settings.
The button configuration structure must be properly initialized before calling this function.
The specified button will be configured and ready for use with the specified settings.
Note
This function handles different configurations based on the board version and button number. For UULP (Ultra-Low Power) and M4 (High-Performance) GPIOs, it sets the pin direction, pin mode, and interrupt settings.
sl_si91x_button_deinit
sl_status_t sl_si91x_button_deinit (const sl_button_t * handle)
Deinitialize the specified button and release associated resources.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const sl_button_t * | [in] | handle | Pointer to an sl_button_t structure containing the button configuration details. |
This function deinitializes the specified button. After deinitialization, the button is no longer functional until reinitialized.
Returns
sl_status_t Status of the operation:
SL_STATUS_OK if the button was successfully deinitialized.
SL_STATUS_INVALID_HANDLE if the button number is invalid.
The button must have been previously initialized with sl_si91x_button_init.
Note
This function handles deinitialization for HP (High-Performance), ULP and UULP buttons.
sl_si91x_button_isr
void sl_si91x_button_isr (uint8_t pin, int8_t state)
To handle the interrupt when a button changes its state.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | pin | The button pin which has changed state, either BUTTON0 pin or BUTTON1 pin as defined. |
| int8_t | [in] | state | The new state of the button referenced by the button parameter, either BUTTON_PRESSED if the button has been pressed or BUTTON_RELEASED if the button has been released. |
This callback is called in the interrupt context whenever a button changes its state. It must be implemented by the application to handle the functionality in response to the button state change.
Note
This function should contain the functionality to be executed in response to changes of state in each of the buttons or callbacks to the appropriate functionality.
sl_si91x_button_get_state
uint8_t sl_si91x_button_get_state (uint8_t button_number)
To get the current state (pressed or released) of a button.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | button_number | The button number being queried. |
This function returns the shadow state of the button rather than reading the actual state of the pin. It is correlated with the interrupts and their callbacks, providing a "soft" state.
Returns
int8_t The state of the button:
BUTTON_PRESSED if the button is pressed.
BUTTON_RELEASED if the button is not pressed.
BUTTON_STATE_INVALID if the pin does not match any known button.
sl_si91x_button_state
uint8_t sl_si91x_button_state (uint8_t pin, uint8_t port)
To return the current state (pressed or released) of the pin associated with a button.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | pin | The button pin being queried |
| uint8_t | [in] | port | The button port being queried |
This function reads the actual state of the pin and can be used on startup to determine the initial position of the buttons.
Returns
int8_t The state of the button:
BUTTON_PRESSED if the button is pressed.
BUTTON_RELEASED if the button is not pressed.
sl_si91x_button_toggle_state
void sl_si91x_button_toggle_state (uint8_t button_number)
To toggle the value of a local variable associated with the state of a button.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | button_number | The button number being queried. |
This function toggles the state of a local variable that tracks the state of the specified button. It must be implemented by the application to handle the functionality in response to the button state change.
Note
This function should contain the functionality to be executed in response to changes of state in each of the buttons or callbacks to the appropriate functionality.
sl_si91x_button_set_state
void sl_si91x_button_set_state (uint8_t button_number, int8_t state)
To set the state (pressed or released) of the pin associated with a button.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | button_number | The button number being queried. |
| int8_t | [in] | state | The state of the button to be set:
|
This function sets the state of the specified button pin. It must be implemented by the application to handle the functionality in response to changes of state in each of the buttons or callbacks to the appropriate functionality.
Note
This function should contain the functionality to be executed in response to changes of state in each of the buttons or callbacks to the appropriate functionality.
sl_si91x_button_state_get
int8_t sl_si91x_button_state_get (uint8_t pin)
Older API - Not recommended to use.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | pin | The button pin being queried, either SL_BUTTON_BTN0_PIN or SL_BUTTON_BTN1_PIN as defined. |
This function returns the shadow state of the button rather than reading the actual state of the pin. It is correlated with the interrupts and their callbacks, providing a "soft" state.
Returns
int8_t The state of the button:
BUTTON_PRESSED if the button is pressed.
BUTTON_RELEASED if the button is not pressed.
BUTTON_STATE_INVALID if the pin does not match any known button.
Note
This function is deprecated and should be replaced with
sl_si91x_button_get_state.
sl_si91x_button_pin_state
int8_t sl_si91x_button_pin_state (uint8_t pin)
Older API - Not recommended to use.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | pin | The button pin being queried, either BUTTON0 pin or BUTTON1 pin as defined. |
This function reads the actual state of the pin and can be used on startup to determine the initial position of the buttons.
Returns
int8_t The state of the button:
BUTTON_PRESSED if the button is pressed.
BUTTON_RELEASED if the button is not pressed.
Note
This function is deprecated and should be replaced with
sl_si91x_button_state.
sl_si91x_button_state_toggle
void sl_si91x_button_state_toggle (uint8_t pin)
Older API - Not recommended to use.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | pin | The button pin which has changed state, either BUTTON0 pin or BUTTON1 pin as defined. |
This function toggles the state of a local variable that tracks the state of the specified button. It must be implemented by the application to handle the functionality in response to the button state change.
Note
This function should contain the functionality to be executed in response to changes of state in each of the buttons or callbacks to the appropriate functionality.
Note
This function is deprecated and should be replaced with
sl_si91x_button_toggle_state.
sl_si91x_button_state_set
void sl_si91x_button_state_set (uint8_t pin, int8_t state)
Older API - Not recommended to use.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | pin | The button pin which has changed state, either BUTTON0 pin or BUTTON1 pin as defined. |
| int8_t | [in] | state | The state of the button to be set:
|
This function sets the state of the specified button pin. It must be implemented by the application to handle the functionality in response to changes of state in each of the buttons or callbacks to the appropriate functionality.
Note
This function should contain the functionality to be executed in response to changes of state in each of the buttons or callbacks to the appropriate functionality.
Note
This function is deprecated and should be replaced with
sl_si91x_button_set_state.