Sensor Data Collector#

Introduction#

The Sensor Data Collector (SDC) is a low-power peripheral that internally uses ADC, enabling the conversion of analog signals (continuous voltage levels) into digital data (discrete binary values). This conversion allows microcontrollers to interface with analog sensors, such as temperature sensors, light sensors, or joysticks, effectively translating real-world analog signals into data that can be processed by digital systems.

SDC Block DiagramSDC Block Diagram

Features supported by the Watchdog Timer

  • Low power operation: SDC works in PS1 mode.

  • Multiple channels: SDC supports upto 4 channels.

  • Sampling Interval: The SDC can be configured to sample data at different intervals from 1 to 1024 units of seconds or milli seconds.

  • Sampling threshold: The SDC can be configured with a sampling threshold ranging from 1 to 16. device wakeups after reaching the threshold.

  • Single Ended and Differential Mode: SDC supports both single-ended and differential modes of operation.

Configuration#

Configuring the SDC involves several key steps to ensure accurate and efficient operation. These steps vary based on the specific hardware and application requirements. Below are some essential configuration tasks:

  • SDC Common Configurations: Define number of samples, sampling interval (1-1024), sampling threshold (1-16), clock division factor, and millisecond or second selection in the sl_si91x_sdc_config_t structure. After configuring this structure, call sl_si91x_sdc_driver_config() to set the SDC parameters.

  • Channel-Specific Settings: Define transfer count, buffer in the sl_si91x_sdc_channel_info_t structure, Auto buffer reset in sl_si91x_sdc_channel_misc_config_t, Input type and input pins in sl_si91x_sdc_adc_config_t. After configuring this structure, call sl_sdc_driver_channel_config() to set the channel parameters.

For more detailed configuration information, see the specific peripheral example README documents.

Usage#

After defining the ADC configuration structures, use the following functions to initialize and control the ADC module:

  1. Initialize SDC: sl_si91x_sdc_driver_init

  2. Set SDC Configuration: sl_si91x_sdc_driver_config

  3. Set Channel Configuration: sl_si91x_sdc_driver_channel_config

  4. Register Callback: sl_si91x_sdc_driver_register_callback

  5. Start Reading Data: sl_si91x_sdc_driver_read_data_start

  6. Stop Reading Data: sl_si91x_sdc_driver_stop

  7. Store Data: sl_si91x_sdc_driver_store_data

  8. Read Data: sl_si91x_sdc_driver_read_data

Modules#

sl_si91x_sdc_channel_info_t

sl_si91x_sdc_channel_misc_config_t

Enumerations#

enum
SDC_EVENT_SAMPLE_COMPLETE
SDC_EVENT_ERROR
SDC_EVENT_DATA_READY
SDC_EVENT_BUFFER_FULL
SDC_EVENT_BUFFER_RESET
}

Enumeration for SDC Events.

Typedefs#

typedef void(*
sl_sdc_callback_t)(uint8_t channel, sl_sdc_event_t event)

Callback function type for Sensor Data Controller (SDC) events.

Functions#

sl_status_t

Initialize the SDC driver.

sl_status_t

Deinitialize the SDC driver.

sl_status_t
sl_si91x_sdc_driver_config(sl_si91x_sdc_config_t *sl_sdc_config)

Configure the SDC driver with channel and pin configuration.

sl_status_t
sl_si91x_sdc_driver_channel_config(sl_si91x_sdc_adc_config_t *pin_config, sl_si91x_sdc_channel_info_t *sdc_channel_config, sl_si91x_sdc_channel_misc_config_t *misc_config)

Configures an SDC channel with the specified settings.

sl_status_t
sl_si91x_sdc_driver_register_callback(sl_sdc_callback_t callback_event)

Register a callback for SDC events.

sl_status_t

Unregister the SDC callback.

sl_status_t

Start reading data from SDC.

sl_status_t

Stop the SDC driver.

sl_status_t

Store the data from SDC FIFO registers.

sl_status_t
sl_si91x_sdc_driver_read_data(uint32_t channel, int16_t *buffer, uint8_t length)

Reads data from the SDC driver for the specified channel.

Macros#

#define

Mask for transfer complete.

#define

Position for transfer complete.

#define
SDC_CHANNEL1_TRANSFER_COMPLETE (0X1 << 0) << SDC_TRANSFER_COMPLETE_POS

Channel 1 transfer complete flag.

#define
SDC_CHANNEL2_TRANSFER_COMPLETE (0X1 << 1) << SDC_TRANSFER_COMPLETE_POS

Channel 2 transfer complete flag.

#define
SDC_CHANNEL3_TRANSFER_COMPLETE (0X1 << 2) << SDC_TRANSFER_COMPLETE_POS

Channel 3 transfer complete flag.

#define
SDC_CHANNEL4_TRANSFER_COMPLETE (0X1 << 3) << SDC_TRANSFER_COMPLETE_POS

Channel 4 transfer complete flag.

#define

Mask for buffer auto reset.

#define

Position for buffer auto reset.

#define
SDC_CHANNEL1_AUTO_BUFFER_RESET (0X1 << 0) << SDC_AUTO_BUFFER_RESET_POS

Channel 1 buffer auto reset enable flag.

#define
SDC_CHANNEL2_AUTO_BUFFER_RESET (0X1 << 1) << SDC_AUTO_BUFFER_RESET_POS

Channel 2 buffer auto reset enable flag.

#define
SDC_CHANNEL3_AUTO_BUFFER_RESET (0X1 << 2) << SDC_AUTO_BUFFER_RESET_POS

Channel 3 buffer auto reset enable flag.

#define
SDC_CHANNEL4_AUTO_BUFFER_RESET (0X1 << 3) << SDC_AUTO_BUFFER_RESET_POS

Channel 4 buffer auto reset enable flag.

#define

Mask for differential mode.

#define

Position for differential mode.

#define
SDC_CHANNEL1_DIFFERENTIAL_MODE (0X1 << 0) << SDC_DIFFERENTIAL_MODE_POS

Channel 1 differential mode flag.

#define
SDC_CHANNEL2_DIFFERENTIAL_MODE (0X1 << 1) << SDC_DIFFERENTIAL_MODE_POS

Channel 2 differential mode flag.

#define
SDC_CHANNEL3_DIFFERENTIAL_MODE (0X1 << 2) << SDC_DIFFERENTIAL_MODE_POS

Channel 3 differential mode flag.

#define
SDC_CHANNEL4_DIFFERENTIAL_MODE (0X1 << 3) << SDC_DIFFERENTIAL_MODE_POS

Channel 4 differential mode flag.

#define

Status code indicating that buffer has been reset after successfully reading the data.

#define

Status code indicating buffer is full.

#define

Single-ended Mode.

#define

Differential Mode.

#define

Maximum value of the SDC in single-ended mode.

#define

Minimum value of the SDC.

#define

Mid value of the SDC.

#define

Maximum FIFO threshold per channel when only using one channel.

#define

Maximum FIFO threshold per channel for SDC with two channels.

#define

Maximum FIFO threshold per channel for SDC with four channels.

Enumeration Documentation#

sl_sdc_event_t#

sl_sdc_event_t

Enumeration for SDC Events.

Enumerator
SDC_EVENT_SAMPLE_COMPLETE

Sample complete event.

SDC_EVENT_ERROR

Error event.

SDC_EVENT_DATA_READY

SDC data ready.

SDC_EVENT_BUFFER_FULL

Buffer is full.

SDC_EVENT_BUFFER_RESET

Buffer reset.


Typedef Documentation#

sl_sdc_callback_t#

typedef void(* sl_sdc_callback_t) (uint8_t channel, sl_sdc_event_t event) )(uint8_t channel, sl_sdc_event_t event)

Callback function type for Sensor Data Controller (SDC) events.

Parameters
TypeDirectionArgument NameDescription
[in]channel

The SDC channel on which the event occurred

[in]event

The type of event that occurred

This typedef defines a function pointer for SDC event callbacks. The callback function is invoked when SDC events occur.

Note

  • The application must register this callback to receive notifications about SDC events


Function Documentation#

sl_si91x_sdc_driver_init#

sl_status_t sl_si91x_sdc_driver_init (float vref)

Initialize the SDC driver.

Parameters
TypeDirectionArgument NameDescription
float[in]vref

Reference voltage for SDC.

  • This function initializes the SDC driver by performing the following steps:

    1. Initializes the RTC block.

    2. Starts the RTC.

    3. Initializes the SDC peripheral.

    4. Gets the chip voltage and update input voltage if required.

    5. Calibrates the ADC.

    6. Calculates the offset and gain values and stores them.

    7. Configures the SDC LDO voltage based on the reference voltage.

Returns

  • sl_status_t Status code indicating the result:

    • SL_STATUS_OK - Successfully initialized the SDC.

    • SL_STATUS_INVALID_PARAMETER - Parameters are invalid.

For more information on status codes, see SL STATUS DOCUMENTATION.


sl_si91x_sdc_driver_deinit#

sl_status_t sl_si91x_sdc_driver_deinit (void )

Deinitialize the SDC driver.

Parameters
TypeDirectionArgument NameDescription
voidN/A
  • This function performs the following steps:

    1. Stops the RTC to ensure no further operations are performed on it.

    2. Disables the SDC NVIC interrupt to prevent further interrupts.

    3. Deinitializes the SDC peripheral.

    4. Disables the SDC LDO to save power.

    5. Resets the global variable sdc_channel_info to zero.

    6. Resets the global variable sdc_calibration_data to zero.

Returns

  • sl_status_t Status code indicating the result:

    • SL_STATUS_OK - Successfully deinitialized the SDC.

For more information on status codes, see SL STATUS DOCUMENTATION.


sl_si91x_sdc_driver_config#

sl_status_t sl_si91x_sdc_driver_config (sl_si91x_sdc_config_t * sl_sdc_config)

Configure the SDC driver with channel and pin configuration.

Parameters
TypeDirectionArgument NameDescription
sl_si91x_sdc_config_t *[in]sl_sdc_config

Pointer to SDC configuration structure.

  • This function performs the following steps:

    1. Checks if the provided configuration pointer is NULL and returns an error if it is.

    2. Decrements the sample threshold and trigger event select values in the configuration to match the expected values in the SDC register.

    3. Configures the SDC with the provided configuration using the sl_si91x_sdc_config function.

    4. Returns the status of the configuration operation.

Returns

  • sl_status_t Status code indicating the result:

    • SL_STATUS_OK - Successfully configured the SDC.

    • SL_STATUS_INVALID_PARAMETER - Parameters are invalid.


sl_si91x_sdc_driver_channel_config#

sl_status_t sl_si91x_sdc_driver_channel_config (sl_si91x_sdc_adc_config_t * pin_config, sl_si91x_sdc_channel_info_t * sdc_channel_config, sl_si91x_sdc_channel_misc_config_t * misc_config)

Configures an SDC channel with the specified settings.

Parameters
TypeDirectionArgument NameDescription
sl_si91x_sdc_adc_config_t *[in]pin_config

Pointer to a structure containing the ADC pin configuration parameters.

sl_si91x_sdc_channel_info_t *[in]sdc_channel_config

Pointer to a structure containing the SDC channel configuration parameters.

sl_si91x_sdc_channel_misc_config_t *[in]misc_config

Pointer to a structure containing misc config of SDC channel

  • This function performs the following steps:

    1. Checks if the provided pin configuration and channel configuration pointers are NULL and returns an error if they are.

    2. Configures the SDC ADC pins using the sl_si91x_sdc_adc_pin_config function with the provided pin configuration and the number of channels.

    3. Iterates through each channel and initializes the channel information structure with the provided settings:

      • Sets the sample length for each channel.

      • Sets the receive buffer for each channel.

      • Sets the differential mode and auto buffer reset bits in the channel info bit field.

    4. Returns the status of the configuration operation.

Note

    1. pin_config structure is auto-generated when instance is created in the application user can directly use that structure.

Returns

    • SL_STATUS_OK on success.

    • SL_STATUS_FAIL on failure.


sl_si91x_sdc_driver_register_callback#

sl_status_t sl_si91x_sdc_driver_register_callback (sl_sdc_callback_t callback_event)

Register a callback for SDC events.

Parameters
TypeDirectionArgument NameDescription
sl_sdc_callback_t[in]callback_event

Callback function to register.

This API registers a user-provided callback function that is invoked when an SDC event occurs.

Returns

  • sl_status_t Status code indicating the result:

    • SL_STATUS_OK - Successfully registered the callback.

    • SL_STATUS_BUSY - Callback already registered.

    • SL_STATUS_NULL_POINTER - The parameter is a null pointer.

For more information on status codes, see SL STATUS DOCUMENTATION.


sl_si91x_sdc_driver_unregister_callback#

sl_status_t sl_si91x_sdc_driver_unregister_callback (void )

Unregister the SDC callback.

Parameters
TypeDirectionArgument NameDescription
voidN/A

This API unregisters the callback function registered for SDC events.

Returns

  • sl_status_t Status code indicating the result:

    • SL_STATUS_OK - Successfully unregistered the callback.

For more information on status codes, see SL STATUS DOCUMENTATION.


sl_si91x_sdc_driver_read_data_start#

sl_status_t sl_si91x_sdc_driver_read_data_start (void )

Start reading data from SDC.

Parameters
TypeDirectionArgument NameDescription
voidN/A

This API starts the SDC data acquisition process.

  1. It prepares the SDC to read data and provides a buffer to store the received data.

Returns

  • sl_status_t Status code indicating the result:

    • SL_STATUS_OK - Successfully started data read.

For more information on status codes, see SL STATUS DOCUMENTATION.


sl_si91x_sdc_driver_stop#

sl_status_t sl_si91x_sdc_driver_stop (void )

Stop the SDC driver.

Parameters
TypeDirectionArgument NameDescription
voidN/A

This API stops the SDC data acquisition process.

  1. It disables the SDC interrupt and stops the SDC sampling process.

Returns

  • sl_status_t Status code indicating the result:

    • SL_STATUS_OK - Successfully stopped the SDC.

For more information on status codes, see SL STATUS DOCUMENTATION.


sl_si91x_sdc_driver_store_data#

sl_status_t sl_si91x_sdc_driver_store_data (void )

Store the data from SDC FIFO registers.

Parameters
TypeDirectionArgument NameDescription
voidN/A

This API performs the following steps:

  1. Reads the data from the SDC FIFO.

  2. channel_id is decremented by 1 to match the zero-based index.

  3. Checks if the channel is in differential mode and processes the data accordingly.

  4. Stores the processed data in the channel's receive buffer.

  5. Increments the transfer count for the channel.

  6. Checks if the transfer count has reached the sample length for the channel. If it has, it calls the callback function with the SDC_EVENT_SAMPLE_COMPLETE event for that channel.

  7. If the channel is set to auto buffer reset, it resets the transfer count for the channel and clears the transfer complete bit in the channel info bit field.

Note

  • 1. This API should be called only after the SDC is started.

    1. If auto buffer reset is enabled, the write pointer wraps around to the start of the buffer when it reaches the end, allowing new data to overwrite the oldest data.

Returns

  • sl_status_t Status code indicating the result:

    • SL_STATUS_OK - Successfully reads the SDC data.

For more information on status codes, see SL STATUS DOCUMENTATION.


sl_si91x_sdc_driver_read_data#

sl_status_t sl_si91x_sdc_driver_read_data (uint32_t channel, int16_t * buffer, uint8_t length)

Reads data from the SDC driver for the specified channel.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]channel

The SDC channel number to read data from.

int16_t *[out]buffer

Pointer to the buffer where the read data will be stored.

uint8_t[in]length

The number of samples to read from the SDC channel.

This function reads data of specified length from the given SDC channel and stores it in the provided buffer.

Returns

    • SL_STATUS_OK if the data was read successfully.

    • SL_INVALID_PARAMETER if the provided parameters are invalid (e.g., channel number out of range, buffer is NULL, or length > threshold). For more information on status codes, see SL STATUS DOCUMENTATION.


Macro Definition Documentation#

SDC_TRANFER_COMPLETE_MASK#

#define SDC_TRANFER_COMPLETE_MASK
Value:
0xF

Mask for transfer complete.


SDC_TRANSFER_COMPLETE_POS#

#define SDC_TRANSFER_COMPLETE_POS
Value:
0

Position for transfer complete.


SDC_CHANNEL1_TRANSFER_COMPLETE#

#define SDC_CHANNEL1_TRANSFER_COMPLETE
Value:
(0X1 << 0) << SDC_TRANSFER_COMPLETE_POS

Channel 1 transfer complete flag.


SDC_CHANNEL2_TRANSFER_COMPLETE#

#define SDC_CHANNEL2_TRANSFER_COMPLETE
Value:
(0X1 << 1) << SDC_TRANSFER_COMPLETE_POS

Channel 2 transfer complete flag.


SDC_CHANNEL3_TRANSFER_COMPLETE#

#define SDC_CHANNEL3_TRANSFER_COMPLETE
Value:
(0X1 << 2) << SDC_TRANSFER_COMPLETE_POS

Channel 3 transfer complete flag.


SDC_CHANNEL4_TRANSFER_COMPLETE#

#define SDC_CHANNEL4_TRANSFER_COMPLETE
Value:
(0X1 << 3) << SDC_TRANSFER_COMPLETE_POS

Channel 4 transfer complete flag.


SDC_AUTO_BUFFER_RESET_MASK#

#define SDC_AUTO_BUFFER_RESET_MASK
Value:
0xF00

Mask for buffer auto reset.


SDC_AUTO_BUFFER_RESET_POS#

#define SDC_AUTO_BUFFER_RESET_POS
Value:
8

Position for buffer auto reset.


SDC_CHANNEL1_AUTO_BUFFER_RESET#

#define SDC_CHANNEL1_AUTO_BUFFER_RESET
Value:
  (0X1 << 0) << SDC_AUTO_BUFFER_RESET_POS

Channel 1 buffer auto reset enable flag.


SDC_CHANNEL2_AUTO_BUFFER_RESET#

#define SDC_CHANNEL2_AUTO_BUFFER_RESET
Value:
  (0X1 << 1) << SDC_AUTO_BUFFER_RESET_POS

Channel 2 buffer auto reset enable flag.


SDC_CHANNEL3_AUTO_BUFFER_RESET#

#define SDC_CHANNEL3_AUTO_BUFFER_RESET
Value:
  (0X1 << 2) << SDC_AUTO_BUFFER_RESET_POS

Channel 3 buffer auto reset enable flag.


SDC_CHANNEL4_AUTO_BUFFER_RESET#

#define SDC_CHANNEL4_AUTO_BUFFER_RESET
Value:
  (0X1 << 3) << SDC_AUTO_BUFFER_RESET_POS

Channel 4 buffer auto reset enable flag.


SDC_DIFFERENTIAL_MODE_MASK#

#define SDC_DIFFERENTIAL_MODE_MASK
Value:
0xF0000

Mask for differential mode.


SDC_DIFFERENTIAL_MODE_POS#

#define SDC_DIFFERENTIAL_MODE_POS
Value:
16

Position for differential mode.


SDC_CHANNEL1_DIFFERENTIAL_MODE#

#define SDC_CHANNEL1_DIFFERENTIAL_MODE
Value:
(0X1 << 0) << SDC_DIFFERENTIAL_MODE_POS

Channel 1 differential mode flag.


SDC_CHANNEL2_DIFFERENTIAL_MODE#

#define SDC_CHANNEL2_DIFFERENTIAL_MODE
Value:
(0X1 << 1) << SDC_DIFFERENTIAL_MODE_POS

Channel 2 differential mode flag.


SDC_CHANNEL3_DIFFERENTIAL_MODE#

#define SDC_CHANNEL3_DIFFERENTIAL_MODE
Value:
(0X1 << 2) << SDC_DIFFERENTIAL_MODE_POS

Channel 3 differential mode flag.


SDC_CHANNEL4_DIFFERENTIAL_MODE#

#define SDC_CHANNEL4_DIFFERENTIAL_MODE
Value:
(0X1 << 3) << SDC_DIFFERENTIAL_MODE_POS

Channel 4 differential mode flag.


SL_SDC_BUFFER_RESET#

#define SL_SDC_BUFFER_RESET
Value:
  0x75

Status code indicating that buffer has been reset after successfully reading the data.


SL_SDC_BUFFER_FULL#

#define SL_SDC_BUFFER_FULL
Value:
0x76

Status code indicating buffer is full.


SL_SDC_SINGLE_ENDED_MODE#

#define SL_SDC_SINGLE_ENDED_MODE
Value:
0

Single-ended Mode.


SL_SDC_DIFFERENTIAL_MODE#

#define SL_SDC_DIFFERENTIAL_MODE
Value:
1

Differential Mode.


SDC_MAX_VALUE#

#define SDC_MAX_VALUE
Value:
4095

Maximum value of the SDC in single-ended mode.


SDC_MIN_VALUE#

#define SDC_MIN_VALUE
Value:
0

Minimum value of the SDC.


SDC_MID_VALUE#

#define SDC_MID_VALUE
Value:
2048

Mid value of the SDC.


SDC_ONE_CH_MAX_FIFO_TH#

#define SDC_ONE_CH_MAX_FIFO_TH
Value:
16

Maximum FIFO threshold per channel when only using one channel.


SDC_TWO_CH_MAX_FIFO_TH#

#define SDC_TWO_CH_MAX_FIFO_TH
Value:
8

Maximum FIFO threshold per channel for SDC with two channels.


SDC_FOUR_CH_MAX_FIFO_TH#

#define SDC_FOUR_CH_MAX_FIFO_TH
Value:
4

Maximum FIFO threshold per channel for SDC with four channels.