Socket Configuration#
This section provides a reference for the socket configuration API functions.
These functions enable various socket-related configurations, including ciphers used for secure communication.
Modules#
sl_si91x_socket_type_length_value_t
SiWx91x Socket Extended Ciphers
Functions#
Configures SiWx91x specific socket settings.
Sets the list of ciphers to be used when creating sockets.
Sets the list of extended ciphers to be used when creating sockets.
Function Documentation#
sl_si91x_config_socket#
sl_status_t sl_si91x_config_socket (sl_si91x_socket_config_t socket_config)
Configures SiWx91x specific socket settings.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_si91x_socket_config_t | [in] | socket_config | Socket configuration of type sl_si91x_socket_config_t. |
This function sets up the socket configuration specific to the SiWx91x. It must be called before invoking sl_si91x_socket_async. The configuration includes setting parameters such as socket type, protocol, and other options specific to the SiWx91x series.
Pre-conditions:
Ensure that the necessary initialization for the SiWx91x module has been completed.
This API is called before calling sl_si91x_socket_async.
Returns
sl_status_t. See https://docs.silabs.com/gecko-platform/latest/platform-common/status for details.
sl_si91x_set_socket_cipherlist#
void sl_si91x_set_socket_cipherlist (uint32_t cipher_list)
Sets the list of ciphers to be used when creating sockets.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | cipher_list | A bitmap of the selected ciphers from SiWx91x Socket Ciphers. |
This function allows you to specify the ciphers that should be used when creating sockets for secure communication.
sl_si91x_set_extended_socket_cipherlist#
void sl_si91x_set_extended_socket_cipherlist (uint32_t extended_cipher_list)
Sets the list of extended ciphers to be used when creating sockets.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | extended_cipher_list | A bitmap of the selected extended ciphers from SiWx91x Socket Extended Ciphers. |
This function allows you to specify the extended ciphers that should be used when creating sockets for secure communication.