Types#
This section provides a reference to Wi-Fi API data types.
Modules#
sl_wifi_buffer_configuration_t
sl_wifi_extended_scan_result_t
sl_wifi_extended_scan_result_parameters_t
sl_wifi_advanced_scan_configuration_t
sl_wifi_advanced_ap_configuration_t
sl_wifi_client_configuration_t
sl_wifi_advanced_client_configuration_t
sl_wifi_reschedule_twt_config_t
sl_wifi_operational_statistics_t
sl_wifi_client_info_response_t
sl_wifi_async_stats_response_t
sl_wifi_transmitter_test_info_t
sl_wifi_multicast_filter_info_t
sl_wifi_transceiver_tx_data_control_t
sl_wifi_transceiver_cw_config_t
sl_wifi_transceiver_parameters_t
sl_wifi_transceiver_set_channel_t
sl_wifi_transceiver_peer_update_t
sl_wifi_transceiver_mcast_filter_t
sl_wifi_transceiver_configuration_t
sl_wifi_transceiver_tx_data_confirmation_t
sl_wifi_module_state_stats_response_t
sl_wifi_system_fw_version_info_t
sl_wifi_request_tx_test_info_t
sl_wifi_advanced_stats_response_t
Enumerations#
Enumeration for types of Wi-Fi buffers.
Wireless co-existence mode.
Enumeration of Wi-Fi operation modes for the Si91x wireless device.
Performance profile.
Typedefs#
Generic callback for handling Wi-Fi events.
Wi-Fi credential handle.
Wi-Fi Access Point dynamic configuration structure.
Enumeration Documentation#
sl_wifi_buffer_type_t#
sl_wifi_buffer_type_t
Enumeration for types of Wi-Fi buffers.
| Enumerator | |
|---|---|
| SL_WIFI_TX_FRAME_BUFFER | Buffer for sending socket data to NWP. |
| SL_WIFI_RX_FRAME_BUFFER | Buffer for storing response from NWP. |
| SL_WIFI_CONTROL_BUFFER | Buffer for sending command to NWP. |
| SL_WIFI_SCAN_RESULT_BUFFER | Buffer for storing scan results. |
sl_wifi_system_coex_mode_t#
sl_wifi_system_coex_mode_t
Wireless co-existence mode.
Note
Only BLE, WLAN, and WLAN + BLE modes are supported.
| Enumerator | |
|---|---|
| SL_WIFI_SYSTEM_WLAN_ONLY_MODE | Wireless local area network (WLAN) only mode. |
| SL_WIFI_SYSTEM_WLAN_MODE | WLAN mode (not currently supported) |
| SL_WIFI_SYSTEM_BLUETOOTH_MODE | Bluetooth only mode (not currently supported) |
| SL_WIFI_SYSTEM_WLAN_BLUETOOTH_MODE | WLAN and Bluetooth mode (not currently supported) |
| SL_WIFI_SYSTEM_DUAL_MODE | Dual mode (not currently supported) |
| SL_WIFI_SYSTEM_WLAN_DUAL_MODE | WLAN dual mode (not currently supported) |
| SL_WIFI_SYSTEM_BLE_MODE | Bluetooth Low Energy (BLE) only mode, used when power save mode is not needed. |
| SL_WIFI_SYSTEM_WLAN_BLE_MODE | WLAN and BLE mode. |
| __SL_WIFI_FORCE_COEX_ENUM_16BIT | Force the enumeration to be 16-bit. |
sl_wifi_operation_mode_t#
sl_wifi_operation_mode_t
Enumeration of Wi-Fi operation modes for the Si91x wireless device.
This enumeration defines the various operation modes supported by the wireless device. Each mode configures the device for a specific use case, such as client mode, access point mode, or transceiver mode.
| Enumerator | |
|---|---|
| SL_WIFI_CLIENT_MODE | Wi-Fi personal client mode. |
| SL_WIFI_ENTERPRISE_CLIENT_MODE | Wi-Fi enterprise client mode. |
| SL_WIFI_ACCESS_POINT_MODE | Wi-Fi access point mode. |
| SL_WIFI_TRANSCEIVER_MODE | Wi-Fi transceiver mode. |
| SL_WIFI_TRANSMIT_TEST_MODE | Wi-Fi transmit test mode. |
| SL_WIFI_CONCURRENT_MODE | Wi-Fi concurrent mode. |
| __SL_WIFI_FORCE_OPERATION_ENUM_16BIT | Force the enumeration to be 16-bit. |
sl_wifi_system_performance_profile_t#
sl_wifi_system_performance_profile_t
Performance profile.
| Enumerator | |
|---|---|
| SL_WIFI_SYSTEM_HIGH_PERFORMANCE | Power save is disabled and throughput is maximum. |
| SL_WIFI_SYSTEM_ASSOCIATED_POWER_SAVE | Low power profile when the device is associated with an AP (MAX PSP). |
| SL_WIFI_SYSTEM_ASSOCIATED_POWER_SAVE_LOW_LATENCY | Low power profile when the device is associated with an AP (FAST PSP). |
| SL_WIFI_SYSTEM_DEEP_SLEEP_WITHOUT_RAM_RETENTION | Deep Sleep without RAM Retention when the device is not associated with AP. |
| SL_WIFI_SYSTEM_DEEP_SLEEP_WITH_RAM_RETENTION | Deep Sleep with RAM Retention when the device is not associated with AP. |
Typedef Documentation#
sl_wifi_event_handler_t#
sl_wifi_event_handler_t )(sl_wifi_event_t event, sl_wifi_buffer_t *buffer)
Generic callback for handling Wi-Fi events.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| N/A | event | Wi-Fi event of type sl_wifi_event_t. | |
| N/A | buffer | Pointer to a Wi-Fi buffer contains information related to the event, of type sl_wifi_buffer_t |
Returns
sl_status_t. See Status Codes and WiSeConnect Status Codes for details.
Note
In case of event failure, SL_WIFI_FAIL_EVENT_STATUS_INDICATION bit is set in the event. The data would be of type sl_status_t, and data_length can be ignored.
sl_si91x_ap_reconfiguration_t#
typedef sl_wifi_ap_reconfiguration_t sl_si91x_ap_reconfiguration_t
Wi-Fi Access Point dynamic configuration structure.