Documentation Revision History#
Revision 3.5.2 released Septemeber, 2025#
SoC only#
Updated applications prints for Wi-Fi M4 firmware update.
NCP only#
None
SoC and NCP#
Updated readme of Wi-Fi - Azure IoT MQTT client application.
Marked internal Wi-Fi transceiver mode configurations as unsupported for the current release.
Updated the readme for WLAN TCP TX on periodic wakeup example.
Updated readme of Wi-Fi - Embedded MQTT client example correcting the units of Keepalive timer as seconds.
Updated readme of Crypto - AES example.
Removed incorrect HTTPS server references from documentation.
Added documentation for the TLS_EXTENSION_ENABLE macro in the TLS client example.
Added recommendation settings as a note in example applications.
Update Flash Read Write readme to include note on flash memory erasure before write operations.
Added readme for NAT application, Wi-Fi - Dual Network Stack NWP + M4.
Updated application prints for Wi-Fi Firmware update example.
Updated the error code for SL_STATUS_SI91X_HOST_VOLTAGE_OUT_OF_RANGE.
Updated the readme of Wi-Fi Coex - Wi-Fi Client BLE Provisioning with AWS (Devkit) example.
Updated
sl_wifi_update_su_gain_tableAPI documentation to improve clarity.Updated
sl_si91x_rsp_wireless_info_tstructure documentation to improve clarity.Updated
SL_WIFI_FEAT_DISABLE_SHORT_GIdocumentation with a note on it's impact on 802.11n and 802.11ax data rates.
Revision 3.5.0 released June, 2025#
SoC only#
Updated README documentation with output images in Wi-Fi - NWP Or Combined (NWP & M4) Firmware Update via TCP example.
Updated the Wi-Fi – AWS IoT MQTT Client example README to include the latest application print images.
NCP only#
Updated the API description for
sl_http_server_init()and updated the README for the multithreading application.
SoC and NCP#
Updated the README documentation with the path to scripts to be used in Wi-Fi - HTTP Client and Wi-Fi - HTTP Server examples.
Updated the README documentation for the Wi-Fi - Concurrent HTTP Server Provisioning as per new flow.
Updated the README documentation with the steps to update the user gain table for the Wireless Test example.
Updated the
sl_wifi_stats_callback_tdocumentation to include a note directing users to the reference section for Access Point (AP) deauthentication reason codes.Updated documentation for
sl_wifi_bss_type_tto specify supported and unsupported BSS types.Updated documentation for NWP UART baud rate and steps to capture RAM dump details.
Revised the documentation to specify that
sl_wifi_send_raw_data_frame()usage is supported only after the module is in connected state.Updated README documentation with alarm-based wakeup information in Wi-Fi - AWS IoT MQTT Client example.
Updated documentation in the note section
sl_net_deinit()to explain that this function should not be called after an M4 OTA firmware upgrade.Updated type variable documentation in
sl_si91x_socket_type_length_value_tstructure.Updated README with images aligned to the mobile application interface.
Updated interface usage recommendation note in the
sl_net_deinit()API documentation.Updated
option_nameandoption_valuedocumentation for the TLS feature insl_si91x_setsockopt()API.Updated connection timeout recommendations in
sl_wifi_connect()for different security modes.Updated usage notes to clarify correct sequencing of sl_wifi_* and sl_net_* API functions, helping prevent undefined behavior during Wi-Fi/Network interface.
Updated the error code for SL_STATUS_SI91X_HOST_VOLTAGE_OUT_OF_RANGE.
Updated the
sl_si91x_gcmAPI documentation to specify the maximum supported message length.Added a note for configuring crystal good time using the
sl_si91x_set_nwp_config_requestAPI.