WiSeConnect - Multiprotocol Version 4.0.0 (Jan 22, 2026) - Release Notes#

Wi-Fi 6 + BLE (WiSeConnect) SDK Version 4.0.0

Simplicity SDK Version 2025.12.0

The Multiprotocol Software Development Kit (SDK) provides Wi-Fi and BLE coexistence and packet traffic arbitration (PTA) features.

Click here for earlier releases.

Release Summary#

Key Features | API Changes | Bug Fixes | Chip Enablement

Key Features#

None

API Changes#

None

Bug Fixes#

  • Fixed multiple issues where the SiWx917 encountered socket/SSL failures, hangs, MQTT data stoppage, BLE disconnections, and instability during Wi-Fi reconnect loops, MQTT cycling, BLE scanning/advertising, and heavy stress with up to 10 BLE connections.

  • Resolved long-duration test failures including errors 0x4E08 and -13; Pixel DLE interoperability issues; connection-parameter update hangs; and instances where the device became unresponsive under continuous Wi-Fi, MQTT, and GATT notification load.

  • Fixed an issue where the ble_get_local_address API became unresponsive when invoked after a specific sequence involving Wi-Fi initialization, scan, and connection; followed by BLE advertising and scanning start/stop operations; and a subsequent Wi-Fi disconnect.

Chip Enablement#

None

Key Features#

New Features | Enhancements | Removed Features | Deprecated Features

Note: See Feature Matrix for a list of any applicable APIs, examples, software variants, modes, hardware, and host interfaces applicable for each feature.

New Features#

None

Enhancements#

None

Removed Features#

None

Deprecated Features#

None

API Changes#

New APIs | Modified APIs | Removed APIs | Deprecated APIs

New APIs#

None

Modified APIs#

None

Removed APIs#

None

Deprecated APIs#

None

Bug Fixes#

Note: See the Feature Matrix section for a list of all hardware parts that work with the WiSeConnect SDK.

ID Issue Description GitHub / Salesforce Reference (if any) Affected Software Variants, Hardware, Modes, Host Interfaces
1521233 Fixed an issue where the DUT became non-connectable after the second remote central auto-disconnect (~40 min) when operating with 8 BLE peripheral connections and 2 BLE central connections performing active data transmission/reception, along with continuous MQTT connect/disconnect operations running in a loop. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1511407 Fixed a command disallowed (0x4E0C) error occurring when stopping BLE advertising in the SoftAP+BLE provisioning application after remote client disconnect and reconnect. Also resolved web interface unresponsiveness that occurred during subsequent connection attempts. None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1505752 Fixed an issue where socket connections failed during SSL transmission when BLE scanning and advertising were active concurrently in power-save mode with encrypted firmware. None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1453288 Resolved connectivity instability under high-stress conditions involving Wi-Fi MQTT cycling and simultaneous GATT notifications from 10 BLE connections when using encrypted firmware. None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1276739 Fixed device hangs when continuous WLAN connect/disconnect and HTTPS GET/deinit operations occur alongside a BLE LE Secure connection. None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1521722 Fixed an issue where MQTT data transfer stopped after approximately 30 minutes, followed by BLE disconnections after about 1 hour and 30 minutes. None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1515995 Fixed hang issue during MQTT data transfer with 10 concurrent BLE bidirectional data transfers (TX/RX with notifications) when one peripheral connection was a Pixel device with DLE enabled. None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1505989 Fixed a connection timeout error (0x4E08) observed on the remote central device during long-duration testing involving MQTT data transfer and 10 concurrent BLE connections performing bidirectional data transfers None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1397267 Fixed an issue where MQTT connections occasionally failed with error code -13 when provisioning via a OnePlus 7T mobile device. None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1471402 Fixed an issue where the ble_get_local_address API became unresponsive when invoked after a specific sequence of Wi-Fi and BLE operations, including: Wi-Fi and BLE initialization, an initial ble_get_local_address call, Wi-Fi scan and connection, BLE advertising start/stop, BLE scanning start/stop, Wi-Fi disconnect, ble_get_state, and a subsequent ble_get_local_address call. None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1443334 Fixed an issue where the SiWx917 could become unresponsive and experience disconnections from both Wi-Fi and BLE under heavy-load conditions involving continuous Wi-Fi activity, MQTT traffic, and GATT notifications from 10 BLE connections. None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART

Chip Enablement#

None

Application Example Changes#

New Examples | Modified Examples | Removed Examples | Deprecated Examples

Note: See the Feature Matrix section for a list of all hardware parts that work with the WiSeConnect SDK.

New Examples#

None

Modified Examples#

Example Name Changes Supported Software Variants if applicable Supported Modes Supported OPNs / Boards / OPN Combinations Supported Host Interfaces

Wi-Fi Client BLE Throughput App

Added continuous throughput support for TCP RX and UDP RX traffic in the Wi-Fi Station BLE Throughput application.

See README

Standard and Lite
  • SoC
  • NCP
  • OPNs: All
  • Boards: All
SPI, UART

Removed Examples#

None

Deprecated Examples#

None

Known Issues and Limitations#

ID Issue or Limitation Description GitHub / Salesforce Reference (if any) Workaround (if any) Affected Software Variants, Hardware, Modes, Host Interfaces
1455876 MQTT publish failure (error code -7) occurs for QoS 0 messages after 30 minutes when running 10 concurrent BLE connections and GATT notifications without SMP on an encrypted connectivity (network processor) firmware image. None None
  • Software variants: Standard and Lite
  • OPNs: All except IC OPNs
  • Boards: All applicable boards
  • Modes: SoC, NCP
  • Host interfaces SPI, UART
1451820 SiWx917 fails to re-connect after a few MQTT disconnections during a BLE scan start and stop loop with the wlan_ble_unified_coex_app_soc example application. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1479757 A bus thread looping issue was observed while running a multi-socket application. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1444697 BLE disconnections occur when loading or clearing the TLS certificate. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1512574 When the DUT is configured to advertise with BLE SMP enabled and a continuous WLAN scan is active, the remote BLE central device may frequently fail to pair and occasionally fail to connect. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
N/A In co-existence mode, configuring 480 KB of RAM for the network processor and 192 KB for the application processor can reduce Wi-Fi throughput by approximately 10 Mbps due to limited memory available for data packets. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
N/A Multiprotocol operation (Wi-Fi station + BLE) with EAP security modes is supported only for memory configurations EXT_FEAT_416K_M4SS_256K (416 KB network processor + 256 KB application processor) and EXT_FEAT_480K_M4SS_192K (480 KB network processor + 192 KB application processor). None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
N/A System-level changes introduced to enhance stability have resulted in some increase in power numbers (up to 15% for smaller connection intervals of 200 ms) for BLE-connected only cases for modules. Impact is smaller for longer connection intervals. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1557787 The Wi-Fi station returns error 0x1FF9C (SL_STATUS_SI91X_DHCP_HANDSHAKE_FAILURE) in congested environments when operating in concurrent mode with both NAT and PAT features enabled. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1574418 Using slc generate --toolchain gcc or slc generate --with toolchain_gcc may fail with exclusivity errors due to the wiseconnect_toolchain_gcc_standard component incorrectly providing toolchain_gcc, resulting in a conflict with the Simplicity SDK toolchain_gcc component. If using those two command line options results in exclusivity errors, then you can remove them. Note that in a future WiseConnect release, you might have to reintroduce the toolchain option on the command line. Refer to future WiseConnect release notes for updates on possible behavior changes. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART