RPS Format#

The RPS file format is used for delivering update images which are optionally signed and encrypted. An RPS file may contain a TA application image, M4 application image, or both. The format is specified in the table below:

46 bytes 64 bytes … 71 or 72 bytes

RPS header

Boot descriptors

Application binary (size varies)

Digital signature (optional)¹

Note: Signature is stored in ASN.1 format, not plain binary. The size of ASN.1 can vary depending on the content.

The RPS header is defined in the follow table.

Field Size (bits) Description
Control Flags 16 BIT(0): 0 - NWPSS image

1 – M4 image

BIT(1): 0 – No encryption is present

1 - Image is encrypted

BIT(2): 0 - CRC based integrity check

1 - MIC based integrity check

BIT(3): 0 – No digital signature

1 - Digitally signed (digital signature is located at the end of the RPS file)

BIT(4): 0 – image will not be combined with another image

1 – image will be combined with another image

BITS: (5-15) - Reserved

SHA size 16 Represents the SHA size used to compute the digest for the digital signature

0 - Reserved

1 - SHA_256

2 - SHA_384

3 - SHA_512

Magic word 32 0x900D900D
Image Size 32 Size of the binary image
Firmware Version 32 Firmware version number, See table 2.1 for the version layout
Flash Address 32 Address in flash to store the image
CRC 32 CRC of the image 1
MIC 128 MIC of the image
Firmware Extended Version 32 Patch Version, Customer ID, Chip id, ROM Version
Reserved 96 -
Magic bytes 32 0x900D900D
Note:
  1. Polynomial to use can be decided at the time of manufacturing

The following table describes the boot descriptors layout.

Field

Size (bytes)

Description

Magic pattern

2

Pattern for identification of a valid Flash content (0x5aa5)

Offset

2

Offset of the binary image where the transfer should start from flash to RAM

IVT offset

4

Value to program VTOR register

Bootloader descriptor entries

56

Bootloader descriptor entries which are executed by the Bootloader while loading firmware. See following table that describes the bootloader descriptors layout. Space is provided for 7 bootloader descriptor entries.

The following table describes the bootloader descriptors layout.

Field

Size (bits)

Description

Length

24

Length of transfer to destination

Reserved

7

-

Last entry

1

If set, indicate it is last boot descriptor entry

Destination address

32

Destination address

Encrypted XIP#

Encrypted execute-in-place (XIP) allows encrypted firmware images to be decrypted immediately before runtime. Encrypted XIP is useful when program and data are stored in external flash.

In-System Programming (ISP)#

The secure firmware upgrade feature of the security bootloader checks the authenticity and integrity of the new firmware image, provided that these features have been enabled in the eFuse settings. The security bootloader will only update the image after successfully validating the authenticity of the image using the digital signature check and the integrity of the image using the MIC check, depending on which checks are enabled. If enabled, the anti-rollback feature will prevent downgrades to a lower firmware version, refer to section 2.x for more details. The security bootloader also supports OTA updates.