You are viewing documentation for version:
PDFRepresents the result of an mDNS query.
This structure contains details about the discovered mDNS service, including instance name, service type, protocol, hostname, port, TXT records, IP addresses, and TTL.
Public Attributes#
uint16_t
Type of mDNS query (e.g., PTR, SRV, A, AAAA, ANY)
const char *
Name of the service instance (e.g., "My Web Server")
const char *
Service type string (e.g., "_http")
const char *
Protocol string (e.g., "_tcp")
const char *
Hostname of the device offering the service.
uint16_t
Port number where the service is running.
const char **
Array of TXT record strings in "key=value" format.
struct sl_mdns_response_s::@0
TXT records associated with the service.
sl_ip_address_t *
Array of IP addresses (IPv4 or IPv6)
struct sl_mdns_response_s::@1
IP addresses associated with the service.
uint32_t
Time-to-live for the DNS record (in seconds)
Public Attribute Documentation#
query_type#
uint16_t sl_mdns_response_s::query_type
Type of mDNS query (e.g., PTR, SRV, A, AAAA, ANY)
instance_name#
const char* sl_mdns_response_s::instance_name
Name of the service instance (e.g., "My Web Server")
service_type#
const char* sl_mdns_response_s::service_type
Service type string (e.g., "_http")
proto#
const char* sl_mdns_response_s::proto
Protocol string (e.g., "_tcp")
hostname#
const char* sl_mdns_response_s::hostname
Hostname of the device offering the service.
port#
uint16_t sl_mdns_response_s::port
Port number where the service is running.
txt#
const char** sl_mdns_response_s::txt
Array of TXT record strings in "key=value" format.
txt_count#
uint32_t sl_mdns_response_s::txt_count
Number of TXT records.
txt#
struct sl_mdns_response_s::@0 sl_mdns_response_s::txt
TXT records associated with the service.
addr#
sl_ip_address_t* sl_mdns_response_s::addr
Array of IP addresses (IPv4 or IPv6)
addr_count#
uint32_t sl_mdns_response_s::addr_count
Number of IP addresses.
addr#
struct sl_mdns_response_s::@1 sl_mdns_response_s::addr
IP addresses associated with the service.
ttl#
uint32_t sl_mdns_response_s::ttl
Time-to-live for the DNS record (in seconds)