Sensor Hub#


Introduction#

  • Sensor Hub products are primarily intended to address consumer, industrial, and medical applications that require wireless connectivity, extremely low power, and high performance for sensor fusion algorithms. The MCU core, wireless connectivity, and peripherals are identical to the SI917 CCP Radio board.

  • Sensor Hub functions as a sensor management system, facilitating hardware abstraction layer, peripheral drivers, and sensor driver layer integration to collect and distribute desired sensor data.

  • It enables users to collect sensor data based on time interval or number of samples or when a specific data requirement are met.

  • Sensor Hub serves as a framework that can be seamlessly integrated into any application requiring sensor management.

  • The Sensor HUB works with sensors as per configurations provided by the application and notifies the necessary events throughout the application.

  • The configuration for the sensors must be provided through the sensor hub config file on which the sensor hub should act.

  • Sensor Hub relies on FreeRTOS using CMSIS RTOS version 2 wrapper.


Configuration#

  • Sensor Hub has 2 Sensor Mode:

  • - SL_SH_POLLING_MODE: This mode is Timer based.

  • - SL_SH_INTERRUPT_MODE: This mode is NPSS Button 0 GPIO Interrupt based.

  • There are 3 types of data_deliver.mode in Polling Sensor Mode and they are - SL_SH_THRESHOLD, - SL_SH_TIMEOUT and - SL_SH_NUM_OF_SAMPLES.

  • - SL_SH_NO_DATA data_deliver.mode is used when Interrupt Sensor Mode is selected.

  • If the user wants a value that sets a limit or boundary, above which the sensor data should be shown then - SL_SH_THRESHOLD mode should be chosen

  • - SL_SH_TIMEOUT mode is used when user wants to get the data at some intervals of time for some sampling time

  • - SL_SH_NUM_OF_SAMPLES mode is used when user wants to get the particular number of sensor data 

  • - SL_SH_NO_DATA mode is used when .

  • Here data_deliver.timeout is the time for which the sensor should keep collecting the data for.

  • sampling_interval is the the amount of time between two sensor data read is sampled or collected.

  • sampling_intr_req_pin is the GPIO pin for sampling the sensor data

  • Configure the number of sensors info in the /sensors/inc/sensors_config.h file

    #define - SL_MAX_NUM_SENSORS              5   // Maximum sensors present in the system
    
  • Modes: Using the configuration structure, one can configure the following parameters in the sensorhub_config.c file:

    • For POLLING Sensor Mode configure the below parameters:

      .sensor_mode                = - SL_SH_POLLING_MODE,
      .sampling_interval          = 100,
      
      • If sensor_mode is selected as - SL_SH_POLLING_MODE, then data_deliver.mode should be configured as one of the following for a sensor configuration structure:

        • For TIMEOUT Data Mode configure the below parameters:

          .data_deliver.mode          = - SL_SH_TIMEOUT,
          .data_deliver.timeout       = 1000,
          
        • For THRESHOLD Data Mode configure the below parameters:

          .data_deliver.mode          = - SL_SH_THRESHOLD,
          .data_deliver.threshold     = 1000,
          
        • For SAMPLING Data Mode configure the below parameters:

          .data_deliver.mode          = - SL_SH_NUM_OF_SAMPLES,
          .data_deliver.numOfSamples  = 5,
          
    • For INTERRUPT Sensor Mode configure the below parameters:

      .sensor_mode                = - SL_SH_INTERRUPT_MODE,
      .sampling_intr_req_pin      = BUTTON_0_GPIO_PIN,
      .sensor_intr_type           = - SL_SH_FALL_EDGE,
      .data_deliver.data_mode     = - SL_SH_NO_DATA_MODE,
      
  • To configure the PS2, please update the below macro in the preprocessor settings:

    - SL_SENSORHUB_POWERSAVE=1
    Enabling this macro will move the application from PS4 state to PS2 state. In PS2 state the sensor data will be sampled and collected.
    
  • To configure the power states to PS4 sleep or PS2 Sleep, please update the defines in sisdk/util/third_party/freertos/kernel/include/FreeRTOS.h file as below:

    #ifndef SL_SI91X_TICKLESS_MODE
    #define SL_SI91X_TICKLESS_MODE  1           // 1 is to Enable the tickless Idle mode
    #endif
    
    #ifndef configPRE_SLEEP_PROCESSING
    #define configPRE_SLEEP_PROCESSING(x) sli_si91x_sleep_wakeup(x)               // Here x is idle time,
    #endif
    
    // Configure the sleep time by using the below macro.
    // If the number of Ideal task ticks exceeds this value, the system is allowed to sleep.
    #ifndef configEXPECTED_IDLE_TIME_BEFORE_SLEEP
       #define configEXPECTED_IDLE_TIME_BEFORE_SLEEP    70
    #endif
    

    Note:

  • By using above sleep configuration, sensor hub is going to sleep by using the idle task and idle time.

  • If the Ideal time exceeds the expected sleep time value, the system is allowed to sleep.

  • The above idle time is fed to the Alarm timer, which we are using as a wake-up source.

ADC Configurations: Configure only below parameters for ADC to change its mode from FIFO to STATIC and vice versa

  • For ADC FIFO mode, configure as shown below:

    .adc_config.adc_cfg.operation_mode        = - SL_ADC_FIFO_MODE,
    .adc_config.adc_ch_cfg.sampling_rate[0]   = - SL_SH_ADC_SAMPLING_RATE, // Use 100 for FIFO Mode
    
  • For ADC Static mode, configure as shown below:

    .adc_config.adc_cfg.operation_mode        = - SL_ADC_STATIC_MODE,
    .adc_config.adc_ch_cfg.sampling_rate[0]   = - SL_SH_ADC_SAMPLING_RATE, // Use 1000 for Static Mode
    
  • To configure the PS1 power state from PS2 State, please update the below macro in the preprocessor settings:

    - SL_SH_ADC_PS1=1
     Enabling this macro will move the core from PS2 Active state to PS1 state
    
    • Please update the defines in sisdk/util/third_party/freertos/kernel/include/FreeRTOS.h file as below:

      #ifndef configUSE_TICKLESS_IDLE
      #define configUSE_TICKLESS_IDLE 1           // 1 is to Enable the tickless Idle mode
      #endif
      
      #ifndef configPRE_SLEEP_PROCESSING
      #define configPRE_SLEEP_PROCESSING(x) sli_si91x_sleep_wakeup(x)               // Here x is idle time,
      #endif
      

      Note:

    • The PS1 state transition only applies to ADC FIFO Mode. Before entering this mode, kindly turn off any other sensors.


Usage#

Sensorhub provides two apis which user can use for intergrating into any application

  • sl_si91x_sensorhub_app_task(void);

  • sl_si91x_sensor_event_handler(uint8_t sensor_id, uint8_t event);

sl_si91x_sensorhub_app_task(void): initialises and starts sensor data collection. it achieves this by calling the following apis

sl_si91x_sensorhub_notify_cb_register(sl_sensor_signalEvent_t cb_event, sl_sensor_id_t *cb_ack): links the event handler provided by the user as a callback function in the event task

sl_si91x_sensorhub_init(): initializes the peripherals I2C, SPI, ADC, SDC

sl_si91x_sensorhub_detect_sensors(sl_sensor_id_t *sensor_id_info, uint8_t num_of_sensors): scans the i2c sensors provided in the sensorhub_config.c and returns the number of these sensors that are currently connected

sl_si91x_sensorhub_create_sensor(sl_sensor_id_t sensor_id): Initializes the sensor by calling the init function of the sensor provided by the user in the respective HAL, Assigs memory to it based on the data delivery mode, Creates a timer for this sensor if required

sl_si91x_sensor_hub_start(): initializes the sensor task, event task and power task

sl_si91x_sensorhub_start_sensor(sl_sensor_id_t sensor_id): starts the timers of the sensors created in create sensor api

sl_si91x_sensor_event_handler(uint8_t sensor_id, uint8_t event) is called by the event task after sensor data is collected ,in the sensorhub appilcation it prints the data based on the sensor id and uploads it to the cloud

Modules#

sl_sensorhub_errors_t

sl_data_deliver_type_t

sl_sensor_info_t

sl_sensor_handle_t

sl_sensor_list_t

sl_intr_list_t

sl_intr_list_map_t

sl_em_event_t

sl_sensor_cb_info_t

sl_i2c_config_t

sl_spi_config_t

sl_adc_config

sl_gpio_config_t

Enumerations#

enum
SL_SH_POLLING_MODE
SL_SH_INTERRUPT_MODE
SL_SH_NO_MODE
}

Enumeration for Sensor HUB data reading mode.

enum
SL_SENSOR_CREATION_FAILED
SL_SENSOR_STARTED
SL_SENSOR_STOPPED
SL_SENSOR_DATA_READY
SL_SENSOR_CNFG_INVALID
SL_SENSOR_START_FAILED
SL_SENSOR_STOP_FAILED
SL_SENSOR_DELETED
SL_SENSOR_DELETE_FAILED
}

Enumeration for Sensor Hub Callback Events.

enum
SL_SH_RISE_EDGE
SL_SH_FALL_EDGE
SL_SH_LOW_LEVEL
SL_SH_HIGH_LEVEL
}

Enumeration for GPIO Interrupt Configurations.

enum
SL_SH_THRESHOLD
SL_SH_TIMEOUT
SL_SH_NUM_OF_SAMPLES
SL_SH_NO_DATA_MODE
}

Enumeration for Sensor HUB data delivery mode.

enum
SL_SENSOR_INVALID
SL_SENSOR_VALID
SL_SENSOR_START
SL_SENSOR_STOP
}

Enumeration for Sensors Status.

Typedefs#

typedef struct sl_adc_config

ADC bus interface configuration structure.

Functions#

sl_status_t

To initialize Peripherals of Sensor HUB.

sl_status_t
sl_si91x_sensorhub_detect_sensors(sl_sensor_id_t sensor_id_info[], uint8_t num_of_sensors)

To detect the I2C sensors.

sl_status_t
sl_si91x_sensorhub_delete_sensor(sl_sensor_id_t sensor_id)

To delete specific sensor from the Sensor HUB list.

sl_status_t
sl_si91x_sensorhub_create_sensor(sl_sensor_id_t sensor_id)

To create a sensor instance in the sensor hub list.

sl_status_t
sl_si91x_sensorhub_start_sensor(sl_sensor_id_t sensor_id)

To start sensor operation of the given sensor.

sl_status_t
sl_si91x_sensorhub_stop_sensor(sl_sensor_id_t sensor_id)

To stop sensor operation of the given sensor.

void
sl_si91x_em_post_event(sl_sensor_id_t sensor_id, sl_sensorhub_event_t event, void *dataPtr, TickType_t ticks_to_wait) SL_DEPRECATED_API_WISECONNECT_4_0

To post the events to Event Manager (EM) to be notified to the application.

void
sl_si91x_sensor_task(void) SL_DEPRECATED_API_WISECONNECT_4_0

Task to handle the sensor operations.

void
sl_si91x_power_state_task(void) SL_DEPRECATED_API_WISECONNECT_4_0

Task to handle the system power operations.

void
sl_si91x_em_task(void) SL_DEPRECATED_API_WISECONNECT_4_0

Task to handle the operations of the Event Manager (EM).

int32_t
sli_si91x_i2c_init(void) SL_DEPRECATED_API_WISECONNECT_4_0

To initialize the I2C interface based on configuration.

int32_t
sli_si91x_spi_init(void) SL_DEPRECATED_API_WISECONNECT_4_0

To initialize SPI Interface based on configuration.

int32_t
sli_si91x_i2c_sensors_scan(uint16_t address) SL_DEPRECATED_API_WISECONNECT_4_0

To scan the I2C sensors.

sl_sensor_impl_type_t *
sli_si91x_get_sensor_implementation(int32_t sensor_id) SL_DEPRECATED_API_WISECONNECT_4_0

To get sensor implementation.

int32_t
sli_si91x_create_sensor_list_index() SL_DEPRECATED_API_WISECONNECT_4_0

To create sensor list index.

uint32_t
sli_si91x_get_sensor_index(sl_sensor_id_t sensor_id) SL_DEPRECATED_API_WISECONNECT_4_0

To get sensor index for the sensor list.

uint32_t
sli_si91x_delete_sensor_list_index(sl_sensor_id_t sensor_id) SL_DEPRECATED_API_WISECONNECT_4_0

To delete the sensor index for the sensor list.

sli_si91x_get_sensor_info(sl_sensor_id_t sensor_id) SL_DEPRECATED_API_WISECONNECT_4_0

To get sensor info from the sensor configuration structure.

sl_status_t
sl_si91x_sensorhub_notify_cb_register(sl_sensor_signalEvent_t cb_event, sl_sensor_id_t *cb_ack)

To register callback function to the application.

void
sl_si91x_sensors_timer_cb(TimerHandle_t xTimer) SL_DEPRECATED_API_WISECONNECT_4_0

Callback function to set the event flag.

sl_status_t
sl_si91x_gpio_interrupt_config(uint16_t gpio_pin, sl_si91x_gpio_interrupt_config_flag_t intr_type) SL_DEPRECATED_API_WISECONNECT_4_0

To configuring different types of NPSS GPIO interrupts in the Sensor HUB.

void
sl_si91x_gpio_interrupt_start(uint16_t gpio_pin) SL_DEPRECATED_API_WISECONNECT_4_0

To enable and set the priority of NPSS GPIO interrupt.

void
sl_si91x_gpio_interrupt_stop(uint16_t gpio_pin) SL_DEPRECATED_API_WISECONNECT_4_0

To mask and disable the NPSS GPIO interrupt.

sl_status_t

To start the sensor hub tasks.

void
sli_si91x_set_alarm_intr_time(uint16_t interval) SL_DEPRECATED_API_WISECONNECT_4_0

To set the alarm interrupt time.

void
sli_si91x_init_m4alarm_config(void) SL_DEPRECATED_API_WISECONNECT_4_0

To initialize the Alarm block.

void
sli_si91x_config_wakeup_source(uint16_t sleep_time) SL_DEPRECATED_API_WISECONNECT_4_0

To configure wake-up source for the system.

void
sli_si91x_sleep_wakeup(uint16_t sh_sleep_time) SL_DEPRECATED_API_WISECONNECT_4_0

To configures sleep/wakeup sources for the system.

void
sli_si91x_sensorhub_ps4tops2_state(void) SL_DEPRECATED_API_WISECONNECT_4_0

To change the system status from PS4 to PS2.

void
sli_si91x_sensorhub_ps2tops4_state(void) SL_DEPRECATED_API_WISECONNECT_4_0

To change the system status from PS2 to PS4.

sl_status_t
sli_si91x_adc_init(void) SL_DEPRECATED_API_WISECONNECT_4_0

To initialize ADC Interface based on configuration.

void

To initialize and configure systic timer for the RTOS.

void
ARM_I2C_SignalEvent(uint32_t event)

I2C event handler.

To fetch ADC bus interface information.

void
sl_si91x_adc_callback(uint8_t channel_no, uint8_t event) SL_DEPRECATED_API_WISECONNECT_4_0

ADC callback to set event flag.

sl_status_t
sli_si91x_sdc_init(void) SL_DEPRECATED_API_WISECONNECT_4_0

To initialize sdc Interface based on the configuration.

Macros#

#define
SL_SH_SENSOR_TASK_STACK_SIZE (1024 * 2)

Sensor task stack size.

#define
SL_SH_EM_TASK_STACK_SIZE (512 * 2)

EM task stack size.

#define
SL_SH_POWER_SAVE_TASK_STACK_SIZE (512 * 2)

Power task stack size.

#define
SL_EM_TASK_RUN_TICKS osWaitForever

Max wait time of message queue in Event task.

#define
MAP_TABLE_SIZE 10

Size of the sensors interrupt MAP table.

#define
NPSS_GPIO_IRQHandler IRQ021_Handler

NPSS gpio IRQ handler.

#define
NPSS_GPIO_NVIC NPSS_TO_MCU_GPIO_INTR_IRQn

NPSS gpio IRQ Number 21.

#define
SL_ALARM_PERIODIC_TIME 10

Periodic alarm configuration in milliseconds.

#define
RC_TRIGGER_TIME 5

RC clock trigger time.

#define
RO_TRIGGER_TIME 0

RO clock trigger time.

#define
NO_OF_HOURS_IN_A_DAY 24

Number of hours in a day.

#define
NO_OF_MINUTES_IN_AN_HOUR 60

Number of minutes in an hour.

#define
NO_OF_SECONDS_IN_A_MINUTE 60

Number of Seconds in a minute.

#define
NO_OF_MILLISECONDS_IN_A_SECOND 1000

Number of milliseconds in a second.

#define
NO_OF_MONTHS_IN_A_YEAR 12

Number of months in a year.

#define
BASE_YEAR 2000

Start year for alarm configuration.

#define
NO_OF_DAYS_IN_A_MONTH_1 28

Month with 28 days.

#define
NO_OF_DAYS_IN_A_MONTH_2 29

Month with 29 days.

#define
NO_OF_DAYS_IN_A_MONTH_3 30

Month with 30 days.

#define
NO_OF_DAYS_IN_A_MONTH_4 31

Month with 31 days.

#define
RTC_ALARM_IRQHandler IRQ028_Handler

Alarm IRQ handler.

#define
NVIC_RTC_ALARM MCU_CAL_ALARM_IRQn

Alarm IRQ number 28.

#define
SL_SH_TIMER_CREATION_FAILED (1 << SL_SH_SENSORHUB_ERRORS_MASK)

Creating OS timer for the sensor failed.

#define
SL_SH_TIMER_DELETION_FAILED (2 << SL_SH_SENSORHUB_ERRORS_MASK)

Deleting OS timer of the sensor failed.

#define
SL_SH_TIMER_START_FAIL (3 << SL_SH_SENSORHUB_ERRORS_MASK)

Starting OS timer of the sensor failed.

#define
SL_SH_TIMER_STOP_FAIL (4 << SL_SH_SENSORHUB_ERRORS_MASK)

Stopping OS timer of the sensor failed.

#define
SL_SH_MAX_SENSORS_REACHED (5 << SL_SH_SENSORHUB_ERRORS_MASK)

Max number of sensor limit reached.

#define
SL_SH_MEMORY_LIMIT_EXCEEDED (6 << SL_SH_SENSORHUB_ERRORS_MASK)

Memory allocation for sensor data storage failed.

#define
SL_SH_SENSOR_CREATE_FAIL (7 << SL_SH_SENSORHUB_ERRORS_MASK)

Sensor API is called for a sensor without creating it.

#define
SL_SH_COMMAND_SET_POWER_FAIL (8 << SL_SH_SENSORHUB_ERRORS_MASK)

Sensor set power command execution failed.

#define
SL_SH_COMMAND_SET_RANGE_FAIL (9 << SL_SH_SENSORHUB_ERRORS_MASK)

Sensor set range command execution failed.

#define
SL_SH_COMMAND_SELF_TEST_FAIL (10 << SL_SH_SENSORHUB_ERRORS_MASK)

Sensor self-test command execution failed.

#define
SL_SH_INVALID_PARAMETERS (11 << SL_SH_SENSORHUB_ERRORS_MASK)

Generic error code for any invalid parameters.

#define
SL_SH_GPIO_OUT_OF_RANGE (12 << SL_SH_SENSORHUB_ERRORS_MASK)

Invalid gpio number.

#define
SL_SH_SENSOR_IMPLEMENTATION_NOT_FOUND (13 << SL_SH_SENSORHUB_ERRORS_MASK)

No hal implementation found for given sensor type.

#define
SL_SH_INTERRUPT_TYPE_CONFIG_FAIL (14 << SL_SH_SENSORHUB_ERRORS_MASK)

Interrupt type configuration failed.

#define
SL_SH_MEMORY_ALLOCATION_FAILED (15 << SL_SH_SENSORHUB_ERRORS_MASK)

Allocating memory for sensor hal failed.

#define
SL_SH_SENSOR_INDEX_NOT_FOUND (0xFF)

Sensor not created.

#define
SL_SH_CONFIG_NOT_FOUND (16 << SL_SH_SENSORHUB_ERRORS_MASK)

Sensor configuration not found.

#define
SL_SH_INVALID_ADDRESS (17 << SL_SH_SENSORHUB_ERRORS_MASK)

No sensor found at given address.

#define
SL_SH_WRONG_INTERRUPT_TYPE (18 << SL_SH_SENSORHUB_ERRORS_MASK)

Invalid interrupt type is given for the sensor.

#define
SL_SH_INVALID_MODE (19 << SL_SH_SENSORHUB_ERRORS_MASK)

Invalid mode is given for the sensor.

#define
SL_SH_INVALID_DELIVERY_MODE (20 << SL_SH_SENSORHUB_ERRORS_MASK)

Invalid delivery mode is given for the sensor.

#define
SL_SH_HAL_SENSOR_CREATION_FAILED (21 << SL_SH_SENSORHUB_ERRORS_MASK)

Create sensor in HAL failed.

#define
SL_SH_HAL_SENSOR_DELETION_FAILED (22 << SL_SH_SENSORHUB_ERRORS_MASK)

Delete sensor in HAL failed.

#define
SL_SH_HAL_SENSOR_SAMPLE_FAIL (23 << SL_SH_SENSORHUB_ERRORS_MASK)

Sample sensor in HAL failed.

#define
SL_SH_HAL_SENSOR_CONTROL_FAIL (24 << SL_SH_SENSORHUB_ERRORS_MASK)

Control sensor in HAL failed.

#define
SL_SH_POWER_TASK_CREATION_FAILED (25 << SL_SH_SENSORHUB_ERRORS_MASK)

Power task creation failed.

#define
SL_SH_SENSOR_TASK_CREATION_FAILED (26 << SL_SH_SENSORHUB_ERRORS_MASK)

Sensor task creation failed.

#define
SL_SH_EM_TASK_CREATION_FAILED (27 << SL_SH_SENSORHUB_ERRORS_MASK)

EM task creation failed.

#define
SL_ALL_PERIPHERALS_INIT_FAILED (28 << SL_SH_SENSORHUB_ERRORS_MASK)

All(i2c,spi,adc) peripheral's initialization failed.

Enumeration Documentation#

sl_sensor_mode_t#

sl_sensor_mode_t

Enumeration for Sensor HUB data reading mode.

Enumerator
SL_SH_POLLING_MODE

POLLING_MODE.

SL_SH_INTERRUPT_MODE

INTERRUPT_MODE.

SL_SH_NO_MODE

NO_MODE.


sl_sensorhub_event_t#

sl_sensorhub_event_t

Enumeration for Sensor Hub Callback Events.

This enumeration defines various events related to the operation of sensors within a Sensor Hub. The events represent different states and actions of the sensors, such as creation, starting, stopping, and data readiness.

Enumerator
SL_SENSOR_CREATION_FAILED

Event indicating that sensor creation failed.

SL_SENSOR_STARTED

Event indicating that the sensor has started successfully.

SL_SENSOR_STOPPED

Event indicating that the sensor has stopped.

SL_SENSOR_DATA_READY

Event indicating that sensor data is ready to be read.

SL_SENSOR_CNFG_INVALID

Event indicating that the sensor configuration is invalid.

SL_SENSOR_START_FAILED

Event indicating that the sensor failed to start.

SL_SENSOR_STOP_FAILED

Event indicating that the sensor failed to stop.

SL_SENSOR_DELETED

Event indicating that the sensor has been deleted.

SL_SENSOR_DELETE_FAILED

Event indicating that the sensor deletion failed.


sl_gpio_intr_type_t#

sl_gpio_intr_type_t

Enumeration for GPIO Interrupt Configurations.

Enumerator
SL_SH_RISE_EDGE

Interrupt at GPIO rise edge.

SL_SH_FALL_EDGE

Interrupt at GPIO fall edge.

SL_SH_LOW_LEVEL

Interrupt at GPIO low level.

SL_SH_HIGH_LEVEL

Interrupt at GPIO high level.


sl_data_deliver_mode_t#

sl_data_deliver_mode_t

Enumeration for Sensor HUB data delivery mode.

Enumerator
SL_SH_THRESHOLD

Threshold value for sensor data delivery.

SL_SH_TIMEOUT

Timeout value for sensor data delivery.

SL_SH_NUM_OF_SAMPLES

Number of samples for sensor data delivery.

SL_SH_NO_DATA_MODE

Intterupt mode data delivery.


sl_sensor_status_t#

sl_sensor_status_t

Enumeration for Sensors Status.

Enumerator
SL_SENSOR_INVALID

Sensor is Invalid.

SL_SENSOR_VALID

Sensor is Valid.

SL_SENSOR_START

Sensor has Started.

SL_SENSOR_STOP

Sensor has Stoped.


Typedef Documentation#

sl_adc_cfg_t#

typedef struct sl_adc_config sl_adc_cfg_t

ADC bus interface configuration structure.


Function Documentation#

sl_si91x_sensorhub_init#

sl_status_t sl_si91x_sensorhub_init ()

To initialize Peripherals of Sensor HUB.

This function will initialize the Peripherals like I2C/SPI/ADC, based on the user configuration.

Returns

  • Status code indicating the result:

    • SL_STATUS_OK - Success, peripherals initialization was done properly.

    • SL_STATUS_FAIL - Failed, peripherals initialization failed.

    • SL_ALL_PERIPHERALS_INIT_FAILED , All peripherals initializaion failed.

For more information on status codes, see SL STATUS DOCUMENTATION.


sl_si91x_sensorhub_detect_sensors#

sl_status_t sl_si91x_sensorhub_detect_sensors (sl_sensor_id_t sensor_id_info, uint8_t num_of_sensors)

To detect the I2C sensors.

Parameters
TypeDirectionArgument NameDescription
sl_sensor_id_t[in]sensor_id_info

- Sensor IDs.

uint8_t[in]num_of_sensors

- Number of sensors given by user.

This function detects I2C sensors according to user configuration and stores the scanned sensor IDs in the provided structure. Returns

  • Number of sensors scanned, if successful.


sl_si91x_sensorhub_delete_sensor#

sl_status_t sl_si91x_sensorhub_delete_sensor (sl_sensor_id_t sensor_id)

To delete specific sensor from the Sensor HUB list.

Parameters
TypeDirectionArgument NameDescription
sl_sensor_id_t[in]sensor_id

- Sensor ID.

This function will delete the specific sensor from the sensor list, modify the sensor status to invalid, and publish the events to the event task.

Returns

  • Status code indicating the result:

    • SL_STATUS_OK - Success, delete sensor success.

    • SL_SH_TIMER_DELETION_FAILED - Timer deletion failed.

    • SL_SH_COMMAND_SET_POWER_FAIL - Set power failed.

    • SL_SH_HAL_SENSOR_DELETION_FAILED - Sensor deletion failed at HAL layer.

    • SL_SH_SENSOR_INDEX_NOT_FOUND - Given sensor index not found.

For more information on status codes, see SL STATUS DOCUMENTATION.


sl_si91x_sensorhub_create_sensor#

sl_status_t sl_si91x_sensorhub_create_sensor (sl_sensor_id_t sensor_id)

To create a sensor instance in the sensor hub list.

Parameters
TypeDirectionArgument NameDescription
sl_sensor_id_t[in]sensor_id

- Sensor ID.

This function creates a sensor instance as per user configuration. It also allocates max sample memory for the configured sensor.

Returns

  • Status code indicating the result:

    • SL_STATUS_OK - Create sensor instance success.

    • SL_SH_TIMER_CREATION_FAILED - Timer creation for the sensor failed.

    • SL_SH_MAX_SENSORS_REACHED - Maximum number of sensors reached.

    • SL_SH_MEMORY_LIMIT_EXCEEDED - Memory limit exceeded.

    • SL_SH_COMMAND_SET_POWER_FAIL - Command to set power failed.

    • SL_SH_COMMAND_SET_RANGE_FAIL - Command to set range failed.

    • SL_SH_COMMAND_SELF_TEST_FAIL - Command for the self test failed.

    • SL_SH_SENSOR_IMPLEMENTATION_NOT_FOUND - Implementation of the sensor not found.

    • SL_SH_CONFIG_NOT_FOUND - Configuration of the sensor not found.

    • SL_SH_INVALID_MODE - Invalid mode.

    • SL_SH_HAL_SENSOR_CREATION_FAILED - Sensor creation failed at HAL. For more information on status codes, see SL STATUS DOCUMENTATION.


sl_si91x_sensorhub_start_sensor#

sl_status_t sl_si91x_sensorhub_start_sensor (sl_sensor_id_t sensor_id)

To start sensor operation of the given sensor.

Parameters
TypeDirectionArgument NameDescription
sl_sensor_id_t[in]sensor_id

- Sensor ID.

This function can be called after creating a sensor with given sensor ID It performs the following operations:

  • Starts timer for sensor with polling mode.

  • Enable IRQ handle for sensor with interrupt mode.

Returns

  • Status code indicating the result:

    • SL_STATUS_OK - Success, sensor started.

    • SL_SH_TIMER_START_FAIL - Failed to start timer.

    • SL_SH_SENSOR_CREATE_FAIL - Given sensor not created.

    • SL_SH_INVALID_MODE - Invaild mode given.

For more information on status codes, see SL STATUS DOCUMENTATION.


sl_si91x_sensorhub_stop_sensor#

sl_status_t sl_si91x_sensorhub_stop_sensor (sl_sensor_id_t sensor_id)

To stop sensor operation of the given sensor.

Parameters
TypeDirectionArgument NameDescription
sl_sensor_id_t[in]sensor_id

- Sensor ID.

This function performs the following operations:

  • Stop the sensor operations of the given sensor.

  • Based on the sensor mode it will stop the polling/interrupt mode operations and updates the sensor statutes.

  • Disable IRQ handles of the interrupt mode sensors.

Returns

  • Status code indicating the result:

    • SL_STATUS_OK - Success, sensor stopped.

    • SL_SH_TIMER_STOP_FAIL - Failed to stop timer.

    • SL_SH_SENSOR_CREATE_FAIL - Given sensor not created.

For more information on status codes, see SL STATUS DOCUMENTATION.


sl_si91x_em_post_event#

void sl_si91x_em_post_event (sl_sensor_id_t sensor_id, sl_sensorhub_event_t event, void * dataPtr, TickType_t ticks_to_wait)

To post the events to Event Manager (EM) to be notified to the application.

Parameters
TypeDirectionArgument NameDescription
sl_sensor_id_t[in]sensor_id

- Sensor ID.

sl_sensorhub_event_t[in]event

- Sensor hub events.

void *[in]dataPtr

- Sensor data pointer.

TickType_t[in]ticks_to_wait

- Max time to wait for the post.

It waits for mutex till ticks_to_wait and updates event queue if mutex is acquired


sl_si91x_sensor_task#

void sl_si91x_sensor_task (void )

Task to handle the sensor operations.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Sensor Task performs the following operations:

  • Create the OS event and mutex to perform the sensor operations.

  • Sample the sensor data based on the event flags.

  • Check the events and post the sensor data to the EM task based on the sensor data delivery mode.


sl_si91x_power_state_task#

void sl_si91x_power_state_task (void )

Task to handle the system power operations.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Power state task changes the system from one power save mode to another power save mode like(PS4 to PS2),(PS2toPS4),(Sleep_mode) using Binary semaphore.


sl_si91x_em_task#

void sl_si91x_em_task (void )

Task to handle the operations of the Event Manager (EM).

Parameters
TypeDirectionArgument NameDescription
voidN/A

EM task performs the following operations:

  • Create the osMessageQueue and mutex to perform the event operations.

  • Calls the callback event.


sli_si91x_i2c_init#

int32_t sli_si91x_i2c_init (void )

To initialize the I2C interface based on configuration.

Parameters
TypeDirectionArgument NameDescription
voidN/A

This function will configure/Initialize I2C Interface based on configuration.

Returns

  • I2C Initializtion status


sli_si91x_spi_init#

int32_t sli_si91x_spi_init (void )

To initialize SPI Interface based on configuration.

Parameters
TypeDirectionArgument NameDescription
voidN/A

This function will configure/Initialize SPI Interface based on configuration.

Returns

  • SPI Initializtion status.


sli_si91x_i2c_sensors_scan#

int32_t sli_si91x_i2c_sensors_scan (uint16_t address)

To scan the I2C sensors.

Parameters
TypeDirectionArgument NameDescription
uint16_t[in]address

- Address of sensor

This function will scan the I2C sensors based on the sensor address.

Returns

  • Status 0 if successful; otherwise, it will wait for the sensor response.


sli_si91x_get_sensor_implementation#

sl_sensor_impl_type_t * sli_si91x_get_sensor_implementation (int32_t sensor_id)

To get sensor implementation.

Parameters
TypeDirectionArgument NameDescription
int32_t[in]sensor_id

- Sensor ID.

This function will get the sensor implementation of the sensor based on sensor ID.

Returns

  • If successful, it returns the Sensor implementation structure. Otherwise, it returns NULL.


sli_si91x_create_sensor_list_index#

int32_t sli_si91x_create_sensor_list_index ()

To create sensor list index.

This function will create the sensor list index based on the sensor status For the maximum sensors available in the sensor hub

Returns

  • Returns the sensor index in sensor_list.


sli_si91x_get_sensor_index#

uint32_t sli_si91x_get_sensor_index (sl_sensor_id_t sensor_id)

To get sensor index for the sensor list.

Parameters
TypeDirectionArgument NameDescription
sl_sensor_id_t[in]sensor_id

- Sensor ID.

This function will retrieve the sensor index from the sensor list based on the sensor status and sensor ID for the maximum number of sensors available in the sensor hub.

Returns

  • If successful, it returns the sensor index. Otherwise, it returns - SL_SH_SENSOR_INDEX_NOT_FOUND.


sli_si91x_delete_sensor_list_index#

uint32_t sli_si91x_delete_sensor_list_index (sl_sensor_id_t sensor_id)

To delete the sensor index for the sensor list.

Parameters
TypeDirectionArgument NameDescription
sl_sensor_id_t[in]sensor_id

- Sensor ID.

This function will delete the sensor from the sensor list based on the sensor ID for the maximum number of sensors available in the sensor hub.

Returns

  • If successful, it returns the sensor index. Otherwise, it returns error code - SL_SH_SENSOR_INDEX_NOT_FOUND.


sli_si91x_get_sensor_info#

sl_sensor_info_t * sli_si91x_get_sensor_info (sl_sensor_id_t sensor_id)

To get sensor info from the sensor configuration structure.

Parameters
TypeDirectionArgument NameDescription
sl_sensor_id_t[in]sensor_id

- Sensor ID.

This function will retrieve sensor data from the sensor configuration structure to update the sensor list configuration structure for the maximum number of sensors available in the sensor hub.

Returns

  • If successful, it returns the sensor information. Otherwise, it returns NULL.


sl_si91x_sensorhub_notify_cb_register#

sl_status_t sl_si91x_sensorhub_notify_cb_register (sl_sensor_signalEvent_t cb_event, sl_sensor_id_t * cb_ack)

To register callback function to the application.

Parameters
TypeDirectionArgument NameDescription
sl_sensor_signalEvent_t[in]cb_event

- Pointer to the callback event.

sl_sensor_id_t *[in]cb_ack

- Pointer to callback acknowledge to the application.

This function will update the callback function event and acknowledgment.

Returns

  • Status code indicating the result:

    • SL_STATUS_OK - Success, callback registered.

    • SL_SH_INVALID_PARAMETERS - Invalid parameters.

For more information on status codes, see SL STATUS DOCUMENTATION.


sl_si91x_sensors_timer_cb#

void sl_si91x_sensors_timer_cb (TimerHandle_t xTimer)

Callback function to set the event flag.

Parameters
TypeDirectionArgument NameDescription
TimerHandle_t[in]xTimer

- Timer handle.

This function will set the event flag bits based on the sensor sampling intervals. In the polling mode call the timer call-back function.


sl_si91x_gpio_interrupt_config#

sl_status_t sl_si91x_gpio_interrupt_config (uint16_t gpio_pin, sl_si91x_gpio_interrupt_config_flag_t intr_type)

To configuring different types of NPSS GPIO interrupts in the Sensor HUB.

Parameters
TypeDirectionArgument NameDescription
uint16_t[in]gpio_pin

- NPSS GPIO pin number.

sl_si91x_gpio_interrupt_config_flag_t[in]intr_type

- NPSS GPIO interrupt type.

This function configures the NPSS GPIOs and enables the interrupt mode for the gpios.

Returns

  • Status code indicating the result:

    • SL_STATUS_OK - Success, interrupt configured.

    • SL_SH_INTERRUPT_TYPE_CONFIG_FAIL - Invaild interrupt type.

For more information on status codes, see SL STATUS DOCUMENTATION.


sl_si91x_gpio_interrupt_start#

void sl_si91x_gpio_interrupt_start (uint16_t gpio_pin)

To enable and set the priority of NPSS GPIO interrupt.

Parameters
TypeDirectionArgument NameDescription
uint16_t[in]gpio_pin

- NPSS GPIO pin number.

This function configures and sets the priority of the NPSS GPIO interrupt. GPIO interrupt priority is (configMAX_SYSCALL_INTERRUPT_PRIORITY - 1)


sl_si91x_gpio_interrupt_stop#

void sl_si91x_gpio_interrupt_stop (uint16_t gpio_pin)

To mask and disable the NPSS GPIO interrupt.

Parameters
TypeDirectionArgument NameDescription
uint16_t[in]gpio_pin

- NPSS GPIO pin number.

This function masks and disables the IRQ handler of the NPSS GPIO interrupt.


sl_si91x_sensor_hub_start#

sl_status_t sl_si91x_sensor_hub_start (void )

To start the sensor hub tasks.

Parameters
TypeDirectionArgument NameDescription
voidN/A

This Starts the sensor hub Tasks.

Returns

  • Status code indicating the result:

    • SL_STATUS_OK - Success, sensorhub started.

    • SL_SH_POWER_TASK_CREATION_FAILED - Failed to create power task.

    • SL_SH_SENSOR_TASK_CREATION_FAILED - Failed to create sensor task.

    • SL_SH_EM_TASK_CREATION_FAILED - Failed to create EM task.

For more information on status codes, see SL STATUS DOCUMENTATION.


sli_si91x_set_alarm_intr_time#

void sli_si91x_set_alarm_intr_time (uint16_t interval)

To set the alarm interrupt time.

Parameters
TypeDirectionArgument NameDescription
uint16_t[in]interval

- interval time

This function will set the alarm interrupt based on the periodic time.


sli_si91x_init_m4alarm_config#

void sli_si91x_init_m4alarm_config (void )

To initialize the Alarm block.

Parameters
TypeDirectionArgument NameDescription
voidN/A

This function will initialize the Alarm block.


sli_si91x_config_wakeup_source#

void sli_si91x_config_wakeup_source (uint16_t sleep_time)

To configure wake-up source for the system.

Parameters
TypeDirectionArgument NameDescription
uint16_t[in]sleep_time

- Sleep time for the sensor hub.

This function will configure the wake-up source to the system.


sli_si91x_sleep_wakeup#

void sli_si91x_sleep_wakeup (uint16_t sh_sleep_time)

To configures sleep/wakeup sources for the system.

Parameters
TypeDirectionArgument NameDescription
uint16_t[in]sh_sleep_time

- Sleep time for the sensor hub, in ADC PS-1 no parameters.

This function will configure sleep/wakeup sources.


sli_si91x_sensorhub_ps4tops2_state#

void sli_si91x_sensorhub_ps4tops2_state (void )

To change the system status from PS4 to PS2.

Parameters
TypeDirectionArgument NameDescription
voidN/A

This function will change the system status from PS4 to PS2.


sli_si91x_sensorhub_ps2tops4_state#

void sli_si91x_sensorhub_ps2tops4_state (void )

To change the system status from PS2 to PS4.

Parameters
TypeDirectionArgument NameDescription
voidN/A

This function will change the system status from PS2 to PS4.


sli_si91x_adc_init#

sl_status_t sli_si91x_adc_init (void )

To initialize ADC Interface based on configuration.

Parameters
TypeDirectionArgument NameDescription
voidN/A

This function will configure/Initialize ADC Interface based on configuration.

Returns

  • Status code indicating the result:

    • SL_STATUS_OK - Success, ADC initialized.

    • SL_STATUS_FAIL - Failed to initialize ADC .

For more information on status codes, see SL STATUS DOCUMENTATION.


vPortSetupTimerInterrupt#

void vPortSetupTimerInterrupt (void )

To initialize and configure systic timer for the RTOS.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Set up the systic timer to generate the tick interrupts at the required frequency.


ARM_I2C_SignalEvent#

void ARM_I2C_SignalEvent (uint32_t event)

I2C event handler.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]event

- I2C transmit and receive events.


sl_si91x_fetch_adc_bus_intf_info#

sl_adc_cfg_t * sl_si91x_fetch_adc_bus_intf_info (void )

To fetch ADC bus interface information.

Parameters
TypeDirectionArgument NameDescription
voidN/A

This can be used by lower level layers. Returns

  • Pointer to ADC configuration structure.


sl_si91x_adc_callback#

void sl_si91x_adc_callback (uint8_t channel_no, uint8_t event)

ADC callback to set event flag.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]channel_no

- Respective channel number.

uint8_t[in]event

- Callback event (ADC_STATIC_MODE_CALLBACK, ADC_THRSHOLD_CALLBACK, INTERNAL_DMA, FIFO_MODE_EVENT).

This callback function is called when ADC event occured and it sets event flag corresponding to that event


sli_si91x_sdc_init#

sl_status_t sli_si91x_sdc_init (void )

To initialize sdc Interface based on the configuration.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • Returns status 0 if successful. Otherwise, it returns an error code.

    • SL_STATUS_FAIL - Fail.

    • SL_STATUS_OK - Success.

For more information on status codes, see SL STATUS DOCUMENTATION.