Structure to configure a vendor-specific IE.

This structure is used to add or remove a vendor-specific IE.

Public Attributes#

uint8_t

Unique ID for the IE (must be < SLI_MAX_VENDOR_IE)

uint16_t

Bitmap indicating which management frames to include the IE in.

uint16_t

Length of the IE buffer (must be < SLI_MAX_VENDOR_IE_BUFFER_LENGTH)

uint8_t *

Pointer to raw IE buffer.

Public Attribute Documentation#

unique_id#

uint8_t sl_wifi_vendor_ie_t::unique_id

Unique ID for the IE (must be < SLI_MAX_VENDOR_IE)


mgmt_frame_bitmap#

uint16_t sl_wifi_vendor_ie_t::mgmt_frame_bitmap

Bitmap indicating which management frames to include the IE in.


ie_buffer_length#

uint16_t sl_wifi_vendor_ie_t::ie_buffer_length

Length of the IE buffer (must be < SLI_MAX_VENDOR_IE_BUFFER_LENGTH)


ie_buffer#

uint8_t* sl_wifi_vendor_ie_t::ie_buffer

Pointer to raw IE buffer.