License#
Copyright 2025 Silicon Laboratories Inc. www.silabs.com
SPDX-License-Identifier: Zlib
The licensor of this software is Silicon Laboratories Inc.
This software is provided 'as-is', without any express or implied warranty. In no event will the authors be held liable for any damages arising from the use of this software.
Permission is granted to anyone to use this software for any purpose, including commercial applications, and to alter it and redistribute it freely, subject to the following restrictions:
The origin of this software must not be misrepresented; you must not claim that you wrote the original software. If you use this software in a product, an acknowledgment in the product documentation would be appreciated but is not required.
Altered source versions must be plainly marked as such, and must not be misrepresented as being the original software.
This notice may not be removed or altered from any source distribution.
/***************************************************************************/ /**
* @file sli_wifi_callback_framework.h
*******************************************************************************
* # License
* <b>Copyright 2025 Silicon Laboratories Inc. www.silabs.com</b>
*******************************************************************************
*
* SPDX-License-Identifier: Zlib
*
* The licensor of this software is Silicon Laboratories Inc.
*
* This software is provided 'as-is', without any express or implied
* warranty. In no event will the authors be held liable for any damages
* arising from the use of this software.
*
* Permission is granted to anyone to use this software for any purpose,
* including commercial applications, and to alter it and redistribute it
* freely, subject to the following restrictions:
*
* 1. The origin of this software must not be misrepresented; you must not
* claim that you wrote the original software. If you use this software
* in a product, an acknowledgment in the product documentation would be
* appreciated but is not required.
* 2. Altered source versions must be plainly marked as such, and must not be
* misrepresented as being the original software.
* 3. This notice may not be removed or altered from any source distribution.
*
******************************************************************************/
#pragma once
#include "sl_wifi_device.h"
/**
* @brief Forward declaration for legacy Wi-Fi event callback function pointer type of @ref sl_wifi_callback_function_t.
*/
typedef sl_status_t (*sl_wifi_callback_function_t)(sl_wifi_event_t event,
void *data,
uint32_t data_length,
void *optional_arg);
/**
* @brief Forward declaration for enhanced Wi-Fi event callback function pointer type (with status code) of @ref sl_wifi_callback_function_v2_t.
*
*/
typedef sl_status_t (*sl_wifi_callback_function_v2_t)(sl_wifi_event_t event,
sl_status_t status_code,
void *data,
uint32_t data_length,
void *optional_arg);
/**
* @struct sli_wifi_callback_entry_t
* @brief Structure representing an internal Wi-Fi callback entry.
*/
typedef struct {
sl_wifi_callback_function_t function; ///< Legacy callback function pointer (deprecated)
sl_wifi_callback_function_v2_t function_v2; ///< Enhanced callback function pointer with status code support
void *arg; ///< User-provided argument passed to the callback function
} sli_wifi_callback_entry_t;
/***************************************************************************/
/**
* @brief
* Retrieve the callback entry for a specified Wi-Fi event group.
*
* @details
* This function returns a pointer to the callback entry associated with the given
* Wi-Fi event group.
*
* @param[in] group
* Wi-Fi event group of type @ref sl_wifi_event_group_t for which to retrieve the callback entry.
* If the group value exceeds SL_WIFI_EVENT_GROUP_COUNT, the function will attempt to
* derive the event group from the event value. The SL_WIFI_EVENT_FAIL_INDICATION bit
* is automatically masked out during processing.
*
* @return
* Pointer to the callback entry of type @ref sli_wifi_callback_entry_t if the group is valid,
* NULL if the group index is out of bounds or invalid.
*
* @note
* The returned pointer points to an entry in the global registered_callbacks array
* and should not be freed by the caller.
******************************************************************************/
sli_wifi_callback_entry_t *sli_get_callback_entry(sl_wifi_event_group_t group);
/***************************************************************************/
/**
* @brief
* Internal function to register a callback for a selected event group. All the individual Wi-Fi events related to specific group would be triggered via this group callback.
*
* This function allows the user to register a callback function for a specific group of Wi-Fi events @ref sl_wifi_event_group_t.
* When any event within the specified group occurs, the registered callback function will be invoked, providing the event details and any associated data.
*
* @param[in] group
* Group ID of the event for which the callback is registered. See @ref sl_wifi_event_group_t for possible values.
* @param[in] function
* Function pointer to callback of type @ref sl_wifi_callback_function_t that would be invoked when an event in the specified group occurs.
* @param[in] function_v2
* Function pointer to callback of type @ref sl_wifi_callback_function_v2_t that would be invoked when an event in the specified group occurs.
* @param[in] optional_arg
* Optional user provided argument to pass additional context or information to the callback function. This would be passed back to callback handler of type @ref sl_wifi_callback_function_t.
* @return
* sl_status_t. See [Status Codes](https://docs.silabs.com/gecko-platform/latest/platform-common/status)
* and [WiSeConnect Status Codes](../wiseconnect-api-reference-guide-err-codes/wiseconnect-status-codes) for details.
* @note
* Callbacks can be set only for event groups defined in @ref sl_wifi_event_group_t, not for individual events defined in @ref sl_wifi_event_t.
******************************************************************************/
sl_status_t sli_wifi_set_callback(sl_wifi_event_group_t group,
sl_wifi_callback_function_t function,
sl_wifi_callback_function_v2_t function_v2,
void *optional_arg);
Modules#
Typedefs#
Forward declaration for legacy Wi-Fi event callback function pointer type of sl_wifi_callback_function_t.
Forward declaration for enhanced Wi-Fi event callback function pointer type (with status code) of sl_wifi_callback_function_v2_t.
Functions#
Retrieve the callback entry for a specified Wi-Fi event group.
Internal function to register a callback for a selected event group.
Typedef Documentation#
sl_wifi_callback_function_t#
typedef sl_status_t(* sl_wifi_callback_function_t) (sl_wifi_event_t event, void *data, uint32_t data_length, void *optional_arg) )(sl_wifi_event_t event, void *data, uint32_t data_length, void *optional_arg)
Forward declaration for legacy Wi-Fi event callback function pointer type of sl_wifi_callback_function_t.
sl_wifi_callback_function_v2_t#
typedef sl_status_t(* sl_wifi_callback_function_v2_t) (sl_wifi_event_t event, sl_status_t status_code, void *data, uint32_t data_length, void *optional_arg) )(sl_wifi_event_t event, sl_status_t status_code, void *data, uint32_t data_length, void *optional_arg)
Forward declaration for enhanced Wi-Fi event callback function pointer type (with status code) of sl_wifi_callback_function_v2_t.
Function Documentation#
sli_get_callback_entry#
sli_wifi_callback_entry_t * sli_get_callback_entry (sl_wifi_event_group_t group)
Retrieve the callback entry for a specified Wi-Fi event group.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_wifi_event_group_t | [in] | group | Wi-Fi event group of type sl_wifi_event_group_t for which to retrieve the callback entry. If the group value exceeds SL_WIFI_EVENT_GROUP_COUNT, the function will attempt to derive the event group from the event value. The SL_WIFI_EVENT_FAIL_INDICATION bit is automatically masked out during processing. |
This function returns a pointer to the callback entry associated with the given Wi-Fi event group.
Returns
Pointer to the callback entry of type sli_wifi_callback_entry_t if the group is valid, NULL if the group index is out of bounds or invalid.
Note
The returned pointer points to an entry in the global registered_callbacks array and should not be freed by the caller.
sli_wifi_set_callback#
sl_status_t sli_wifi_set_callback (sl_wifi_event_group_t group, sl_wifi_callback_function_t function, sl_wifi_callback_function_v2_t function_v2, void * optional_arg)
Internal function to register a callback for a selected event group.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_wifi_event_group_t | [in] | group | Group ID of the event for which the callback is registered. See sl_wifi_event_group_t for possible values. |
| sl_wifi_callback_function_t | [in] | function | Function pointer to callback of type sl_wifi_callback_function_t that would be invoked when an event in the specified group occurs. |
| sl_wifi_callback_function_v2_t | [in] | function_v2 | Function pointer to callback of type sl_wifi_callback_function_v2_t that would be invoked when an event in the specified group occurs. |
| void * | [in] | optional_arg | Optional user provided argument to pass additional context or information to the callback function. This would be passed back to callback handler of type sl_wifi_callback_function_t. |
All the individual Wi-Fi events related to specific group would be triggered via this group callback.
This function allows the user to register a callback function for a specific group of Wi-Fi events sl_wifi_event_group_t. When any event within the specified group occurs, the registered callback function will be invoked, providing the event details and any associated data.
Returns
sl_status_t. See Status Codes and WiSeConnect Status Codes for details.
Note
Callbacks can be set only for event groups defined in sl_wifi_event_group_t, not for individual events defined in sl_wifi_event_t.