Callback Framework#
This section provides a reference to Wi-Fi API callback handling functions.
Note
Stack overflows may occur if you invoke functions or use your own variables or data structures while handling callbacks. Please configure the stack size by modifying the pre-processor macro
SL_SI91X_EVENT_HANDLER_STACK_SIZEas per your application's requirements. See here for the instructions for modifying a pre-processor macro.Event/Callback handlers must not contain function calls or code which can block or delay the execution of the event/callback handler as it causes all the other events to queue up and delay the execution of other events since all the events are invoked and handled from a single thread.
Do not call any synchronous SDK APIs from within the Event/Callback handlers.
Typedefs#
Generic callback for Wi-Fi group events of type sl_wifi_event_group_t.
Callback for SL_WIFI_SCAN_RESULT_EVENTS group event of type sl_wifi_event_group_t.
Callback for SL_WIFI_STATS_RESPONSE_EVENTS group events of type sl_wifi_event_group_t.
Callback for SL_WIFI_JOIN_EVENTS group events of type sl_wifi_event_group_t.
Callback for SL_WIFI_TWT_RESPONSE_EVENTS group events.
Callback for SL_WIFI_TRANSCEIVER_EVENTS group events.
Callback for SL_WIFI_COMMAND_ENGINE_STATUS_EVENTS group events of type sl_wifi_event_group_t.
Generic callback for Wi-Fi group events of type sl_wifi_event_group_t.
Callback for SL_WIFI_SCAN_RESULT_EVENTS group event of type sl_wifi_event_group_t.
Callback for SL_WIFI_STATS_RESPONSE_EVENTS group events of type sl_wifi_event_group_t.
Callback for SL_WIFI_JOIN_EVENTS group events of type sl_wifi_event_group_t.
Callback for SL_WIFI_TWT_RESPONSE_EVENTS group events.
Callback for SL_WIFI_TRANSCEIVER_EVENTS group events.
Functions#
Register a callback for a selected event group.
Register a callback for a selected event group.
Default Wi-Fi event handler to be passed to sl_wifi_init.
Register a callback for the SL_WIFI_SCAN_RESULT_EVENTS group event from sl_wifi_event_group_t.
Register a callback for SL_WIFI_JOIN_EVENTS group event from sl_wifi_event_group_t.
Register a callback for SL_WIFI_TWT_RESPONSE_EVENTS group event from sl_wifi_event_group_t.
Register a callback for SL_WIFI_STATS_RESPONSE_EVENTS group event from sl_wifi_event_group_t.
Register a callback for SL_WIFI_TRANSCEIVER_EVENTS group event of tye sl_wifi_event_group_t.
Register a callback for the SL_WIFI_SCAN_RESULT_EVENTS group event from sl_wifi_event_group_t.
Register a callback for SL_WIFI_JOIN_EVENTS group event from sl_wifi_event_group_t.
Register a callback for SL_WIFI_TWT_RESPONSE_EVENTS group event from sl_wifi_event_group_t.
Register a callback for SL_WIFI_STATS_RESPONSE_EVENTS group event from sl_wifi_event_group_t.
Register a callback for SL_WIFI_TRANSCEIVER_EVENTS group event of tye sl_wifi_event_group_t.
Retrieves the saved thread-specific firmware status value.
Register a callback for SL_WIFI_COMMAND_ENGINE_STATUS_EVENTS group event from sl_wifi_event_group_t.
Macros#
Generic macro for callback functions to check if the event has failed.
Typedef Documentation#
sl_wifi_callback_function_t#
sl_wifi_callback_function_t )(sl_wifi_event_t event, void *data, uint32_t data_length, void *optional_arg)
Generic callback for Wi-Fi group events of type sl_wifi_event_group_t.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| N/A | event | Wi-Fi event of type sl_wifi_event_t. This parameter indicates the specific Wi-Fi event that triggered the callback. | |
| N/A | data | Pointer to the data received. The type and content of this data depend on the specific event. | |
| N/A | data_length | Length of the data received in bytes. | |
| N/A | optional_arg | Optional user-provided argument passed in sl_wifi_set_callback. This parameter allows the user to pass additional context or information to the callback function. |
This typedef defines a callback function that handles Wi-Fi events of type sl_wifi_event_t. The callback is invoked when a Wi-Fi event occurs, providing the event details and any associated data.
Returns
sl_status_t. See Status Codes and WiSeConnect Status Codes for details.
Note
In case of event failure, the
SL_WIFI_FAIL_EVENT_STATUS_INDICATIONbit is set in theeventparameter. When this bit is set, thedataparameter will be of typesl_status_t, and thedata_lengthparameter can be ignored.Moving forward, this API will be deprecated. Instead, use the sl_wifi_callback_function_v2_t API. This is retained for backward compatibility.
sl_wifi_scan_callback_t#
sl_wifi_scan_callback_t )(sl_wifi_event_t event, sl_wifi_scan_result_t *data, uint32_t data_length, void *optional_arg)
Callback for SL_WIFI_SCAN_RESULT_EVENTS group event of type sl_wifi_event_group_t.
| Type | Direction | Argument Name | Description | ||||
|---|---|---|---|---|---|---|---|
| N/A | event | Wi-Fi event of type sl_wifi_event_t. This parameter indicates the specific Wi-Fi event that triggered the callback.
| |||||
| N/A | data | Pointer to the scan results of type sl_wifi_scan_result_t. This parameter provides the scan results obtained from the Wi-Fi scan operation. | |||||
| N/A | data_length | Length of the scan results data received in bytes. | |||||
| N/A | optional_arg | Optional user-provided argument passed in sl_wifi_set_scan_callback. |
This typedef defines a callback function that handles Wi-Fi scan result events of type sl_wifi_event_t. The callback is triggered when a Wi-Fi module tries to scan and receive the response, providing the event details and any associated scan results.
Wi-Fi module must call sl_wifi_start_scan to receive SL_WIFI_SCAN_RESULT_EVENTS event.
Returns
sl_status_t. See Status Codes and WiSeConnect Status Codes for details.
Note
In case of event failure, SL_WIFI_FAIL_EVENT_STATUS_INDICATION bit is set in the event. When this bit is set, the
dataparameter will be of typesl_status_t, and thedata_lengthparameter can be ignored.Moving forward, this API will be deprecated. Instead, use the sl_wifi_scan_callback_v2_t API. This is retained for backward compatibility.
sl_wifi_stats_callback_t#
sl_wifi_stats_callback_t )(sl_wifi_event_t event, void *data, uint32_t data_length, void *optional_arg)
Callback for SL_WIFI_STATS_RESPONSE_EVENTS group events of type sl_wifi_event_group_t.
| Type | Direction | Argument Name | Description | ||||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
| N/A | event | Wi-Fi event of type sl_wifi_event_t that triggered the callback. Individual Wi-Fi events related to SL_WIFI_STATS_RESPONSE_EVENTS is as follows:
| |||||||||||||
| N/A | data | Pointer to the payload received. | |||||||||||||
| N/A | data_length | Length of the payload received in bytes. | |||||||||||||
| N/A | optional_arg | Optional user-provided argument passed in sl_wifi_set_stats_callback. |
This typedef defines a callback function that handles Wi-Fi statistics response events of type sl_wifi_event_t. The callback is invoked when a Wi-Fi statistics response event occurs, providing the event details and any associated data.
Returns
sl_status_t. See Status Codes and WiSeConnect Status Codes for details.
Note
SL_WIFI_STATS_MODULE_STATE_EVENT messages are used to indicate module state to the host. These messages are enabled by setting the 10th bit of the custom feature bitmap in opermode. For the event SL_WIFI_STATS_MODULE_STATE_EVENT response structure refer sl_wifi_module_state_stats_response_t.
state_code of this response (1 byte), indicates the state of the module.
state_codecontains two parts, the upper nibble and lower nibble. The state code is formed by combining the upper and the lower nibbles using a bitwise OR operation, that is, State code = upper nibble | lower nibble For example, if the state code is 82 but is not found in the table, it can be divided as follows: state_code = 80 | 02, where 80 is the upper nibble and 02 is the lower nibble.The upper nibble indicates the state of the rejoin process. The following table documents the possible values of the upper nibble of the state_code.
Module state code
upper nibble
Description
Scan Trigger (State I)
0x00
Startup (Initial state or idle state).
Indicates the reason for the scan
-----------—
-------------------------------------------------------------------------—
triggered.
0x10
Beacon Loss (Failover Roam).
-----------—
-------------------------------------------------------------------------—
0x20
De-authentication from AP.
----------------------------------—
-----------—
-------------------------------------------------------------------------—
Scan Result/Decision (State II)
0x50
Current AP is best.
Indicates a state change based on
-----------—
------------------------------------------------------------------------—
the scan result.
0x60
Better AP found while roaming.
-----------—
-------------------------------------------------------------------------—
0x70
No AP found.
----------------------------------—
-----------—
-------------------------------------------------------------------------—
Final Connection or Join (State III)
0x80
Associated or joined to an Access point.
Indicates the connection state
-----------—
-------------------------------------------------------------------------—
change
0x90
Unassociated(Disconnected from host or join failure).
The lower nibble of state_code indicates the reason for a state change. The table below lists the possible values of the lower nibble of the state_code.
Module state code lower nibble
Description
0x00
No reason specified (Initial state or idle state).
0x01
No response from AP for authentication request(Authentication denial).
0x02
Association denial (Association timeout or Association failure due to unknown reasons).
0x03
User configured AP is not present.
0x05
Four-way Handshake failure.
0x06
Deauthentication from user.
0x07
PSK not configured.
0x08
key-handshake failure during rejoin/roaming/after connection(Disconnection from supplicant).
0x09
Roaming not enabled.
Module reason code
Description
0x00
No reason specified (Initial state or idle state).
0x01
No response from AP for authentication request(Authentication denial).
0x02
Association denial (caused by Association timeout or Association failure due to unknown reasons).
0x03
User configured AP is not present.
0x05
Four-way Handshake failure.
0x06
Deauthentication from user.
0x07
PSK not configured.
0x08
key-handshake failure during rejoin/roaming/after connection(Disconnection from supplicant).
0x09
Roaming not enabled
0x10
Beacon Loss (Failover Roam).
0x20
De-authentication from AP.
0x28
TLS CA Cert not present
0x29
TLS PRIVATE key not present.
0x2A
TLS Client Cert not present.
0x2B
TLS no Cert present.
0x2C
PEAP CA Cert not present.
0x2D
Server Cert Invalid Key Type.
0x2E
Server Intermediate CA Invalid Key Type.
0x2F
Server Root CA Invalid Key Type.
0x30
Client Cert Invalid Key Type.
0x31
Client Root CA Invalid Key Type.
0x37
Server Cert 4096-bit length support is not enabled.
0x38
Server Intermediate CA 4096-bit length support is not enabled.
0x39
Server Root CA 4096-bit length support is not enabled.
0x3A
Client Cert 4096-bit length support is not enabled.
0x3B
Client Root CA 4096-bit length support is not enabled.
0x3C
Server Cert Invalid Sign Alg.
0x3D
Server Intermediate CA Invalid Sign Alg.
0x3E
Server Root CA Invalid Sign Length.
0x3F
Client Cert Invalid Sign Alg.
0x40
Client Root CA Invalid Sign Length.
0x41
Server Intermediate CA not Present.
0x42
Server Root CA Parse Error.
0x43
Server Intermediate Root CA Parse Error.
0x44
Sever Cert Parse Error.
0x45
Client Cert Parse Error.
0x46
Incorrect Private Key Password.
0x47
EAP Failure Received.
0x48
Client Cert Bad Date Error.
0x49
Server Cert Bad Date Error.
0x4A
Server Root CA Bad Date Error.
0x4B
Client Root CA Bad Date Error.
0x4C
Server Intermediate Root CA Bad Date Error.
0x4D
Pem Header Error.
0x4E
Pem Footer Error.
0x4F
Client Intermediate CA Invalid Sign Length.
0x50
Client Intermediate CA Invalid Length.
0x52
Client Intermediate CA invalid Key Type.
0x53
Pem Error.
0x54
Pathlen certificate is Invalid.
In addition to the above, the reason code received in the Deauthentication/Disassociation frame from the AP is modified by setting the Most Significant Bit (MSB) of the reason code. If the MSB is set in the reason code, it should be masked with 0x7F to extract the actual reason code received in the Deauthentication/Disassociation frame. Refer to the "Reason Codes Table" section in the IEEE 802.11 standard to learn about the de-authentication or disassociation reason codes. Pem Header Error (0x4D) and Pem Footer Error (0x4E) apply only when certificates are loaded individually. If certificates are loaded together in a single file, only the Pem Error (0x53) triggers for any header or footer errors. In case of event failure, the
SL_WIFI_FAIL_EVENT_STATUS_INDICATIONbit is set in theeventparameter. When this bit is set, thedataparameter will be of typesl_status_t, and thedata_lengthparameter can be ignored.Moving forward, this API will be deprecated. Instead, use the sl_wifi_stats_callback_v2_t API. This is retained for backward compatibility.
sl_wifi_join_callback_t#
sl_wifi_join_callback_t )(sl_wifi_event_t event, char *data, uint32_t data_length, void *optional_arg)
Callback for SL_WIFI_JOIN_EVENTS group events of type sl_wifi_event_group_t.
| Type | Direction | Argument Name | Description | ||||||
|---|---|---|---|---|---|---|---|---|---|
| N/A | event | Wi-Fi event of type sl_wifi_event_t that triggered the callback. | |||||||
| N/A | data | Pointer to the response data received (1 byte). The possible values and their descriptions are as follows:
| |||||||
| N/A | data_length | Length of the data received in bytes. This parameter indicates the size of the data buffer pointed to by the | |||||||
| N/A | optional_arg | Optional user-provided argument passed in sl_wifi_set_join_callback. |
This typedef defines a callback function that handles Wi-Fi join events of type sl_wifi_event_t. The callback is invoked when a Wi-Fi join event occurs, providing the event details and any associated data.
Returns
sl_status_t. See Status Codes and WiSeConnect Status Codes for details.
Note
This is valid in WiFi client mode only
In case of event failure, the
SL_WIFI_FAIL_EVENT_STATUS_INDICATIONbit is set in theeventparameter. When this bit is set, thedataparameter will be of typesl_status_t, and thedata_lengthparameter can be ignored.Moving forward, this API will be deprecated. Instead, use the sl_wifi_join_callback_v2_t API. This is retained for backward compatibility.
sl_wifi_twt_config_callback_t#
sl_wifi_twt_config_callback_t )(sl_wifi_event_t event, sl_wifi_twt_response_t *data, uint32_t data_length, void *optional_arg)
Callback for SL_WIFI_TWT_RESPONSE_EVENTS group events.
| Type | Direction | Argument Name | Description | ||||||||||||||||||||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
| N/A | event | Wi-Fi event of type sl_wifi_event_t that triggered the callback. Individual Wi-Fi events related to SL_WIFI_TWT_RESPONSE_EVENTS is as follows:
| |||||||||||||||||||||||||||||
| N/A | data | Pointer to the data received of type sl_wifi_twt_response_t. This parameter provides detailed information about the TWT response event. The structure contains various fields that describe the TWT session parameters and status. | |||||||||||||||||||||||||||||
| N/A | data_length | Length of the data received in bytes. | |||||||||||||||||||||||||||||
| N/A | optional_arg | Optional user-provided argument passed in sl_wifi_set_twt_config_callback. |
This typedef defines a callback function that handles Wi-Fi Target Wake Time (TWT) configuration response events. The callback is invoked when a TWT response event occurs, providing the event details and any associated data.
Returns
sl_status_t. See Status Codes and WiSeConnect Status Codes for details.
Note
In case of event failure, the
SL_WIFI_FAIL_EVENT_STATUS_INDICATIONbit is set in theeventparameter. When this bit is set, thedataparameter will be of typesl_status_t, and thedata_lengthparameter can be ignored.Moving forward, this API will be deprecated. Instead, use the sl_wifi_twt_config_callback_v2_t API. This is retained for backward compatibility.
sl_wifi_transceiver_callback_t#
sl_wifi_transceiver_callback_t )(sl_wifi_event_t event, void *data, uint32_t data_length, void *optional_arg)
Callback for SL_WIFI_TRANSCEIVER_EVENTS group events.
| Type | Direction | Argument Name | Description | ||||||
|---|---|---|---|---|---|---|---|---|---|
| [out] | event | Wi-Fi event of type sl_wifi_event_t. This parameter indicates the specific Wi-Fi event that triggered the callback. Individual Wi-Fi events related to SL_WIFI_TRANSCEIVER_EVENTS are as follows:
| |||||||
| [out] | data |
| |||||||
| [out] | data_length | Reserved. | |||||||
| [out] | optional_arg | Optional user-provided argument passed in sl_wifi_set_transceiver_callback |
This typedef defines a callback function that handles Wi-Fi transceiver events. The callback is invoked when a transceiver event occurs, providing the event details and any associated data.
Returns
sl_status_t. See Status Codes and WiSeConnect Status Codes for details.
Note
This API is only supported in Wi-Fi Transceiver opermode (7).
In case of event failure, the
SL_WIFI_FAIL_EVENT_STATUS_INDICATIONbit is set in theeventparameter. When this bit is set, thedataparameter will be of typesl_status_t, and thedata_lengthparameter can be ignored.Moving forward, this API will be deprecated. Instead, use the sl_wifi_transceiver_callback_v2_t API. This is retained for backward compatibility.
sl_wifi_command_engine_status_callback_t#
sl_wifi_command_engine_status_callback_t )(sl_wifi_event_t event, sl_status_t status_code, void *data, uint32_t data_length, void *optional_arg)
Callback for SL_WIFI_COMMAND_ENGINE_STATUS_EVENTS group events of type sl_wifi_event_group_t.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| N/A | event | Wi-Fi event of type sl_wifi_event_t that triggered the callback. | |
| N/A | status_code | Status code of type sl_status_t. This parameter always indicates a failure event and contains the failure status code. See Status Codes and WiSeConnect Status Codes for details. | |
| N/A | data | Unused parameter. Reserved for future use. | |
| N/A | data_length | Unused parameter. Reserved for future use. | |
| N/A | optional_arg | Optional user-provided argument passed in sl_wifi_set_command_engine_status_handler. |
This typedef defines a callback function that handles command engine status events of type sl_wifi_event_t. The callback is invoked when a command engine status event occurs, providing the status details.
Returns
sl_status_t. See Status Codes and Additional Status Codes for details.
Note
The
dataanddata_lengthparameters are currently unused and should be ignored by the callback implementation.
sl_wifi_callback_function_v2_t#
sl_wifi_callback_function_v2_t )(sl_wifi_event_t event, sl_status_t status_code, void *data, uint32_t data_length, void *optional_arg)
Generic callback for Wi-Fi group events of type sl_wifi_event_group_t.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| N/A | event | Wi-Fi event of type sl_wifi_event_t. This parameter indicates the specific Wi-Fi event that triggered the callback. | |
| N/A | status_code | Status code of type sl_status_t. On success/regular events always indicates SL_STATUS_OK, on failure events indicates the status code of failure. See Status Codes and WiSeConnect Status Codes for details. | |
| N/A | data | Pointer to the data received. The type and content of this data depend on the specific event. | |
| N/A | data_length | Length of the data received in bytes. | |
| N/A | optional_arg | Optional user-provided argument passed in sl_wifi_set_callback_v2. This parameter allows the user to pass additional context or information to the callback function. |
This typedef defines a callback function that handles Wi-Fi events of type sl_wifi_event_t. The callback is invoked when a Wi-Fi event occurs, providing the event details, status code and any associated data.
Returns
sl_status_t. See Status Codes and WiSeConnect Status Codes for details.
Note
In case of event failure, the
SL_WIFI_FAIL_EVENT_STATUS_INDICATIONbit is set in theeventparameter. When this bit is set, thedataand thedata_lengthparameter can be ignored.
sl_wifi_scan_callback_v2_t#
sl_wifi_scan_callback_v2_t )(sl_wifi_event_t event, sl_status_t status_code, sl_wifi_scan_result_t *data, uint32_t data_length, void *optional_arg)
Callback for SL_WIFI_SCAN_RESULT_EVENTS group event of type sl_wifi_event_group_t.
| Type | Direction | Argument Name | Description | ||||
|---|---|---|---|---|---|---|---|
| N/A | event | Wi-Fi event of type sl_wifi_event_t. This parameter indicates the specific Wi-Fi event that triggered the callback.
| |||||
| N/A | status_code | Status code of type sl_status_t. On successful scan event always indicates SL_STATUS_OK, on failure indicates the status code of failure. See Status Codes and WiSeConnect Status Codes for details. | |||||
| N/A | data | Pointer to the scan results of type sl_wifi_scan_result_t. This parameter provides the scan results obtained from the Wi-Fi scan operation. | |||||
| N/A | data_length | Length of the scan results data received in bytes. | |||||
| N/A | optional_arg | Optional user-provided argument passed in sl_wifi_set_scan_callback_v2. |
This typedef defines a callback function that handles Wi-Fi scan result events of type sl_wifi_event_t. The callback is triggered when a Wi-Fi module tries to scan and receive the response, providing the event details and any associated scan results.
Wi-Fi module must call sl_wifi_start_scan to receive SL_WIFI_SCAN_RESULT_EVENTS event.
Returns
sl_status_t. See Status Codes and WiSeConnect Status Codes for details.
Note
In case of event failure, SL_WIFI_FAIL_EVENT_STATUS_INDICATION bit is set in the event. When this bit is set, the
dataparameter and thedata_lengthparameter can be ignored. In the case of SL_WIFI_SCAN_TYPE_EXTENDED, the scan callback is invoked with data set to NULL and data_length indicating the total size of the scan results (that is, scan count * sizeof(sl_wifi_extended_scan_result_t)). Upon receiving this callback, the application must allocate a buffer of size data_length and explicitly call the sl_wifi_get_stored_scan_results() API, passing the allocated buffer to retrieve the complete scan results.
sl_wifi_stats_callback_v2_t#
sl_wifi_stats_callback_v2_t )(sl_wifi_event_t event, sl_status_t status_code, void *data, uint32_t data_length, void *optional_arg)
Callback for SL_WIFI_STATS_RESPONSE_EVENTS group events of type sl_wifi_event_group_t.
| Type | Direction | Argument Name | Description | ||||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
| N/A | event | Wi-Fi event of type sl_wifi_event_t that triggered the callback. Individual Wi-Fi events related to SL_WIFI_STATS_RESPONSE_EVENTS is as follows:
| |||||||||||||
| N/A | status_code | Status code of type sl_status_t. On successful events always indicates SL_STATUS_OK, on failure events indicates the status code of failure. See Status Codes and WiSeConnect Status Codes for details. | |||||||||||||
| N/A | data | Pointer to the payload received. | |||||||||||||
| N/A | data_length | Length of the payload received in bytes. | |||||||||||||
| N/A | optional_arg | Optional user-provided argument passed in sl_wifi_set_stats_callback_v2. |
This typedef defines a callback function that handles Wi-Fi statistics response events of type sl_wifi_event_t. The callback is invoked when a Wi-Fi statistics response event occurs, providing the event details and any associated data.
Returns
sl_status_t. See Status Codes and WiSeConnect Status Codes for details.
Note
SL_WIFI_STATS_MODULE_STATE_EVENT messages are used to indicate module state to the host. These messages are enabled by setting the 10th bit of the custom feature bitmap in opermode. For the event SL_WIFI_STATS_MODULE_STATE_EVENT response structure refer sl_wifi_module_state_stats_response_t.
state_code of this response (1 byte), indicates the state of the module.
state_codecontains two parts, the upper nibble and lower nibble. The state code is formed by combining the upper and the lower nibbles using a bitwise OR operation, that is, State code = upper nibble | lower nibble For example, if the state code is 82 but is not found in the table, it can be divided as follows: state_code = 80 | 02, where 80 is the upper nibble and 02 is the lower nibble.The upper nibble indicates the state of the rejoin process. The following table documents the possible values of the upper nibble of the state_code.
Module state code
upper nibble
Description
Scan Trigger (State I)
0x00
Startup (Initial state or idle state).
Indicates the reason for the scan
-----------—
-------------------------------------------------------------------------—
triggered.
0x10
Beacon Loss (Failover Roam).
-----------—
-------------------------------------------------------------------------—
0x20
De-authentication from AP.
----------------------------------—
-----------—
-------------------------------------------------------------------------—
Scan Result/Decision (State II)
0x50
Current AP is best.
Indicates a state change based on
-----------—
------------------------------------------------------------------------—
the scan result.
0x60
Better AP found while roaming.
-----------—
-------------------------------------------------------------------------—
0x70
No AP found.
----------------------------------—
-----------—
-------------------------------------------------------------------------—
Final Connection or Join (State III)
0x80
Associated or joined to an Access point.
Indicates the connection state
-----------—
-------------------------------------------------------------------------—
change
0x90
Unassociated(Disconnected from host or join failure).
The lower nibble of state_code indicates the reason for a state change. The table below lists the possible values of the lower nibble of the state_code.
Module state code lower nibble
Description
0x00
No reason specified (Initial state or idle state).
0x01
No response from AP for authentication request(Authentication denial).
0x02
Association denial (Association timeout or Association failure due to unknown reasons).
0x03
User configured AP is not present.
0x05
Four-way Handshake failure.
0x06
Deauthentication from user.
0x07
PSK not configured.
0x08
key-handshake failure during rejoin/roaming/after connection(Disconnection from supplicant).
0x09
Roaming not enabled.
Module reason code
Description
0x00
No reason specified (Initial state or idle state).
0x01
No response from AP for authentication request(Authentication denial).
0x02
Association denial (caused by Association timeout or Association failure due to unknown reasons).
0x03
User configured AP is not present.
0x05
Four-way Handshake failure.
0x06
Deauthentication from user.
0x07
PSK not configured.
0x08
key-handshake failure during rejoin/roaming/after connection(Disconnection from supplicant).
0x09
Roaming not enabled
0x10
Beacon Loss (Failover Roam).
0x20
De-authentication from AP.
0x28
TLS CA Cert not present
0x29
TLS PRIVATE key not present.
0x2A
TLS Client Cert not present.
0x2B
TLS no Cert present.
0x2C
PEAP CA Cert not present.
0x2D
Server Cert Invalid Key Type.
0x2E
Server Intermediate CA Invalid Key Type.
0x2F
Server Root CA Invalid Key Type.
0x30
Client Cert Invalid Key Type.
0x31
Client Root CA Invalid Key Type.
0x37
Server Cert 4096-bit length support is not enabled.
0x38
Server Intermediate CA 4096-bit length support is not enabled.
0x39
Server Root CA 4096-bit length support is not enabled.
0x3A
Client Cert 4096-bit length support is not enabled.
0x3B
Client Root CA 4096-bit length support is not enabled.
0x3C
Server Cert Invalid Sign Alg.
0x3D
Server Intermediate CA Invalid Sign Alg.
0x3E
Server Root CA Invalid Sign Length.
0x3F
Client Cert Invalid Sign Alg.
0x40
Client Root CA Invalid Sign Length.
0x41
Server Intermediate CA not Present.
0x42
Server Root CA Parse Error.
0x43
Server Intermediate Root CA Parse Error.
0x44
Sever Cert Parse Error.
0x45
Client Cert Parse Error.
0x46
Incorrect Private Key Password.
0x47
EAP Failure Received.
0x48
Client Cert Bad Date Error.
0x49
Server Cert Bad Date Error.
0x4A
Server Root CA Bad Date Error.
0x4B
Client Root CA Bad Date Error.
0x4C
Server Intermediate Root CA Bad Date Error.
0x4D
Pem Header Error.
0x4E
Pem Footer Error.
0x4F
Client Intermediate CA Invalid Sign Length.
0x50
Client Intermediate CA Invalid Length.
0x52
Client Intermediate CA invalid Key Type.
0x53
Pem Error.
0x54
Pathlen certificate is Invalid.
In addition to the above, the reason code received in the Deauthentication/Disassociation frame from the AP is modified by setting the Most Significant Bit (MSB) of the reason code.If the MSB is set in the reason code, it should be masked with 0x7F to extract the actual reason code received in the Deauthentication/Disassociation frame. Please refer to the "Reason Codes Table" section in the IEEE 802.11 standard to learn about the de-authentication or disassociation reason codes. Pem Header Error (0x4D) and Pem Footer Error (0x4E) apply only when certificates are loaded individually. If certificates are loaded together in a single file, only the Pem Error (0x53) triggers for any header or footer errors. In case of event failure, the
SL_WIFI_FAIL_EVENT_STATUS_INDICATIONbit is set in theeventparameter. When this bit is set, thedataparameter and thedata_lengthparameter can be ignored.
sl_wifi_join_callback_v2_t#
sl_wifi_join_callback_v2_t )(sl_wifi_event_t event, sl_status_t status_code, char *data, uint32_t data_length, void *optional_arg)
Callback for SL_WIFI_JOIN_EVENTS group events of type sl_wifi_event_group_t.
| Type | Direction | Argument Name | Description | ||||||
|---|---|---|---|---|---|---|---|---|---|
| N/A | event | Wi-Fi event of type sl_wifi_event_t that triggered the callback. | |||||||
| N/A | status_code | Status code of type sl_status_t. On successful events always indicates SL_STATUS_OK, on failure events indicates the status code of failure. See Status Codes and WiSeConnect Status Codes for details. | |||||||
| N/A | data | Pointer to the response data received (1 byte). The possible values and their descriptions are as follows:
| |||||||
| N/A | data_length | Length of the data received in bytes. This parameter indicates the size of the data buffer pointed to by the | |||||||
| N/A | optional_arg | Optional user-provided argument passed in sl_wifi_set_join_callback_v2. |
This typedef defines a callback function that handles Wi-Fi join events of type sl_wifi_event_t. The callback is invoked when a Wi-Fi join event occurs, providing the event details and any associated data.
Returns
sl_status_t. See Status Codes and WiSeConnect Status Codes for details.
Note
This is valid in WiFi client mode only
In case of event failure, the
SL_WIFI_FAIL_EVENT_STATUS_INDICATIONbit is set in theeventparameter. When this bit is set, thedataparameter and thedata_lengthparameter can be ignored.
sl_wifi_twt_config_callback_v2_t#
sl_wifi_twt_config_callback_v2_t )(sl_wifi_event_t event, sl_status_t status_code, sl_wifi_twt_response_t *data, uint32_t data_length, void *optional_arg)
Callback for SL_WIFI_TWT_RESPONSE_EVENTS group events.
| Type | Direction | Argument Name | Description | ||||||||||||||||||||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
| N/A | event | Wi-Fi event of type sl_wifi_event_t that triggered the callback. Individual Wi-Fi events related to SL_WIFI_TWT_RESPONSE_EVENTS is as follows:
| |||||||||||||||||||||||||||||
| N/A | status_code | Status code of type sl_status_t. On successful events always indicates SL_STATUS_OK, on failure events indicates the status code of failure. See Status Codes and WiSeConnect Status Codes for details. | |||||||||||||||||||||||||||||
| N/A | data | Pointer to the data received of type sl_wifi_twt_response_t. This parameter provides detailed information about the TWT response event. The structure contains various fields that describe the TWT session parameters and status. | |||||||||||||||||||||||||||||
| N/A | data_length | Length of the data received in bytes. | |||||||||||||||||||||||||||||
| N/A | optional_arg | Optional user-provided argument passed in sl_wifi_set_twt_config_callback_v2. |
This typedef defines a callback function that handles Wi-Fi Target Wake Time (TWT) configuration response events. The callback is invoked when a TWT response event occurs, providing the event details and any associated data.
Returns
sl_status_t. See Status Codes and WiSeConnect Status Codes for details.
Note
In case of event failure, the
SL_WIFI_FAIL_EVENT_STATUS_INDICATIONbit is set in theeventparameter. When this bit is set, thedataparameter and thedata_lengthparameter can be ignored.
sl_wifi_transceiver_callback_v2_t#
sl_wifi_transceiver_callback_v2_t )(sl_wifi_event_t event, sl_status_t status_code, void *data, uint32_t data_length, void *optional_arg)
Callback for SL_WIFI_TRANSCEIVER_EVENTS group events.
| Type | Direction | Argument Name | Description | ||||||
|---|---|---|---|---|---|---|---|---|---|
| [out] | event | Wi-Fi event of type sl_wifi_event_t. This parameter indicates the specific Wi-Fi event that triggered the callback. Individual Wi-Fi events related to SL_WIFI_TRANSCEIVER_EVENTS are as follows:
| |||||||
| N/A | status_code | Status code of type sl_status_t. On successful events always indicates SL_STATUS_OK, on failure events indicates the status code of failure. See Status Codes and WiSeConnect Status Codes for details. | |||||||
| [out] | data |
| |||||||
| [out] | data_length | Reserved. | |||||||
| [out] | optional_arg | Optional user-provided argument passed in sl_wifi_set_transceiver_callback_v2 |
This typedef defines a callback function that handles Wi-Fi transceiver events. The callback is invoked when a transceiver event occurs, providing the event details and any associated data.
Returns
sl_status_t. See Status Codes and WiSeConnect Status Codes for details.
Note
This API is only supported in Wi-Fi Transceiver opermode (7).
In case of event failure, the
SL_WIFI_FAIL_EVENT_STATUS_INDICATIONbit is set in theeventparameter. When this bit is set, thedataparameter and thedata_lengthparameter can be ignored.
Function Documentation#
sl_wifi_set_callback#
sl_status_t sl_wifi_set_callback (sl_wifi_event_group_t group, sl_wifi_callback_function_t function, void * optional_arg)
Register a callback for a selected event group.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_wifi_event_group_t | [in] | group | Group ID of the event for which the callback is registered. See sl_wifi_event_group_t for possible values. |
| sl_wifi_callback_function_t | [in] | function | Function pointer to callback of type sl_wifi_callback_function_t that would be invoked when an event in the specified group occurs. |
| void * | [in] | optional_arg | Optional user-provided argument to pass additional context or information to the callback function. This would be passed back to callback handler of type sl_wifi_callback_function_t. |
All the individual Wi-Fi events related to specific group would be triggered via this group callback.
This function allows the user to register a callback function for a specific group of Wi-Fi events sl_wifi_event_group_t. When any event within the specified group occurs, the registered callback function will be invoked, providing the event details and any associated data.
Pre-conditions:
The Wi-Fi module must be initialized by calling sl_wifi_init before this API can be used.
Returns
sl_status_t. See Status Codes and WiSeConnect Status Codes for details.
Note
Callbacks can be set only for event groups defined in sl_wifi_event_group_t, not for individual events defined in sl_wifi_event_t.
Moving forward, this API will be deprecated. Instead, use the sl_wifi_set_callback_v2 API. This is retained for backward compatibility.
sl_wifi_set_callback_v2#
sl_status_t sl_wifi_set_callback_v2 (sl_wifi_event_group_t group, sl_wifi_callback_function_v2_t function, void * optional_arg)
Register a callback for a selected event group.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_wifi_event_group_t | [in] | group | Group ID of the event for which the callback is registered. See sl_wifi_event_group_t for possible values. |
| sl_wifi_callback_function_v2_t | [in] | function | Function pointer to callback of type sl_wifi_callback_function_v2_t that would be invoked when an event in the specified group occurs. |
| void * | [in] | optional_arg | Optional user-provided argument to pass additional context or information to the callback function. This would be passed back to callback handler of type sl_wifi_callback_function_v2_t. |
All the individual Wi-Fi events related to specific group would be triggered via this group callback.
This function allows the user to register a callback function for a specific group of Wi-Fi events sl_wifi_event_group_t. When any event within the specified group occurs, the registered callback function will be invoked, providing the event details and any associated data.
Pre-conditions:
The Wi-Fi module must be initialized by calling sl_wifi_init before this API can be used.
Returns
sl_status_t. See Status Codes and WiSeConnect Status Codes for details.
Note
Callbacks can be set only for event groups defined in sl_wifi_event_group_t, not for individual events defined in sl_wifi_event_t.
sl_wifi_default_event_handler#
sl_status_t sl_wifi_default_event_handler (sl_wifi_event_t event, sl_wifi_buffer_t * buffer)
Default Wi-Fi event handler to be passed to sl_wifi_init.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_wifi_event_t | [in] | event | Wi-Fi event of type of sl_wifi_event_t. |
| sl_wifi_buffer_t * | [in] | buffer | Buffer containing raw data from NWP firmware |
This event handler would dispatch all the Wi-Fi events and invoke respective Wi-Fi group event.
This function serves as the default event handler for Wi-Fi events. When passed to the sl_wifi_init function, it would handle incoming Wi-Fi events by dispatching them to the appropriate group event functions.
Returns
sl_status_t. See Status Codes and WiSeConnect Status Codes for details.
Note
Passing the event handler is optional. User can implement their own event dispatching handler if they prefer.
sl_wifi_set_scan_callback#
static sl_status_t sl_wifi_set_scan_callback (sl_wifi_scan_callback_t function, void * optional_arg)
Register a callback for the SL_WIFI_SCAN_RESULT_EVENTS group event from sl_wifi_event_group_t.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_wifi_scan_callback_t | [in] | function | Callback function to register. This parameter specifies the callback function of type sl_wifi_scan_callback_t that would be invoked when an event in the SL_WIFI_SCAN_RESULT_EVENTS group occurs. |
| void * | [in] | optional_arg | Optional user-provided argument. This would be passed back to callback handler of type sl_wifi_scan_callback_t. |
This function allows the user to register a callback function for the SL_WIFI_SCAN_RESULT_EVENTS group. When any event within this group occurs, the registered callback function would be invoked, providing the event details and any associated data.
Pre-conditions:
sl_wifi_init should be called before this API.
Returns
sl_status_t. See Status Codes and WiSeConnect Status Codes for details.
Note
All the individual Wi-Fi events related to this group would be triggered via this callback.
Moving forward, this API will be deprecated. Instead, use the sl_wifi_set_scan_callback_v2 API. This is retained for backward compatibility.
sl_wifi_set_join_callback#
static sl_status_t sl_wifi_set_join_callback (sl_wifi_join_callback_t function, void * optional_arg)
Register a callback for SL_WIFI_JOIN_EVENTS group event from sl_wifi_event_group_t.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_wifi_join_callback_t | [in] | function | Function pointer to callback of type sl_wifi_join_callback_t. This parameter specifies the callback function that would be invoked when an event in the SL_WIFI_JOIN_EVENTS group occurs. |
| void * | [in] | optional_arg | Optional user-provided argument. This parameter allows the user to pass additional context or information to the callback function. This would be passed back to callback handler of type sl_wifi_twt_config_callback_t. |
This function allows the user to register a callback function for the SL_WIFI_JOIN_EVENTS group. When any event within this group occurs, the registered callback function would be invoked, providing the event details and any associated data.
Pre-conditions: sl_wifi_init should be called before this API.
Returns
sl_status_t. See Status Codes and WiSeConnect Status Codes for details.
Note
All the individual Wi-Fi events related to this group will be triggered via this callback.
Moving forward, this API will be deprecated. Instead, use the sl_wifi_set_join_callback_v2 API. This is retained for backward compatibility.
sl_wifi_set_twt_config_callback#
static sl_status_t sl_wifi_set_twt_config_callback (sl_wifi_twt_config_callback_t function, void * optional_arg)
Register a callback for SL_WIFI_TWT_RESPONSE_EVENTS group event from sl_wifi_event_group_t.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_wifi_twt_config_callback_t | [in] | function | Function pointer to the callback of type sl_wifi_twt_config_callback_t. This parameter specifies the callback function that would be invoked when an event in the SL_WIFI_TWT_RESPONSE_EVENTS group occurs. |
| void * | [in] | optional_arg | Optional user-provided argument. This would be passed back to callback handler. |
This function allows the user to register a callback function for the SL_WIFI_TWT_RESPONSE_EVENTS group. When any event within this group occurs, the registered callback function will be invoked, providing the event details and any associated data.
Pre-conditions: sl_wifi_init should be called before this API.
Returns
sl_status_t. See Status Codes and WiSeConnect Status Codes for details.
Note
All the individual Wi-Fi events related to this group would be triggered via this callback.
Moving forward, this API will be deprecated. Instead, use the sl_wifi_set_twt_config_callback_v2 API. This is retained for backward compatibility.
sl_wifi_set_stats_callback#
static sl_status_t sl_wifi_set_stats_callback (sl_wifi_stats_callback_t function, void * optional_arg)
Register a callback for SL_WIFI_STATS_RESPONSE_EVENTS group event from sl_wifi_event_group_t.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_wifi_stats_callback_t | [in] | function | Function pointer to the callback of type sl_wifi_stats_callback_t. This parameter specifies the callback function that would be invoked when an event in the SL_WIFI_STATS_RESPONSE_EVENTS group occurs. |
| void * | [in] | optional_arg | Optional user-provided argument. This parameter allows the user to pass additional context or information to the callback function. This would be passed back to callback handler. |
This function allows the user to register a callback function for the SL_WIFI_STATS_RESPONSE_EVENTS group. When any event within this group occurs, the registered callback function would be invoked, providing the event details and any associated data.
Pre-conditions: sl_wifi_init should be called before this API.
Returns
sl_status_t. See Status Codes and WiSeConnect Status Codes for details.
Note
All the individual Wi-Fi events related to this group would be triggered via this callback.
Moving forward, this API will be deprecated. Instead, use the sl_wifi_set_stats_callback_v2 API. This is retained for backward compatibility.
sl_wifi_set_transceiver_callback#
static sl_status_t sl_wifi_set_transceiver_callback (sl_wifi_transceiver_callback_t function, void * optional_arg)
Register a callback for SL_WIFI_TRANSCEIVER_EVENTS group event of tye sl_wifi_event_group_t.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_wifi_transceiver_callback_t | [in] | function | Function pointer to the callback of type sl_wifi_transceiver_callback_t. This parameter specifies the callback function that would be invoked when an event in the SL_WIFI_TRANSCEIVER_EVENTS group occurs. |
| void * | [in] | optional_arg | Optional user-provided argument. This parameter allows the user to pass additional context or information to the callback function. This would be passed back to callback handler. |
This function allows the user to register a callback function for the SL_WIFI_TRANSCEIVER_EVENTS group. When any event within this group occurs, the registered callback function would be invoked, providing the event details and any associated data.
Pre-conditions:
sl_wifi_init should be called before this API.
Returns
sl_status_t. See Status Codes and WiSeConnect Status Codes for details.
Note
All the individual Wi-Fi events related to this group will be triggered via this callback.
Moving forward, this API will be deprecated. Instead, use the sl_wifi_set_transceiver_callback_v2 API. This is retained for backward compatibility.
sl_wifi_set_scan_callback_v2#
static sl_status_t sl_wifi_set_scan_callback_v2 (sl_wifi_scan_callback_v2_t function, void * optional_arg)
Register a callback for the SL_WIFI_SCAN_RESULT_EVENTS group event from sl_wifi_event_group_t.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_wifi_scan_callback_v2_t | [in] | function | Callback function to register. This parameter specifies the callback function of type sl_wifi_scan_callback_v2_t that would be invoked when an event in the SL_WIFI_SCAN_RESULT_EVENTS group occurs. |
| void * | [in] | optional_arg | Optional user-provided argument. This would be passed back to callback handler of type sl_wifi_scan_callback_v2_t. |
This function allows the user to register a callback function for the SL_WIFI_SCAN_RESULT_EVENTS group. When any event within this group occurs, the registered callback function would be invoked, providing the event details and any associated data or failure code.
Pre-conditions:
sl_wifi_init should be called before this API.
Returns
sl_status_t. See Status Codes and WiSeConnect Status Codes for details.
Note
All the individual Wi-Fi events related to this group would be triggered via this callback.
sl_wifi_set_join_callback_v2#
static sl_status_t sl_wifi_set_join_callback_v2 (sl_wifi_join_callback_v2_t function, void * optional_arg)
Register a callback for SL_WIFI_JOIN_EVENTS group event from sl_wifi_event_group_t.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_wifi_join_callback_v2_t | [in] | function | Function pointer to callback of type sl_wifi_join_callback_v2_t. This parameter specifies the callback function that would be invoked when an event in the SL_WIFI_JOIN_EVENTS group occurs. |
| void * | [in] | optional_arg | Optional user-provided argument. This parameter allows the user to pass additional context or information to the callback function. This would be passed back to callback handler of type sl_wifi_join_callback_v2_t. |
This function allows the user to register a callback function for the SL_WIFI_JOIN_EVENTS group. When any event within this group occurs, the registered callback function would be invoked, providing the event details and any associated data or failure code.
Pre-conditions: sl_wifi_init should be called before this API.
Returns
sl_status_t. See Status Codes and WiSeConnect Status Codes for details.
Note
All the individual Wi-Fi events related to this group will be triggered via this callback.
sl_wifi_set_twt_config_callback_v2#
static sl_status_t sl_wifi_set_twt_config_callback_v2 (sl_wifi_twt_config_callback_v2_t function, void * optional_arg)
Register a callback for SL_WIFI_TWT_RESPONSE_EVENTS group event from sl_wifi_event_group_t.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_wifi_twt_config_callback_v2_t | [in] | function | Function pointer to the callback of type sl_wifi_twt_config_callback_v2_t. This parameter specifies the callback function that would be invoked when an event in the SL_WIFI_TWT_RESPONSE_EVENTS group occurs. |
| void * | [in] | optional_arg | Optional user-provided argument. This would be passed back to callback handler. |
This function allows the user to register a callback function for the SL_WIFI_TWT_RESPONSE_EVENTS group. When any event within this group occurs, the registered callback function will be invoked, providing the event details and any associated data or failure code.
Pre-conditions: sl_wifi_init should be called before this API.
Returns
sl_status_t. See Status Codes and WiSeConnect Status Codes for details.
Note
All the individual Wi-Fi events related to this group would be triggered via this callback.
sl_wifi_set_stats_callback_v2#
static sl_status_t sl_wifi_set_stats_callback_v2 (sl_wifi_stats_callback_v2_t function, void * optional_arg)
Register a callback for SL_WIFI_STATS_RESPONSE_EVENTS group event from sl_wifi_event_group_t.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_wifi_stats_callback_v2_t | [in] | function | Function pointer to the callback of type sl_wifi_stats_callback_v2_t. This parameter specifies the callback function that would be invoked when an event in the SL_WIFI_STATS_RESPONSE_EVENTS group occurs. |
| void * | [in] | optional_arg | Optional user-provided argument. This parameter allows the user to pass additional context or information to the callback function. This would be passed back to callback handler. |
This function allows the user to register a callback function for the SL_WIFI_STATS_RESPONSE_EVENTS group. When any event within this group occurs, the registered callback function would be invoked, providing the event details and any associated data or failure code.
Pre-conditions: sl_wifi_init should be called before this API.
Returns
sl_status_t. See Status Codes and WiSeConnect Status Codes for details.
Note
All the individual Wi-Fi events related to this group would be triggered via this callback.
sl_wifi_set_transceiver_callback_v2#
static sl_status_t sl_wifi_set_transceiver_callback_v2 (sl_wifi_transceiver_callback_v2_t function, void * optional_arg)
Register a callback for SL_WIFI_TRANSCEIVER_EVENTS group event of tye sl_wifi_event_group_t.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_wifi_transceiver_callback_v2_t | [in] | function | Function pointer to the callback of type sl_wifi_transceiver_callback_v2_t. This parameter specifies the callback function that would be invoked when an event in the SL_WIFI_TRANSCEIVER_EVENTS group occurs. |
| void * | [in] | optional_arg | Optional user-provided argument. This parameter allows the user to pass additional context or information to the callback function. This would be passed back to callback handler. |
This function allows the user to register a callback function for the SL_WIFI_TRANSCEIVER_EVENTS group. When any event within this group occurs, the registered callback function would be invoked, providing the event details and any associated data or failure code.
Pre-conditions:
sl_wifi_init should be called before this API.
Returns
sl_status_t. See Status Codes and WiSeConnect Status Codes for details.
Note
All the individual Wi-Fi events related to this group will be triggered via this callback.
sl_wifi_get_saved_firmware_status#
static sl_status_t sl_wifi_get_saved_firmware_status (void )
Retrieves the saved thread-specific firmware status value.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
This function fetches the firmware status value that is specific to the current thread.
Returns
sl_status_t. See Status Codes and WiSeConnect Status Codes for details.
sl_wifi_set_command_engine_status_handler#
static sl_status_t sl_wifi_set_command_engine_status_handler (sl_wifi_command_engine_status_callback_t function, void * optional_arg)
Register a callback for SL_WIFI_COMMAND_ENGINE_STATUS_EVENTS group event from sl_wifi_event_group_t.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_wifi_command_engine_status_callback_t | [in] | function | Function pointer to callback of type sl_wifi_command_engine_status_callback_t. This parameter specifies the callback function that would be invoked when an event in the SL_WIFI_COMMAND_ENGINE_STATUS_EVENTS group occurs. |
| void * | [in] | optional_arg | Optional user-provided argument. This parameter allows the user to pass additional context or information to the callback function. This would be passed back to callback handler of type sl_wifi_command_engine_status_callback_t. |
This function allows the user to register a callback function for the SL_WIFI_COMMAND_ENGINE_STATUS_EVENTS group. When any event within this group occurs, the registered callback function would be invoked, providing the event details and any associated data.
Pre-conditions: sl_wifi_init should be called before this API.
Returns
sl_status_t. See Status Codes and Additional Status Codes for details.
Note
All the individual Wi-Fi events related to this group will be triggered via this callback.