You are viewing documentation for version:
WiSeConnect Status Codes#
This section provides a reference to the wiseconnect status codes returned by the WiSeConnect™ SDK which are not included in the list of Silicon Labs standard status codes.
Macros#
#define
SL_STATUS_OS_OPERATION_FAILURE ((sl_status_t)0x16051)
#define
SL_STATUS_BOOTUP_OPTIONS_NOT_SAVED ((sl_status_t)0x16052)
Bootup options were not saved.
#define
SL_STATUS_BOOTUP_OPTIONS_CHECKSUM_FAILURE ((sl_status_t)0x16053)
Bootup options checksum validation failed.
#define
SL_STATUS_BOOTLOADER_VERSION_MISMATCH ((sl_status_t)0x16054)
Bootloader version does not match expected version.
#define
SL_STATUS_WAITING_FOR_BOARD_READY ((sl_status_t)0x16055)
Waiting for the board to be ready.
#define
SL_STATUS_VALID_FIRMWARE_NOT_PRESENT ((sl_status_t)0x16056)
No valid firmware present.
#define
SL_STATUS_INVALID_OPTION ((sl_status_t)0x16057)
Provided option is invalid.
#define
SL_STATUS_SPI_BUSY ((sl_status_t)0x16058)
#define
SL_STATUS_CARD_READY_TIMEOUT ((sl_status_t)0x16059)
Timeout waiting for card to be ready.
#define
SL_STATUS_FW_LOAD_OR_UPGRADE_TIMEOUT ((sl_status_t)0x1605A)
Firmware load or upgrade operation timed out.
#define
SL_STATUS_WIFI_DOES_NOT_EXIST ((sl_status_t)0x0B21)
WiFi network does not exist.
#define
SL_STATUS_WIFI_NOT_AUTHENTICATED ((sl_status_t)0x0B22)
WiFi network is not authenticated.
#define
SL_STATUS_WIFI_NOT_KEYED ((sl_status_t)0x0B23)
Device attempts to connect to a secured WiFi network without providing the correct security key or credentials.
#define
SL_STATUS_WIFI_IOCTL_FAIL ((sl_status_t)0x0B24)
Input/Output Control operation failed.
#define
SL_STATUS_WIFI_BUFFER_UNAVAILABLE_TEMPORARY ((sl_status_t)0x0B25)
WiFi buffer temporarily unavailable.
#define
SL_STATUS_WIFI_BUFFER_UNAVAILABLE_PERMANENT ((sl_status_t)0x0B26)
WiFi buffer permanently unavailable.
#define
SL_STATUS_WIFI_WPS_PBC_OVERLAP ((sl_status_t)0x0B27)
WPS PBC overlap detected.
#define
SL_STATUS_WIFI_OUT_OF_EVENT_HANDLER_SPACE ((sl_status_t)0x0B29)
No space for additional event handlers.
#define
SL_STATUS_WIFI_SEMAPHORE_ERROR ((sl_status_t)0x0B2A)
Semaphore manipulation error.
#define
SL_STATUS_WIFI_FLOW_CONTROLLED ((sl_status_t)0x0B2B)
Packet retrieval cancelled due to flow control.
#define
SL_STATUS_WIFI_NO_CREDITS ((sl_status_t)0x0B2C)
Packet retrieval cancelled due to lack of bus credits.
#define
SL_STATUS_WIFI_NO_PACKET_TO_SEND ((sl_status_t)0x0B2D)
Packet retrieval cancelled due to no pending packets.
#define
SL_STATUS_WIFI_CORE_CLOCK_NOT_ENABLED ((sl_status_t)0x0B2E)
WiFi core disabled due to no clock.
#define
SL_STATUS_WIFI_CORE_IN_RESET ((sl_status_t)0x0B2F)
WiFi core disabled because it is in reset state.
#define
SL_STATUS_WIFI_UNSUPPORTED ((sl_status_t)0x0B30)
Unsupported WiFi function.
#define
SL_STATUS_WIFI_BUS_WRITE_REGISTER_ERROR ((sl_status_t)0x0B31)
Error occurred while writing to the WLAN register.
#define
SL_STATUS_WIFI_SDIO_BUS_UP_FAIL ((sl_status_t)0x0B32)
SDIO bus failed to initialize.
#define
SL_STATUS_WIFI_JOIN_IN_PROGRESS ((sl_status_t)0x0B33)
WiFi join operation is still in progress.
#define
SL_STATUS_WIFI_NETWORK_NOT_FOUND ((sl_status_t)0x0B34)
Specified WiFi network was not found.
#define
SL_STATUS_WIFI_INVALID_JOIN_STATUS ((sl_status_t)0x0B35)
Invalid status encountered during WiFi join.
#define
SL_STATUS_WIFI_UNKNOWN_INTERFACE ((sl_status_t)0x0B36)
Unknown WiFi interface specified.
#define
SL_STATUS_WIFI_SDIO_RX_FAIL ((sl_status_t)0x0B37)
Error occurred during SDIO receive operation.
#define
SL_STATUS_WIFI_HWTAG_MISMATCH ((sl_status_t)0x0B38)
Hardware tag header is corrupt.
#define
SL_STATUS_WIFI_RX_BUFFER_ALLOC_FAIL ((sl_status_t)0x0B39)
Failed to allocate a buffer for WiFi receive operation.
#define
SL_STATUS_WIFI_BUS_READ_REGISTER_ERROR ((sl_status_t)0x0B3A)
Error occurred while reading a bus hardware register.
#define
SL_STATUS_WIFI_THREAD_CREATE_FAILED ((sl_status_t)0x0B3B)
Failed to create a new WiFi thread.
#define
SL_STATUS_WIFI_QUEUE_ERROR ((sl_status_t)0x0B3C)
Error occurred while manipulating a WiFi queue.
#define
SL_STATUS_WIFI_BUFFER_POINTER_MOVE_ERROR ((sl_status_t)0x0B3D)
Error occurred while moving the current pointer of a buffer.
#define
SL_STATUS_WIFI_BUFFER_SIZE_SET_ERROR ((sl_status_t)0x0B3E)
Error occurred while setting the size of the packet buffer.
#define
SL_STATUS_WIFI_THREAD_STACK_NULL ((sl_status_t)0x0B3F)
Null stack pointer passed when a non-null pointer was required.
#define
SL_STATUS_WIFI_THREAD_DELETE_FAIL ((sl_status_t)0x0B40)
Error occurred while deleting a WiFi thread.
#define
SL_STATUS_WIFI_SLEEP_ERROR ((sl_status_t)0x0B41)
Failed to put a WiFi thread to sleep.
#define
SL_STATUS_WIFI_BUFFER_ALLOC_FAIL ((sl_status_t)0x0B42)
Failed to allocate a WiFi packet buffer.
#define
SL_STATUS_WIFI_INTERFACE_NOT_UP ((sl_status_t)0x0B44)
The requested WiFi interface is not active.
#define
SL_STATUS_WIFI_DELAY_TOO_LONG ((sl_status_t)0x0B45)
The requested delay for WiFi operation is too long.
#define
SL_STATUS_WIFI_INVALID_DUTY_CYCLE ((sl_status_t)0x0B46)
The specified WiFi duty cycle is outside the valid range.
#define
SL_STATUS_WIFI_PMK_WRONG_LENGTH ((sl_status_t)0x0B47)
The returned Pairwise Master Key (PMK) length is incorrect.
#define
SL_STATUS_WIFI_UNKNOWN_SECURITY_TYPE ((sl_status_t)0x0B48)
The security type of the WiFi Access Point is unknown.
#define
SL_STATUS_WIFI_WEP_NOT_ALLOWED ((sl_status_t)0x0B49)
WEP security is not allowed; use Open security instead.
#define
SL_STATUS_WIFI_WPA_KEYLEN_BAD ((sl_status_t)0x0B4A)
WPA/WPA2 key length must be between 8 and 64 bytes.
#define
SL_STATUS_WIFI_FILTER_NOT_FOUND ((sl_status_t)0x0B4B)
The specified WiFi filter ID was not found.
#define
SL_STATUS_WIFI_SPI_ID_READ_FAIL ((sl_status_t)0x0B4C)
Failed to read the SPI ID (0xfeedbead) from the chip.
#define
SL_STATUS_WIFI_SPI_SIZE_MISMATCH ((sl_status_t)0x0B4D)
Size mismatch between SPI and SDPCM header.
#define
SL_STATUS_WIFI_ADDRESS_ALREADY_REGISTERED ((sl_status_t)0x0B4E)
Attempted to register a multicast address that is already registered.
#define
SL_STATUS_WIFI_SDIO_RETRIES_EXCEEDED ((sl_status_t)0x0B4F)
SDIO transfer failed after exceeding the maximum number of retries.
#define
SL_STATUS_WIFI_NULL_PTR_ARG ((sl_status_t)0x0B50)
Null pointer argument passed to a function.
#define
SL_STATUS_WIFI_THREAD_FINISH_FAIL ((sl_status_t)0x0B51)
Error occurred while attempting to delete a thread.
#define
SL_STATUS_WIFI_WAIT_ABORTED ((sl_status_t)0x0B52)
Semaphore or mutex wait operation was aborted.
#define
SL_STATUS_WIFI_QUEUE_MESSAGE_UNALIGNED ((sl_status_t)0x0B53)
Unaligned message found in the queue.
#define
SL_STATUS_WIFI_MUTEX_ERROR ((sl_status_t)0x0B54)
Error occurred during a mutex operation.
#define
SL_STATUS_WIFI_SECURE_LINK_DECRYPT_ERROR ((sl_status_t)0x0B57)
Error occurred during decryption over a secure link.
#define
SL_STATUS_WIFI_SECURE_LINK_KEY_RENEGOTIATION_ERROR ((sl_status_t)0x0B59)
Error occurred during key renegotiation over a secure link.
#define
SL_STATUS_WIFI_INVALID_OPERMODE ((sl_status_t)0x0B60)
Invalid operation mode provided.
#define
SL_STATUS_WIFI_INVALID_ENCRYPTION_METHOD ((sl_status_t)0x0B61)
Invalid encryption method provided.
#define
SL_STATUS_TRNG_DUPLICATE_ENTROPY ((sl_status_t)0x0B62)
Error due to duplicate entropy elements in TRNG.
#define
SL_STATUS_TRANSCEIVER_INVALID_MAC_ADDRESS ((sl_status_t)0x0B63)
Provided MAC address is invalid.
#define
SL_STATUS_TRANSCEIVER_INVALID_QOS_PRIORITY ((sl_status_t)0x0B64)
Provided QoS priority is invalid.
#define
SL_STATUS_TRANSCEIVER_INVALID_CHANNEL ((sl_status_t)0x0B65)
Provided channel is invalid.
#define
SL_STATUS_TRANSCEIVER_INVALID_DATA_RATE ((sl_status_t)0x0B66)
Provided data rate is invalid.
#define
SL_STATUS_TRANSCEIVER_INVALID_CONFIG ((sl_status_t)0x0B67)
Provided transceiver configuration parameters are invalid.
#define
SL_STATUS_WIFI_IPV4_OK ((sl_status_t)0x0B68)
IPv4 configured successfully but IPv6 configuration failed (dual-stack partial success).
#define
SL_STATUS_WIFI_IPV6_OK ((sl_status_t)0x0B69)
IPv6 configured successfully but IPv4 configuration failed (dual-stack partial success).
#define
SL_STATUS_CRYPTO_INVALID_PARAMETER ((sl_status_t)0x1CCFE)
Return when parameter passed to Crypto SAPI is invalid.
#define
SL_STATUS_CRYPTO_INVALID_SIGNATURE ((sl_status_t)0x1CC9A)
Return in AEAD (CCM, GCM, Chachapoly) decryption function, when MAC generated during decryption does not match the MAC passed.
#define
SL_STATUS_WIFI_CONNECTION_LOST ((sl_status_t)0x10B28)
#define
SL_STATUS_SI91X_SCAN_ISSUED_IN_ASSOCIATED_STATE ((sl_status_t)0x10002)
Scan command issued while device is already associated with an access point.
#define
SL_STATUS_SI91X_NO_AP_FOUND ((sl_status_t)0x10003)
#define
SL_STATUS_SI91X_INVALID_PSK_IN_WEP_SECURITY ((sl_status_t)0x10004)
Incorrect PSK provided while trying to join an access point with WEP security enabled.
#define
SL_STATUS_SI91X_INVALID_BAND ((sl_status_t)0x10005)
#define
SL_STATUS_SI91X_UNASSOCIATED ((sl_status_t)0x10006)
Device is not associated or is in an unassociated state.
#define
SL_STATUS_SI91X_DEAUTHENTICATION_RECEIVED_FROM_AP ((sl_status_t)0x10008)
De-authentication received from access point.
#define
SL_STATUS_SI91X_ASSOCIATION_FAILED ((sl_status_t)0x10009)
Failed to associate with the access point during "Join".
#define
SL_STATUS_SI91X_INVALID_CHANNEL ((sl_status_t)0x1000A)
Invalid channel specified.
#define
SL_STATUS_SI91X_JOIN_AUTHENTICATION_FAILED ((sl_status_t)0x1000E)
Authentication failure during "Join". Unable to find access point during join which was found during scan.
#define
SL_STATUS_SI91X_BEACON_MISSED_FROM_AP_DURING_JOIN ((sl_status_t)0x1000F)
Missed beacon from access point during join.
#define
SL_STATUS_SI91X_INVALID_MAC_SUPPLIED ((sl_status_t)0x10013)
Non-existent MAC address supplied in "Disassociate" command.
#define
SL_STATUS_SI91X_EAP_CONFIG_NOT_DONE ((sl_status_t)0x10014)
EAP configuration is not completed.
#define
SL_STATUS_SI91X_MEMORY_FAILED_FROM_MODULE ((sl_status_t)0x10015)
Memory allocation failed or store configuration checksum failed.
#define
SL_STATUS_SI91X_INSUFFICIENT_INFO ((sl_status_t)0x10016)
Insufficient or incorrect information provided in join command.
#define
SL_STATUS_SI91X_NOT_AP_INTERFACE ((sl_status_t)0x10017)
Not an access point interface.
#define
SL_STATUS_SI91X_INVALID_PUSH_BUTTON_SEQUENCE ((sl_status_t)0x10018)
Push button command issued before the expiry of the previous push button command.
#define
SL_STATUS_SI91X_REJOIN_FAILURE ((sl_status_t)0x10019)
Rejoin failure: Access point not found.
#define
SL_STATUS_SI91X_FREQUENCY_NOT_SUPPORTED ((sl_status_t)0x1001A)
Operation failed: Frequency not supported.
#define
SL_STATUS_SI91X_INVALID_OPERMODE ((sl_status_t)0x1001B)
Operation failed: Invalid operation mode.
#define
SL_STATUS_SI91X_EAP_CONFIG_FAILED ((sl_status_t)0x1001C)
EAP configuration failed.
#define
SL_STATUS_SI91X_P2P_CONFIG_FAILED ((sl_status_t)0x1001D)
P2P configuration failed.
#define
SL_STATUS_SI91X_GROUP_OWNER_NEGOTIATION_FAILED ((sl_status_t)0x1001E)
Failed to start Group Owner negotiation.
#define
SL_STATUS_SI91X_JOIN_TIMEOUT ((sl_status_t)0x10020)
Join operation timed out.
#define
SL_STATUS_SI91X_COMMAND_GIVEN_IN_INVALID_STATE ((sl_status_t)0x10021)
Command issued in an invalid state.
#define
SL_STATUS_SI91X_INVALID_QUERY_GO_PARAMS ((sl_status_t)0x10022)
Invalid parameters for Query GO in the current operating mode.
#define
SL_STATUS_SI91X_ACCESS_POINT_FAILED ((sl_status_t)0x10023)
Failed to form access point.
#define
SL_STATUS_SI91X_INVALID_SCAN_INFO ((sl_status_t)0x10024)
Invalid scan input parameters.
#define
SL_STATUS_SI91X_COMMAND_ISSUED_IN_REJOIN_STATE ((sl_status_t)0x10025)
Command issued during re-join operation.
#define
SL_STATUS_SI91X_WRONG_PARAMETERS ((sl_status_t)0x10026)
Incorrect parameters provided for the command.
#define
SL_STATUS_SI91X_PROVISION_DISCOVERY_FAILED_IN_P2P ((sl_status_t)0x10027)
Provision discovery failed in P2P mode.
#define
SL_STATUS_SI91X_INVALID_PSK_LENGTH ((sl_status_t)0x10028)
PSK length less than 8 bytes or more than 63 bytes.
#define
SL_STATUS_SI91X_FAILED_TO_CLEAR_OR_SET_EAP_CERTIFICATE ((sl_status_t)0x10029)
Failed to clear or to set the Enterprise Certificate (Set Certificate).
#define
SL_STATUS_SI91X_P2P_GO_NEGOTIATED_FAILED ((sl_status_t)0x1002A)
P2P Group Owner negotiation failed.
#define
SL_STATUS_SI91X_ASSOCIATION_TIMEOUT_IN_P2P_WPS_MODE ((sl_status_t)0x1002B)
Association between nodes failed in P2P WPS mode due to timeout.
#define
SL_STATUS_SI91X_COMMAND_ISSUED_WHILE_INTERNAL_OPERATION ((sl_status_t)0x1002C)
Command issued by the Host while the device is executing an internal operation (for example, auto-join or auto-create).
#define
SL_STATUS_SI91X_INVALID_WEP_KEY_LEN ((sl_status_t)0x1002D)
#define
SL_STATUS_SI91X_ICMP_REQUEST_TIMEOUT_ERROR ((sl_status_t)0x1002E)
#define
SL_STATUS_SI91X_ICMP_DATA_SIZE_EXCEED_MAX_LIMIT ((sl_status_t)0x1002F)
ICMP data size exceeds the maximum limit.
#define
SL_STATUS_SI91X_SEND_DATA_PACKET_EXCEED_LIMIT ((sl_status_t)0x10030)
Data packet size exceeded the limit, MQTT published the data and length mismatched, or MQTT send data packet exceeded the limit.
#define
SL_STATUS_SI91X_ARP_CACHE_NOT_FOUND ((sl_status_t)0x10031)
ARP cache entry not found.
#define
SL_STATUS_SI91X_UART_COMMAND_TIMEOUT ((sl_status_t)0x10032)
#define
SL_STATUS_SI91X_FIXED_DATA_RATE_NOT_SUPPORTED_BY_AP ((sl_status_t)0x10033)
Fixed data rate not supported by the connected AP.
#define
SL_STATUS_SI91X_USERNAME_PASSWORD_CLIENTID_TOPIC_MAX_LEN ((sl_status_t)0x10036)
Maximum length exceeded for username, password, client ID, or topic in MQTT.
#define
SL_STATUS_SI91X_INVALID_WPS_PIN ((sl_status_t)0x10037)
#define
SL_STATUS_SI91X_INVALID_WPS_PIN_LEN ((sl_status_t)0x10038)
#define
SL_STATUS_SI91X_INVALID_PMK_LEN ((sl_status_t)0x10039)
#define
SL_STATUS_SI91X_SSID_NOT_PRESENT_FOR_PMK_GENERATION ((sl_status_t)0x1003A)
SSID not present for PMK generation.
#define
SL_STATUS_SI91X_SSID_INCORRECT_PMK_GENERATION ((sl_status_t)0x1003B)
SSID incorrect for PMK generation(more than 32 bytes).
#define
SL_STATUS_SI91X_BAND_NOT_SUPPORTED ((sl_status_t)0x1003C)
#define
SL_STATUS_SI91X_INVALID_USR_STORE_CONFIGURATION_LEN ((sl_status_t)0x1003D)
Invalid user store configuration length.
#define
SL_STATUS_SI91X_INVALID_COMMAND_LEN ((sl_status_t)0x1003E)
Invalid command length (exceeds the number of characters specified in the PRM).
#define
SL_STATUS_SI91X_DATA_PACKET_DROPPED ((sl_status_t)0x1003F)
#define
SL_STATUS_SI91X_WEP_KEY_NOT_GIVEN ((sl_status_t)0x10040)
#define
SL_STATUS_SI91X_INVALID_STORE_CONFIG_PROFILE ((sl_status_t)0x10041)
Store config profile length error.
#define
SL_STATUS_SI91X_MISSING_PSK_OR_PMK ((sl_status_t)0x10042)
#define
SL_STATUS_SI91X_INVALID_SECURITY_MODE_IN_JOIN_COMMAND ((sl_status_t)0x10043)
Invalid security mode in join command.
#define
SL_STATUS_SI91X_MAX_BEACON_MISCOUNT ((sl_status_t)0x10044)
Maximum beacon miscount reached: De-authentication due to beacon miss.
#define
SL_STATUS_SI91X_DEAUTH_REQUEST_FROM_SUPPLICANT ((sl_status_t)0x10045)
De-authentication request received from supplicant.
#define
SL_STATUS_SI91X_DEAUTH_REQUEST_FROM_FROM_AP ((sl_status_t)0x10046)
De-authentication request received from AP after channel switching.
#define
SL_STATUS_SI91X_MISSED_SYNCHRONIZATION ((sl_status_t)0x10047)
#define
SL_STATUS_SI91X_AUTHENTICATION_TIMEOUT ((sl_status_t)0x10048)
Authentication timeout occurred.
#define
SL_STATUS_SI91X_ASSOCIATION_TIMEOUT ((sl_status_t)0x10049)
#define
SL_STATUS_SI91X_BG_SCAN_NOT_ALLOWED ((sl_status_t)0x1004A)
BG scan in given channels is not allowed.
#define
SL_STATUS_SI91X_SSID_MISMATCH ((sl_status_t)0x1004B)
Scanned SSID and SSID given in join are not matching.
#define
SL_STATUS_SI91X_CLIENT_MAX_SUPPORTED_EXCEEDED ((sl_status_t)0x1004C)
The number of clients exceeds the maximum number of supported stations.
#define
SL_STATUS_SI91X_HT_CAPABILITIES_NOT_SUPPORTED ((sl_status_t)0x1004D)
The specified HT capabilities are not supported.
#define
SL_STATUS_SI91X_UART_FLOW_NOT_SUPPORTED ((sl_status_t)0x1004E)
UART flow control is not supported.
#define
SL_STATUS_SI91X_ZB_BT_BLE_PKT_RECEIVED ((sl_status_t)0x1004F)
ZB/BT/BLE packet received, but the protocol is not enabled.
#define
SL_STATUS_SI91X_MGMT_PKT_DROPPED ((sl_status_t)0x10050)
Management packet dropped.
#define
SL_STATUS_SI91X_INVALID_RF_CURRENT_MODE ((sl_status_t)0x10051)
The current RF mode is invalid.
#define
SL_STATUS_SI91X_POWER_SAVE_NOT_SUPPORTED ((sl_status_t)0x10052)
Power save is not supported for the specified interface.
#define
SL_STATUS_SI91X_CONCURRENT_AP_IN_CONNECTED_STATE ((sl_status_t)0x10053)
Concurrent AP is in a connected state.
#define
SL_STATUS_SI91X_CONNECTED_AP_OR_STATION_CHANNEL_MISMATCH ((sl_status_t)0x10054)
Channel mismatch between connected AP and station.
#define
SL_STATUS_SI91X_IAP_COPROCESSOR_ERROR ((sl_status_t)0x10055)
IAP coprocessor error occurred.
#define
SL_STATUS_SI91X_WPS_NOT_SUPPORTED ((sl_status_t)0x10056)
WPS is not supported in the current operating mode.
#define
SL_STATUS_SI91X_CONCURRENT_AP_CHANNEL_MISMATCH ((sl_status_t)0x10057)
Concurrent AP channel does not match the connected station channel.
#define
SL_STATUS_SI91X_PBC_SESSION_OVERLAP ((sl_status_t)0x10058)
PBC session overlap error.
#define
SL_STATUS_SI91X_BT_FEATURE_BITMAP_INVALID ((sl_status_t)0x10059)
The Bluetooth feature bitmap is invalid.
#define
SL_STATUS_SI91X_FOUR_WAY_HANDSHAKE_FAILED ((sl_status_t)0x1005A)
The 4/4 confirmation of the four-way handshake failed.
#define
SL_STATUS_SI91X_MAC_ADDRESS_NOT_PRESENT_IN_MAC_JOIN ((sl_status_t)0x1005B)
MAC address is not present in the MAC-based join.
#define
SL_STATUS_SI91X_CONCURRENT_MODE_DOWN ((sl_status_t)0x1005C)
Concurrent mode requires both AP and client to be up for configuration.
#define
SL_STATUS_SI91X_CERTIFICATE_LOAD_NOT_ALLOWED_IN_FLASH ((sl_status_t)0x1005D)
Certificate load operation is not allowed in flash memory.
#define
SL_STATUS_SI91X_CERTIFICATE_LOAD_NOT_ALLOWED_IN_RAM ((sl_status_t)0x1005E)
Certificate load operation is not allowed in RAM.
#define
SL_STATUS_SI91X_WRONG_CERTIFICATE_LOAD_INDEX ((sl_status_t)0x1005F)
Certificate load failed due to an incorrect index.
#define
SL_STATUS_SI91X_AP_HT_CAPS_NOT_ENABLED ((sl_status_t)0x10060)
Access Point HT capabilities are not enabled.
#define
SL_STATUS_SI91X_ADDRESS_FAMILY_NOT_SUPPORTED ((sl_status_t)0x10061)
The specified address family is not supported by the protocol.
#define
SL_STATUS_SI91X_INVALID_BEACON_INTERVAL_OR_DTM_PERIOD ((sl_status_t)0x10062)
The provided beacon interval or DTIM period is invalid.
#define
SL_STATUS_SI91X_INVALID_CONFIG_RANGE_PROVIDED ((sl_status_t)0x10063)
The provided configuration range is invalid.
#define
SL_STATUS_SI91X_INVALID_CONFIG_TYPE ((sl_status_t)0x10064)
The provided configuration type (for example, RTS threshold) is invalid.
#define
SL_STATUS_SI91X_ERROR_WITH_MQTT_COMMAND ((sl_status_t)0x10065)
An error occurred with the MQTT command.
#define
SL_STATUS_SI91X_HIGHER_LISTEN_INTERVAL ((sl_status_t)0x10066)
The listen interval in power save mode is greater than that specified in the join command.
#define
SL_STATUS_SI91X_WLAN_RADIO_DEREGISTERED ((sl_status_t)0x10067)
The WLAN radio has been deregistered.
#define
SL_STATUS_SI91X_SAE_FAILURE_DUE_TO_MULTIPLE_CONFIRM_FRAMES_FROM_AP ((sl_status_t)0x10069)
SAE authentication failed due to multiple confirm frames received from the Access Point.
#define
SL_STATUS_SI91X_EC_GROUP_STATION_UNSUPPORTED_BY_AP ((sl_status_t)0x1006A)
The Access Point does not support the EC-group set by the station.
#define
SL_STATUS_SI91X_WPS_CREDENTIALS_RECEIVED_WITHOUT_JOIN_COMMAND ((sl_status_t)0x1006B)
WPS credentials have been received, but the device did not join the network.
#define
SL_STATUS_SI91X_NO_11AX_SUPPORT_IN_AP ((sl_status_t)0x1006C)
802.11ax (Wi-Fi 6) is not supported in Access Point mode.
#define
SL_STATUS_SI91X_NON_PREF_CHAN_CONFIG_FAILED ((sl_status_t)0x1006D)
Non-preferred channel configuration failed.
#define
SL_STATUS_TWT_SUPPORT_NOT_ENABLED_ERR ((sl_status_t)0x10070)
Error occurs when HE_PARAMS_SUPPORT and SLI_SI91X_ENABLE_TWT_FEATURE macros are not enabled.
#define
SL_STATUS_TWT_SETUP_ERR_SESSION_ACTIVE ((sl_status_t)0x10071)
Error occurs when a TWT config command is issued while there is already an active TWT session.
#define
SL_STATUS_TWT_TEARDOWN_ERR_FLOWID_NOT_MATCHED ((sl_status_t)0x10072)
Error occurs when a TWT teardown command is issued with a flow ID that does not match the existing session flow ID.
#define
SL_STATUS_TWT_TEARDOWN_ERR_NOACTIVE_SESS ((sl_status_t)0x10073)
Error occurs when a teardown command is issued while there is no active TWT session.
#define
SL_STATUS_TWT_SESSION_NOT_FEASIBLE ((sl_status_t)0x10074)
Indicates that a TWT session is not feasible. This error is thrown only when the TWT Auto Selection API is used.
#define
SL_STATUS_SI91X_RESCHEDULE_TWT_NOT_SUPPORTED ((sl_status_t)0x10075)
Error occurs when the AP does not support TWT information frame reception.
#define
SL_STATUS_SI91X_RESCHEDULE_TWT_ERR_NOACTIVE_SESS ((sl_status_t)0x10076)
Error occurs when there is no active TWT agreement corresponding to the given flow ID.
#define
SL_STATUS_SI91X_TWT_RESCHEDULING_IN_PROGRESS ((sl_status_t)0x10077)
Indicates that a suspend or resume TWT action is currently in progress.
#define
SL_STATUS_SI91X_RESCHEDULE_TWT_PACKET_CREATION_FAILED ((sl_status_t)0x10078)
Error occurs when TWT information frame packet creation fails in firmware.
#define
SL_STATUS_SI91X_INVALID_STATION_TSF ((sl_status_t)0x10079)
Error occurs when the station TSF is invalid, typically when the station is not connected or has not received at least one beacon.
#define
SL_STATUS_SI91X_BLE_STACK_DEINIT_FAILED ((sl_status_t)0x1007A)
Error occurs when BLE stack deinitialization failed during BLE disable.
#define
SL_STATUS_SI91X_BLE_STACK_REINIT_FAILED ((sl_status_t)0x1007B)
Error occurs when BLE stack reinitialization failed during BLE enable.
#define
SL_STATUS_SI91X_BLE_ALREADY_ENABLED ((sl_status_t)0x1007C)
Error occurs when BLE enable was requested while BLE is already enabled.
#define
SL_STATUS_SI91X_BLE_COEX_MEMORY_NOT_AVAILABLE ((sl_status_t)0x1007D)
Error occurs when BLE coexistence memory is not available; previously allocated BLE memory was not freed before calling BLE enable.
#define
SL_STATUS_SI91X_MQTT_ERROR_UNACCEPTABLE_PROTOCOL ((sl_status_t)0x10081)
Error occurs when the server does not support the level of the MQTT protocol requested by the client.
#define
SL_STATUS_SI91X_MQTT_ERROR_IDENTIFIER_REJECTED ((sl_status_t)0x10082)
Error occurs when the client identifier is correct UTF-8 but is not allowed by the server.
#define
SL_STATUS_SI91X_MQTT_ERROR_SERVER_UNAVAILABLE ((sl_status_t)0x10083)
Error occurs when the network connection has been made but the MQTT service is unavailable.
#define
SL_STATUS_SI91X_MQTT_ERROR_BAD_USERNAME_PASSWORD ((sl_status_t)0x10084)
The data in the username or password is malformed.
#define
SL_STATUS_SI91X_MQTT_ERROR_NOT_AUTHORIZED ((sl_status_t)0x10085)
The client is not authorized to connect.
#define
SL_STATUS_SI91X_SA_QUERY_TIMEOUT ((sl_status_t)0x10086)
Disconnection due to SA Query Timeout.
#define
SL_STATUS_SI91X_TRANSCEIVER_PEER_DS_FEAT_DISABLED ((sl_status_t)0x10096)
Feature to add peers in MAC layer is disabled.
#define
SL_STATUS_SI91X_TRANSCEIVER_PEER_ALREADY_EXISTS ((sl_status_t)0x10097)
Peer already exists in MAC layer.
#define
SL_STATUS_SI91X_TRANSCEIVER_MAX_PEER_LIMIT_REACHED ((sl_status_t)0x10098)
Max peer limit reached in MAC layer.
#define
SL_STATUS_SI91X_TRANSCEIVER_PEER_NOT_FOUND ((sl_status_t)0x10099)
Peer not found in MAC layer.
#define
SL_STATUS_SI91X_DUPLICATE_ENTRY_EXISTS_IN_DNS_SERVER_TABLE ((sl_status_t)0x100AF)
Duplicate entry exists in DNS server table.
#define
SL_STATUS_SI91X_NO_MEM_AVAILABLE ((sl_status_t)0x100B1)
Memory error: No memory available.
#define
SL_STATUS_SI91X_INVALID_CHARACTERS_IN_JSON_OBJECT ((sl_status_t)0x100B2)
Invalid characters in JSON object.
#define
SL_STATUS_SI91X_NO_KEY_FOUND ((sl_status_t)0x100B3)
Update commands: No such key found.
#define
SL_STATUS_SI91X_NO_FILE_FOUND ((sl_status_t)0x100B4)
No such file found: Re-check file name.
#define
SL_STATUS_SI91X_NO_WEB_PAGE_EXISTS_WITH_SAME_FILENAME ((sl_status_t)0x100B5)
No corresponding web page exists with the same filename.
#define
SL_STATUS_SI91X_SPACE_UNAVAILABLE_FOR_NEW_FILE ((sl_status_t)0x100B6)
Space unavailable for new file.
#define
SL_STATUS_SI91X_INVALID_INPUT_DATA ((sl_status_t)0x100C1)
Invalid input data, re-check filename, lengths, etc.
#define
SL_STATUS_SI91X_NO_SPACE_AVAILABLE_FOR_NEW_FILE ((sl_status_t)0x100C2)
Space unavailable for new file.
#define
SL_STATUS_SI91X_EXISTING_FILE_OVERWRITE ((sl_status_t)0x100C3)
Existing file overwrite: Exceeds size of previous file. Use erase and try again.
#define
SL_STATUS_SI91X_NO_SUCH_FILE_FOUND ((sl_status_t)0x100C4)
No such file found. Re-check filename.
#define
SL_STATUS_SI91X_MEMORY_ERROR ((sl_status_t)0x100C5)
Memory Error: No memory available.
#define
SL_STATUS_SI91X_RECEIVED_MORE_WEB_PAGE_DATA ((sl_status_t)0x100C6)
Received more web page data than the total length initially specified.
#define
SL_STATUS_SI91X_SET_REGION_ERROR ((sl_status_t)0x100C7)
Error in set region command.
#define
SL_STATUS_SI91X_INVALID_WEBPAGE_CURRENT_CHUNK_LEN ((sl_status_t)0x100C8)
Web page current chunk length is incorrect.
#define
SL_STATUS_SI91X_AP_SET_REGION_COMMAND_ERROR ((sl_status_t)0x100CA)
Error in AP set region command.
#define
SL_STATUS_SI91X_AP_SET_REGION_COMMAND_PARAMETERS_ERROR ((sl_status_t)0x100CB)
Error in AP set region command parameters.
#define
SL_STATUS_SI91X_REGION_CODE_NOT_SUPPORTED ((sl_status_t)0x100CC)
Region code not supported.
#define
SL_STATUS_SI91X_EXTRACTING_COUNTRY_REGION_FROM_BEACON_FAILED ((sl_status_t)0x100CD)
Error in extracting country region from beacon.
#define
SL_STATUS_SI91X_SELECTED_REGION_NOT_SUPPORTED ((sl_status_t)0x100CE)
Device does not have selected region support.
#define
SL_STATUS_SI91X_HOST_VOLTAGE_OUT_OF_RANGE ((sl_status_t)0x100D0)
#define
SL_STATUS_SI91X_SSL_TLS_CONTEXT_CREATION_FAILED ((sl_status_t)0x100D1)
SSL/TLS context create failed.
#define
SL_STATUS_SI91X_SSL_TLS_HANDSHAKE_FAIL ((sl_status_t)0x100D2)
SSL/TLS handshake failed. Socket will be closed.
#define
SL_STATUS_SI91X_SSL_TLS_MAX_SOCKETS_REACHED ((sl_status_t)0x100D3)
SSL/TLS max sockets reached.
#define
SL_STATUS_SI91X_FTP_CLIENT_NOT_CONNECTED ((sl_status_t)0x100D3)
FTP client is not connected.
#define
SL_STATUS_SI91X_CIPHER_SET_FAILED ((sl_status_t)0x100D4)
#define
SL_STATUS_SI91X_HTTP_CREDENTIALS_MAX_LEN_EXCEEDED ((sl_status_t)0x100F1)
HTTP credentials maximum length exceeded.
#define
SL_STATUS_SI91X_FEATURE_NOT_SUPPORTED ((sl_status_t)0x100F7)
#define
SL_STATUS_SI91X_FLASH_WRITE_OR_FLASH_DATA_VERIFICATION_FAILED ((sl_status_t)0x100F8)
Unable to write to flash OR flash data verification failed.
#define
SL_STATUS_SI91X_CALIBRATION_DATA_VERIFICATION_FAILED ((sl_status_t)0x100F9)
Calibration data verification failed.
#define
SL_STATUS_SI91X_EVM_INDEX_LIMIT_REACHED ((sl_status_t)0x100FD)
#define
SL_STATUS_SI91X_EFUSE_ALREADY_POPULATED ((sl_status_t)0x100FA)
Efuse data is already populated. Write prohibited.
#define
SL_STATUS_SI91X_SNMP_INTERNAL_ERROR ((sl_status_t)0x10100)
#define
SL_STATUS_SI91X_SNMP_INVALID_IP_PROTOCOL ((sl_status_t)0x10104)
SNMP invalid IP protocol error.
#define
SL_STATUS_SI91X_EFUSE_DATA_INVALID ((sl_status_t)0x10106)
#define
SL_STATUS_SI91X_VENDOR_IE_INVALID_IE_LENGTH ((sl_status_t)0x1010E)
Vendor IE buffer length is invalid or exceeds maximum allowed size.
#define
SL_STATUS_SI91X_VENDOR_IE_INVALID_UNIQUE_ID ((sl_status_t)0x1010F)
Vendor IE unique ID is out of valid range or not found.
#define
SL_STATUS_SI91X_VENDOR_IE_INVALID_ACTION ((sl_status_t)0x10110)
Vendor IE operation is not supported or invalid action specified.
#define
SL_STATUS_SI91X_VENDOR_IE_INVALID_PACKET_BITMAP ((sl_status_t)0x10111)
Vendor IE management frame bitmap contains invalid or unsupported frame types.
#define
SL_STATUS_SI91X_VENDOR_IE_NO_SLOTS_AVAILABLE ((sl_status_t)0x10112)
No firmware memory slots available for adding new vendor IE.
#define
SL_STATUS_SI91X_NO_DATA_RECEIVED_OR_RECEIVE_TIMEOUT ((sl_status_t)0x1BB01)
No data received or receive timeout.
#define
SL_STATUS_SI91X_INSUFFICIENT_DATA_FOR_TIME_CONVERSION ((sl_status_t)0x1BB08)
Insufficient data for converting NTP time to mm-dd-yy time format.
#define
SL_STATUS_SI91X_INVALID_SNTP_SERVER_ADDRESS ((sl_status_t)0x1BB0A)
Invalid SNTP server address.
#define
SL_STATUS_SI91X_SNTP_CLIENT_NOT_STARTED ((sl_status_t)0x1BB0B)
#define
SL_STATUS_SI91X_SNTP_SERVER_UNAVAILABLE ((sl_status_t)0x1BB10)
SNTP server not available. Client will not get any time update service from current server.
#define
SL_STATUS_SI91X_SNTP_SERVER_AUTHENTICATION_FAILED ((sl_status_t)0x1BB15)
SNTP server authentication failed.
#define
SL_STATUS_SI91X_INTERNAL_ERROR ((sl_status_t)0x1BB0E)
#define
SL_STATUS_SI91X_MULTICAST_IP_ADDRESS_ENTRY_NOT_FOUND ((sl_status_t)0x1BB16)
Entry not found for multicast IP address.
#define
SL_STATUS_SI91X_MULTICAST_NO_ENTRIES_FOUND ((sl_status_t)0x1BB17)
No more entries found for multicast.
#define
SL_STATUS_SI91X_IP_ADDRESS_ERROR ((sl_status_t)0x1BB21)
#define
SL_STATUS_SI91X_SOCKET_ALREADY_BOUND ((sl_status_t)0x1BB22)
#define
SL_STATUS_SI91X_PORT_UNAVAILABLE ((sl_status_t)0x1BB23)
#define
SL_STATUS_SI91X_SOCKET_NOT_CREATED ((sl_status_t)0x1BB27)
#define
SL_STATUS_SI91X_ICMP_REQUEST_FAILED ((sl_status_t)0x1BB29)
#define
SL_STATUS_SI91X_MAX_LISTEN_SOCKETS_REACHED ((sl_status_t)0x1BB33)
Maximum listen sockets reached.
#define
SL_STATUS_SI91X_DHCP_DUPLICATE_LISTEN ((sl_status_t)0x1BB34)
#define
SL_STATUS_SI91X_PORT_NOT_IN_CLOSE_STATE ((sl_status_t)0x1BB35)
Port not in closed state.
#define
SL_STATUS_SI91X_SOCKET_CLOSED ((sl_status_t)0x1BB36)
Socket is closed or in process of closing.
#define
SL_STATUS_SI91X_PROCESS_IN_PROGRESS ((sl_status_t)0x1BB37)
#define
SL_STATUS_SI91X_CONNECT_TO_NON_EXISTING_TCP_SERVER_SOCKET ((sl_status_t)0x1BB38)
Trying to connect to a non-existing TCP server socket.
#define
SL_STATUS_SI91X_ERROR_IN_LEN_OF_THE_COMMAND ((sl_status_t)0x1BB3E)
Error in the length of the command (exceeds the number of characters mentioned in the PRM).
#define
SL_STATUS_SI91X_WRONG_PACKET_INFO ((sl_status_t)0x1BB40)
Wrong packet information.
#define
SL_STATUS_SI91X_CORRUPTED_RPS ((sl_status_t)0x1BB41)
Corrupted RPS encountered during firmware update.
#define
SL_STATUS_SI91X_SOCKET_STILL_BOUND ((sl_status_t)0x1BB42)
#define
SL_STATUS_SI91X_NO_FREE_PORT ((sl_status_t)0x1BB45)
#define
SL_STATUS_SI91X_INVALID_PORT ((sl_status_t)0x1BB46)
#define
SL_STATUS_SI91X_CORRUPTED_RPS_HEADER ((sl_status_t)0x1BB49)
Corrupted RPS header encountered or Received empty RPS file(no data) during firmware update.
#define
SL_STATUS_SI91X_FEATURE_UNSUPPORTED ((sl_status_t)0x1BB4B)
#define
SL_STATUS_SI91X_SOCKET_IN_UNCONNECTED_STATE ((sl_status_t)0x1BB50)
Socket is not in a connected state. Disconnected from the server. In the case of FTP, the user needs to issue a destroy command after receiving this error.
#define
SL_STATUS_SI91X_POP3_SESSION_CREATION_FAILED ((sl_status_t)0x1BB87)
POP3 session creation failed or POP3 session got terminated.
#define
SL_STATUS_SI91X_DHCPV6_HANDSHAKE_FAIL ((sl_status_t)0x1BB9C)
DHCPv6 handshake failure.
#define
SL_STATUS_SI91X_DHCP_INVALID_IP_RESPONSE ((sl_status_t)0x1BB9D)
DHCP invalid IP response.
#define
SL_STATUS_SI91X_SMTP_AUTHENTICATION_ERROR ((sl_status_t)0x1BBA0)
SMTP authentication error.
#define
SL_STATUS_SI91X_SMTP_OVER_SIZE_MAIL_DATA ((sl_status_t)0x1BBA1)
No DNS server was specified, SMTP over size mail data.
#define
SL_STATUS_SI91X_SMTP_INVALID_SERVER_REPLY ((sl_status_t)0x1BBA2)
SMTP invalid server reply.
#define
SL_STATUS_SI91X_SMTP_DNS_QUERY_FAILED ((sl_status_t)0x1BBA3)
DNS query failed, SMTP internal error.
#define
SL_STATUS_SI91X_SMTP_BAD_DNS_ADDRESS ((sl_status_t)0x1BBA4)
Bad DNS address, SMTP server error code received.
#define
SL_STATUS_SI91X_SMTP_INVALID_PARAMETERS ((sl_status_t)0x1BBA5)
#define
SL_STATUS_SI91X_SMTP_PACKET_ALLOCATION_FAILED ((sl_status_t)0x1BBA6)
SMTP packet allocation failed.
#define
SL_STATUS_SI91X_SMTP_GREET_REPLY_FAILED ((sl_status_t)0x1BBA7)
#define
SL_STATUS_SI91X_SMTP_PARAMETER_ERROR ((sl_status_t)0x1BBA8)
Parameter error, SMTP hello reply error.
#define
SL_STATUS_SI91X_SMTP_MAIL_REPLY_ERROR ((sl_status_t)0x1BBA9)
#define
SL_STATUS_SI91X_SMTP_RCPT_REPLY_ERROR ((sl_status_t)0x1BBAA)
#define
SL_STATUS_SI91X_SMTP_MESSAGE_REPLY_ERROR ((sl_status_t)0x1BBAB)
SMTP message reply error.
#define
SL_STATUS_SI91X_SMTP_DATA_REPLY_ERROR ((sl_status_t)0x1BBAC)
#define
SL_STATUS_SI91X_SMTP_AUTH_REPLY_ERROR ((sl_status_t)0x1BBAD)
SMTP authentication reply error.
#define
SL_STATUS_SI91X_SMTP_SERVER_REPLY_ERROR ((sl_status_t)0x1BBAE)
#define
SL_STATUS_SI91X_DNS_DUPLICATE_ENTRY ((sl_status_t)0x1BBAF)
#define
SL_STATUS_SI91X_SMTP_OVERSIZE_SERVER_REPLY ((sl_status_t)0x1BBB1)
SMTP oversize server reply.
#define
SL_STATUS_SI91X_SMTP_CLIENT_NOT_INITIALIZED ((sl_status_t)0x1BBB2)
SMTP client not initialized.
#define
SL_STATUS_SI91X_DNS_IPV6_NOT_SUPPORTED ((sl_status_t)0x1BBB3)
#define
SL_STATUS_SI91X_INVALID_MAIL_INDEX_FOR_POP3_MAIL_RETRIEVE_COMMAND ((sl_status_t)0x1BBC5)
Invalid mail index specified for the POP3 mail retrieve command.
#define
SL_STATUS_SI91X_SSL_TLS_HANDSHAKE_FAILED ((sl_status_t)0x1BBD2)
SSL/TLS handshake process failed.
#define
SL_STATUS_SI91X_FTP_CLIENT_DISCONNECTED ((sl_status_t)0x1BBD3)
FTP client is either not connected or has been disconnected from the FTP server.
#define
SL_STATUS_SI91X_FTP_CLIENT_NOT_DISCONNECTED ((sl_status_t)0x1BBD4)
FTP client is still connected and has not been disconnected.
#define
SL_STATUS_SI91X_TLS_RX_LEN_ERR_OR_FTP_FILE_NOT_OPEN ((sl_status_t)0x1BBD5)
TLS received data length exceeded or FTP file could not be opened.
#define
SL_STATUS_SI91X_SSL_TLS_HANDSHAKE_TIMEOUT_OR_FTP_FILE_NOT_CLOSED ((sl_status_t)0x1BBD6)
SSL/TLS handshake timed out or the FTP file was not closed properly.
#define
SL_STATUS_SI91X_FTP_EXPECTED_1XX_RESPONSE_NOT_RECEIVED ((sl_status_t)0x1BBD9)
Expected 1XX response from the FTP server was not received.
#define
SL_STATUS_SI91X_FTP_EXPECTED_2XX_RESPONSE_NOT_RECEIVED ((sl_status_t)0x1BBDA)
Expected 2XX response from the FTP server was not received.
#define
SL_STATUS_SI91X_FTP_EXPECTED_22X_RESPONSE_NOT_RECEIVED ((sl_status_t)0x1BBDB)
Expected 22X response from the FTP server was not received.
#define
SL_STATUS_SI91X_FTP_EXPECTED_23X_RESPONSE_NOT_RECEIVED ((sl_status_t)0x1BBDC)
Expected 23X response from the FTP server was not received.
#define
SL_STATUS_SI91X_FTP_EXPECTED_3XX_RESPONSE_NOT_RECEIVED ((sl_status_t)0x1BBDD)
Expected 3XX response from the FTP server was not received.
#define
SL_STATUS_SI91X_FTP_EXPECTED_33X_RESPONSE_NOT_RECEIVED ((sl_status_t)0x1BBDE)
Expected 33X response from the FTP server was not received.
#define
SL_STATUS_SI91X_HTTP_TIMEOUT ((sl_status_t)0x1BBE1)
#define
SL_STATUS_SI91X_HTTP_FAILED ((sl_status_t)0x1BBE2)
#define
SL_STATUS_SI91X_HTTP_PUT_CLIENT_TIMEOUT ((sl_status_t)0x1BBE7)
HTTP PUT client request timed out.
#define
SL_STATUS_SI91X_AUTHENTICATION_ERROR ((sl_status_t)0x1BBEB)
Authentication process failed.
#define
SL_STATUS_SI91X_INVALID_PACKET_LENGTH ((sl_status_t)0x1BBED)
Invalid packet length. Content length and received data length mismatch.
#define
SL_STATUS_SI91X_SERVER_RESPONDS_BEFORE_REQUEST_COMPLETE ((sl_status_t)0x1BBEF)
Server responds before HTTP client request is complete.
#define
SL_STATUS_SI91X_HTTP_PASSWORD_TOO_LONG ((sl_status_t)0x1BBF0)
HTTP/HTTPS password is too long.
#define
SL_STATUS_SI91X_MQTT_PING_TIMEOUT ((sl_status_t)0x1BBF1)
#define
SL_STATUS_SI91X_MQTT_COMMAND_SENT_IN_INCORRECT_STATE ((sl_status_t)0x1BBF2)
MQTT command sent in incorrect state.
#define
SL_STATUS_SI91X_MQTT_ACK_TIMEOUT ((sl_status_t)0x1BBF3)
#define
SL_STATUS_SI91X_POP3_INVALID_MAIL_INDEX ((sl_status_t)0x1BBFF)
POP3 error for invalid mail index.
#define
SL_STATUS_SI91X_FW_UPDATE_DONE ((sl_status_t)0x1DD03)
Firmware update successful.
#define
SL_STATUS_SI91X_FW_UPDATE_FAILED ((sl_status_t)0x1DD04)
#define
SL_STATUS_SI91X_ALLOCATION_FAILED ((sl_status_t)0x1DD3D)
Memory allocation failed in NWP during firmware upgradation.
#define
SL_STATUS_SI91X_INSUFFICIENT_FLASH_MEMORY ((sl_status_t)0x1DD3E)
Insufficient space in NWP flash memory during firmware upgradation.
#define
SL_STATUS_SI91X_FW_UP_WRONG_PACKET_INFO ((sl_status_t)0x1DD40)
#define
SL_STATUS_SI91X_INVALID_LENGTH ((sl_status_t)0x1DD41)
All payload chunks length together can't be greater than total image size in header, during firmware upgradation.
#define
SL_STATUS_SI91X_AB_FALLBACK_NOT_ENABLED ((sl_status_t)0x1DD0A)
AB fall-back feature is not enabled.
#define
SL_STATUS_SI91X_LEGACY_OTA_FEATURE_NOT_SUPPORTED ((sl_status_t)0x1DD0B)
Legacy OTA feature is not supported for fw fallback.
#define
SL_STATUS_SI91X_INVALID_ERASE_LENGTH_OR_ADDRESS ((sl_status_t)0x1DD0C)
Invalid erase length or address specified for the operation for fw fallback.
#define
SL_STATUS_SI91X_INVALID_READ_OR_WRITE_REQUEST ((sl_status_t)0x1DD0D)
The read or write request is invalid or not supported for fw fallback.
#define
SL_STATUS_SI91X_INVALID_FLASH_RANGE ((sl_status_t)0x1DD0E)
The specified flash range is invalid or out of bounds for fw fallback.
#define
SL_STATUS_SI91X_FLASH_ADDRESS_OUT_OF_BOUNDARY ((sl_status_t)0x1DD0F)
The flash address is out of the allowable boundary for fw fallback.
#define
SL_STATUS_SI91X_INVALID_OPERATION_ON_NWP_ACTIVE_IMAGE ((sl_status_t)0x1DD10)
Operation attempted on an active NWP image which is not allowed for fw fallback.
#define
SL_STATUS_SI91X_MAX_INPUT_LENGTH_EXCEED_1K_SIZE ((sl_status_t)0x1DD11)
The input length exceeds the maximum allowed size of 1KB for fw fallback.
#define
SL_STATUS_SI91X_INVALID_FW_ROLLBACK_SUBCOMMAND ((sl_status_t)0x1DD12)
The sub-command for firmware fallback is invalid.
#define
SL_STATUS_SI91X_INVALID_CONFIG_FOR_FW_ROLLBACK ((sl_status_t)0x1DD13)
The configuration for firmware fallback is invalid, applicable for 8MB SoC common-flash.
#define
SL_STATUS_SI91X_FW_DOWNGRADE_NOT_ALLOWED ((sl_status_t)0x1DD14)
The NWP firmware downgrade is not allowed for fw fallback.
#define
SL_STATUS_SI91X_ANTIROLLBACK_IS_NOT_ENABLED ((sl_status_t)0x1DD15)
Anti-rollback feature is not enabled for firmware fallback.
#define
SL_STATUS_SI91X_INVALID_REQUEST_TO_LOAD_QSPI_KEYS ((sl_status_t)0x1DD16)
Invalid request to load QSPI keys for fw fallback.
#define
SL_STATUS_SI91X_INVALID_OPERATION_ON_M4_UPDATER_IMAGE ((sl_status_t)0x1DD17)
Invalid operation on M4 updater image for fw fallback.
#define
SL_SI91X_DEVICE_AND_OTA_IMAGE_SECURITY_MISMATCH ((sl_status_t)0x1DD18)
Device security and OTA image security mismatch for fw fallback.
#define
SL_STATUS_SI91X_FW_UP_CORRUPTED_RPS_HEADER ((sl_status_t)0x1DD49)
Corrupted RPS header encountered or Received empty RPS file(no data) during firmware update.
#define
SL_STATUS_SI91X_SOCKET_NOT_CONNECTED ((sl_status_t)0x1FFFF)
Listening TCP socket in device is not connected to the remote peer, or the LTCP socket is not yet opened in the device.
#define
SL_STATUS_SI91X_SOCKET_LIMIT_EXCEEDED ((sl_status_t)0x1FFFE)
Socket limit exceeded. More than 10 sockets opened.
#define
SL_STATUS_SI91X_HTTP_OTAF_INVALID_PACKET ((sl_status_t)0x1FFFD)
HTTP OTAF invalid packet.
#define
SL_STATUS_SI91X_TCP_IP_INIT_FAILED ((sl_status_t)0x1FFFC)
TCP/IP initialization failed.
#define
SL_STATUS_SI91X_CONCURRENT_IP_CREATION_ERROR ((sl_status_t)0x1FFFB)
Cannot create IP in same interface in concurrent mode.
#define
SL_STATUS_SI91X_HTTP_OTAF_INCOMPLETE_PACKET ((sl_status_t)0x1FFF4)
HTTP OTAF incomplete packet.
#define
SL_STATUS_SI91X_INVALID_STORE_CONFIGURATION_PROFILE ((sl_status_t)0x1FFF5)
Invalid or mismatched store configuration profile type.
#define
SL_STATUS_SI91X_MQTT_REMOTE_TERMINATE_ERROR ((sl_status_t)0x1FFF6)
MQTT remote terminate error.
#define
SL_STATUS_SI91X_MQTT_KEEP_ALIVE_TERMINATE_ERROR ((sl_status_t)0x1BBF1)
MQTT remote terminate error due to keep-alive response timeout.
#define
SL_STATUS_SI91X_BYTE_STUFFING_ERROR_IN_AT_MODE ((sl_status_t)0x1FFF7)
Byte stuffing error in AT mode.
#define
SL_STATUS_SI91X_INVALID_COMMAND_OR_OPERATION ((sl_status_t)0x1FFF8)
Invalid command (e.g. parameters insufficient or invalid in the command). Invalid operation (for example, power save command with the same mode given twice, accessing wrong socket, creating more than allowed sockets ).
#define
SL_STATUS_SI91X_HTTP_OTAF_NO_PACKET ((sl_status_t)0x1FFF9)
HTTP OTAF no packet received.
#define
SL_STATUS_SI91X_TCP_SOCKET_NOT_CONNECTED ((sl_status_t)0x1FFFA)
TCP socket is not connected.
#define
SL_STATUS_SI91X_MAX_STATION_COUNT_EXCEEDED ((sl_status_t)0x1FFC5)
Station count exceeded the maximum supported stations.
#define
SL_STATUS_SI91X_UNABLE_TO_SEND_TCP_DATA ((sl_status_t)0x1FFC4)
#define
SL_STATUS_SI91X_SOCKET_BUFFER_TOO_SMALL ((sl_status_t)0x1FFBC)
#define
SL_STATUS_SI91X_INVALID_CONTENT_IN_DNS_RESPONSE ((sl_status_t)0x1FFBB)
Invalid content in the DNS response to the DNS resolution query.
#define
SL_STATUS_SI91X_DNS_CLASS_ERROR_IN_DNS_RESPONSE ((sl_status_t)0x1FFBA)
DNS class error in response to the DNS resolution query.
#define
SL_STATUS_SI91X_DNS_COUNT_ERROR_IN_DNS_RESPONSE ((sl_status_t)0x1FFB8)
DNS count error in response to the DNS resolution query.
#define
SL_STATUS_SI91X_DNS_RETURN_CODE_ERROR_IN_DNS_RESPONSE ((sl_status_t)0x1FFB7)
DNS return code error in the response to the DNS resolution query.
#define
SL_STATUS_SI91X_DNS_OPCODE_ERROR_IN_DNS_RESPONSE ((sl_status_t)0x1FFB6)
DNS Opcode error in the response to the DNS resolution query.
#define
SL_STATUS_SI91X_DNS_ID_MISMATCH ((sl_status_t)0x1FFB5)
DNS id mismatch between the DNS resolution request and response.
#define
SL_STATUS_SI91X_INVALID_INPUT_IN_DNS_QUERY ((sl_status_t)0x1FFAB)
Invalid input provided in the DNS resolution query.
#define
SL_STATUS_SI91X_DNS_RESPONSE_TIMEOUT ((sl_status_t)0x1FF42)
DNS response was timed out.
#define
SL_STATUS_SI91X_ARP_REQUEST_FAILURE ((sl_status_t)0x1FFA1)
#define
SL_STATUS_SI91X_UNABLE_TO_UPDATE_TCP_WINDOW ((sl_status_t)0x1FF91)
Failed to update TCP window.
#define
SL_STATUS_SI91X_DHCP_LEASE_EXPIRED ((sl_status_t)0x1FF9D)
#define
SL_STATUS_SI91X_DHCP_HANDSHAKE_FAILURE ((sl_status_t)0x1FF9C)
#define
SL_STATUS_SI91X_WEBSOCKET_CREATION_FAILED ((sl_status_t)0x1FF88)
WebSocket creation failed.
#define
SL_STATUS_SI91X_TRYING_TO_CONNECT_NON_EXISTENT_TCP_SERVER_SOCKET ((sl_status_t)0x1FF87)
Attempted to connect to a non-existent TCP server socket on the remote side.
#define
SL_STATUS_SI91X_TRYING_TO_CLOSE_NON_EXISTENT_SOCKET ((sl_status_t)0x1FF86)
Attempted to close a non-existent or invalid socket descriptor.
#define
SL_STATUS_SI91X_INVALID_SOCKET_PARAMETERS ((sl_status_t)0x1FF85)
The provided socket parameters are invalid.
#define
SL_STATUS_SI91X_FEATURE_NOT_AVAILABLE ((sl_status_t)0x1FF82)
The requested feature is not supported.
#define
SL_STATUS_SI91X_SOCKET_ALREADY_OPEN ((sl_status_t)0x1FF81)
The socket is already open.
#define
SL_STATUS_SI91X_MAX_SOCKETS_EXCEEDED ((sl_status_t)0x1FF80)
Attempted to open more than the maximum allowed number of sockets.
#define
SL_STATUS_SI91X_DATA_LENGTH_EXCEEDS_MSS ((sl_status_t)0x1FF7E)
Data length exceeds the Maximum Segment Size (MSS).
#define
SL_STATUS_SI91X_IP_CONFLICT_ERROR ((sl_status_t)0x1FF75)
Device unable to configure IP address due to an IP conflict.
#define
SL_STATUS_SI91X_FEATURE_NOT_ENABLED ((sl_status_t)0x1FF74)
The requested feature is not enabled.
#define
SL_STATUS_SI91X_DHCP_SERVER_NOT_SET ((sl_status_t)0x1FF73)
DHCP server is not configured in AP mode.
#define
SL_STATUS_SI91X_AP_SET_REGION_PARAM_ERROR ((sl_status_t)0x1FF71)
Invalid parameters provided for the AP set region command.
#define
SL_STATUS_SI91X_SSL_TLS_NOT_SUPPORTED ((sl_status_t)0x1FF70)
SSL/TLS is not supported.
#define
SL_STATUS_SI91X_JSON_NOT_SUPPORTED ((sl_status_t)0x1FF6F)
JSON format is not supported.
#define
SL_STATUS_SI91X_INVALID_OPERATING_MODE ((sl_status_t)0x1FF6E)
The specified operating mode is invalid.
#define
SL_STATUS_SI91X_INVALID_SOCKET_CONFIG_PARAMS ((sl_status_t)0x1FF6D)
Invalid socket configuration parameters.
#define
SL_STATUS_SI91X_WEBSOCKET_CREATION_TIMEOUT ((sl_status_t)0x1FF6C)
Web socket creation timeout.
#define
SL_STATUS_SI91X_PARAM_MAX_VALUE_EXCEEDED ((sl_status_t)0x1FF6B)
Parameter exceeds the maximum allowed value.
#define
SL_STATUS_SI91X_SOCKET_READ_TIMEOUT ((sl_status_t)0x1FF6A)
The socket read operation timed out.
#define
SL_STATUS_SI91X_INVALID_COMMAND_SEQUENCE ((sl_status_t)0x1FF69)
The command sequence is invalid.
#define
SL_STATUS_SI91X_DNS_RESPONSE_TIMEOUT_ERROR ((sl_status_t)0x1FF42)
The DNS response timed out.
#define
SL_STATUS_SI91X_HTTP_SOCKET_CREATION_FAILED ((sl_status_t)0x1FF41)
Failed to create an HTTP socket.
#define
SL_STATUS_SI91X_HTTP_GET_CMD_IN_PROGRESS ((sl_status_t)0x10005)
An HTTP GET command is currently in progress.
#define
SL_STATUS_SI91X_TCP_CLOSE_BEFORE_RESPONSE_ERROR ((sl_status_t)0x1FF40)
TCP socket close command issued before receiving the response of the previous close command.
#define
SL_STATUS_SI91X_WAIT_ON_HOST_FEATURE_NOT_ENABLED ((sl_status_t)0x1FF36)
'Wait On Host' feature is not enabled.
#define
SL_STATUS_SI91X_STORE_CONFIG_CHECKSUM_INVALID ((sl_status_t)0x1FF35)
Store configuration checksum validation failed.
#define
SL_STATUS_SI91X_TCP_KEEP_ALIVE_TIMEOUT ((sl_status_t)0x1FF33)
TCP keep-alive timed out.
#define
SL_STATUS_SI91X_TCP_ACK_FAILED_FOR_SYN_ACK ((sl_status_t)0x1FF2D)
TCP ACK failed for TCP SYN-ACK.
#define
SL_STATUS_SI91X_MEMORY_LIMIT_EXCEEDED ((sl_status_t)0x1FF2C)
Memory limit exceeded in the given operating mode.
#define
SL_STATUS_SI91X_MEMORY_LIMIT_EXCEEDED_DURING_AUTO_JOIN ((sl_status_t)0x1FF2A)
Memory limit exceeded in the operating mode during auto join/create.
#define
SL_STATUS_SI91X_MDNS_COMMAND_NOT_SUPPORTED ((sl_status_t)0x1FF2B)
The MDNS command type is invalid.
#define
SL_STATUS_SI91X_CRYPTO_INVALID_SECURITY_MODE ((sl_status_t)0x1CC43)
Invalid security mode in SI91X crypto operations.
#define
SL_STATUS_SI91X_CRYPTO_ERR_DATA_ALIGNMENT_16BYTE ((sl_status_t)0x1CC92)
Input data is not 16-byte aligned (required for AES crypto operation).
#define
SL_STATUS_SI91X_CRYPTO_CMAC_DECRYPTION_NOT_SUPPORTED ((sl_status_t)0x1CC93)
CMAC decryption is not supported.
#define
SL_STATUS_SI91X_CRYPTO_INVALID_KEY_LENGTH ((sl_status_t)0x1CC94)
Invalid key length provided to a crypto operation.
#define
SL_STATUS_SI91X_CRYPTO_INVALID_LENGTH ((sl_status_t)0x1CC95)
Invalid input parameter length (e.g., for CCM operation).
#define
SL_STATUS_SI91X_CRYPTO_SHA_MODE_NOT_SUPPORTED ((sl_status_t)0x1CC96)
#define
SL_STATUS_SI91X_CRYPTO_INVALID_ECDSA_CURVE_ID ((sl_status_t)0x1CC97)
Invalid ECDSA curve identifier.
#define
SL_STATUS_SI91X_CRYPTO_INVALID_ECDH_TYPE ((sl_status_t)0x1CC98)
#define
SL_STATUS_SI91X_CRYPTO_INVALID_ECDSA_SUB_ALGORITHM ((sl_status_t)0x1CC99)
Invalid ECDSA sub-algorithm.
#define
SL_STATUS_SI91X_CRYPTO_OPERATION_FAILED ((sl_status_t)0x1CC9B)
Crypto operation failure.
#define
SL_STATUS_SI91X_CRYPTO_INVALID_SUB_ALGORITHM ((sl_status_t)0x1CC9C)
Invalid sub-algorithm selection.
#define
SL_STATUS_SI91X_CRYPTO_INVALID_ALGORITHM ((sl_status_t)0x1CC9D)
Invalid algorithm selection.
#define
SL_STATUS_SI91X_CRYPTO_INVALID_ECDH_MODE ((sl_status_t)0x1CC9E)
#define
SL_STATUS_SI91X_CRYPTO_INPUT_MSG_LENGTH_EXCEEDED ((sl_status_t)0x1CC9F)
Input message length exceeding the allowed maximum.
#define
SL_STATUS_SI91X_CRYPTO_DEVICE_SECURITY_IS_DISABLED ((sl_status_t)0x1CCA1)
Device security is disabled.
#define
SL_STATUS_SI91X_CRYPTO_INVALID_SIGNATURE ((sl_status_t)0x1CCC6)
Invalid signature or tag mismatch (e.g., authentication failure).
#define
SL_STATUS_SI91X_AUTO_JOIN_IN_PROGRESS ((sl_status_t)0x15A5A)
Auto join or user store configuration is in progress.
#define
SL_STATUS_SI91X_RSNIE_FROM_AP_INVALID ((sl_status_t)0x1FFE1)
Received an invalid RSNIE from the AP to the station.
#define
SL_STATUS_SI91X_SNTP_MAX_ATTEMPTS_REACHED ((sl_status_t)0x1FF5F)
Maximum number of invalid SNTP attempts reached.
#define
SL_STATUS_SI91X_FREQUENCY_OFFSET_ZER0 ((sl_status_t)0x100FC)
The frequency offset sent is zero.
#define
SL_STATUS_SI91X_FREQUENCY_OFFSET_OUT_OF_LIMITS ((sl_status_t)0x100FB)
Frequency offset specified goes beyond upper or lower limits and indicates that frequency offset cannot be changed further.
#define
SL_STATUS_SI91X_UNKNOWN_HCI_COMMAND (0x4E01)
#define
SL_STATUS_SI91X_UNKNOWN_CONNECTION_IDENTIFIER (0x4E02)
Unknown Connection Identifier.
#define
SL_STATUS_SI91X_HARDWARE_FAILURE (0x4E03)
#define
SL_STATUS_SI91X_PAGE_TIMEOUT (0x4E04)
#define
SL_STATUS_SI91X_AUTHENTICATION_FAILURE (0x4E05)
#define
SL_STATUS_SI91X_PIN_MISSING (0x4E06)
#define
SL_STATUS_SI91X_MEMORY_CAPACITY_EXCEED (0x4E07)
Memory capacity exceeded.
#define
SL_STATUS_SI91X_CONNECTION_TIMEOUT (0x4E08)
#define
SL_STATUS_SI91X_CONNECTION_LIMIT_EXCEED (0x4E09)
Connection limit exceeded.
#define
SL_STATUS_SI91X_SCO_LIMIT_EXCEED (0x4E0A)
#define
SL_STATUS_SI91X_ACL_CONNECTION_ALREADY_EXIST (0x4E0B)
ACL Connection already exists.
#define
SL_STATUS_SI91X_COMMAND_DISALLOWED (0x4E0C)
#define
SL_STATUS_SI91X_CONNECTION_REJECTED_LIMITED_RESOURCES (0x4E0D)
Connection rejected due to limited resources .
#define
SL_STATUS_SI91X_CONNECTION_REJECTED_SECURITY_REASONS (0x4E0E)
Connection rejected due to security reasons.
#define
SL_STATUS_SI91X_CONNECTION_REJECTED_FOR_BD_ADDR (0x4E0F)
Connection rejected for BD address.
#define
SL_STATUS_SI91X_CONNECTION_ACCEPT_TIMEOUT (0x4E10)
Connection accept timeout.
#define
SL_STATUS_SI91X_UNSUPPORTED_FEATURE_OR_PARAMETER (0x4E11)
Unsupported feature or parameter.
#define
SL_STATUS_SI91X_INVALID_HCI_COMMAND_PARAMETER (0x4E12)
Invalid HCI command parameter.
#define
SL_STATUS_SI91X_REMOTE_USER_TERMINATED_CONNECTION (0x4E13)
Remote user terminated connection.
#define
SL_STATUS_SI91X_REMOTE_DEVICE_TERMINATED_CONNECTION_LOW_RESOURCES (0x4E14)
Remote device terminated connection due to low resources .
#define
SL_STATUS_SI91X_REMOTE_DEVICE_TERMINATED_CONNECTION_POWER_OFF (0x4E15)
Remote device terminated connection due to power off .
#define
SL_STATUS_SI91X_LOCAL_DEVICE_TERMINATED_CONNECTION (0x4E16)
Local device terminated connection.
#define
SL_STATUS_SI91X_REPEATED_ATTEMPTS (0x4E17)
#define
SL_STATUS_SI91X_PAIRING_NOT_ALLOWED (0x4E18)
#define
SL_STATUS_SI91X_UNKNOWN_LMP_PDU (0x4E19)
#define
SL_STATUS_SI91X_UNSUPPORTED_REMOTE_FEATURE (0x4E1A)
Unsupported remote feature.
#define
SL_STATUS_SI91X_SCO_OFFSET_REJECTED (0x4E1B)
#define
SL_STATUS_SI91X_SCO_INTERVAL_REJECTED (0x4E1C)
#define
SL_STATUS_SI91X_SCO_AIR_MODE_REJECTED (0x4E1D)
#define
SL_STATUS_SI91X_INVALID_LMP_PARAMETERS (0x4E1E)
#define
SL_STATUS_SI91X_UNSPECIFIED (0x4E1F)
#define
SL_STATUS_SI91X_UNSUPPORTED_LMP_PARAMETER (0x4E20)
Unsupported LMP Parameter.
#define
SL_STATUS_SI91X_ROLE_CHANGE_NOT_ALLOWED (0x4E21)
#define
SL_STATUS_SI91X_LMP_RESPONSE_TIMEOUT (0x4E22)
#define
SL_STATUS_SI91X_LMP_TRANSACTION_COLLISION (0x4E23)
LMP transaction collision.
#define
SL_STATUS_SI91X_LMP_PDU_NOT_ALLOWED (0x4E24)
#define
SL_STATUS_SI91X_ENCRYPTION_MODE_NOT_ACCEPTABLE (0x4E25)
Encryption mode not acceptable.
#define
SL_STATUS_SI91X_LINK_KEY_CANNOT_CHANGE (0x4E26)
#define
SL_STATUS_SI91X_REQUESTED_QOS_NOT_SUPPORTED (0x4E27)
Requested QOS not supported.
#define
SL_STATUS_SI91X_INSTANT_PASSED (0x4E28)
#define
SL_STATUS_SI91X_PAIRING_WITH_UNIT_KEY_NOT_SUPPORTED (0x4E29)
Pairing with unit key not supported.
#define
SL_STATUS_SI91X_DIFFERENT_TRANSACTION_COLLISION (0x4E2A)
Different transaction collision.
#define
SL_STATUS_SI91X_RESERVED_1 (0x4E2B)
#define
SL_STATUS_SI91X_QOS_PARAMETER_NOT_ACCEPTABLE (0x4E2C)
QOS parameter not acceptable.
#define
SL_STATUS_SI91X_QOS_REJECTED (0x4E2D)
#define
SL_STATUS_SI91X_CHANNEL_CLASSIFICATION_NOT_SUPPORTED (0x4E2E)
Channel classification not supported.
#define
SL_STATUS_SI91X_INSUFFICIENT_SECURITY (0x4E2F)
#define
SL_STATUS_SI91X_PARAMETER_OUT_OF_MANDATORY_RANGE (0x4E30)
Parameter out of mandatory range.
#define
SL_STATUS_SI91X_RESERVED_2 (0x4E31)
#define
SL_STATUS_SI91X_ROLE_SWITCH_PENDING (0x4E32)
#define
SL_STATUS_SI91X_RESERVED_3 (0x4E33)
#define
SL_STATUS_SI91X_RESERVED_SLOT_VIOLATION (0x4E34)
#define
SL_STATUS_SI91X_ROLE_SWITCH_FAILED (0x4E35)
#define
SL_STATUS_SI91X_EXTENDED_INQUIRY_RESPONSE_TOO_LARGE (0x4E36)
Extended Inquiry Response too large.
#define
SL_STATUS_SI91X_EXTENDED_SECURE_SIMPLE_PAIRING_NOT_SUPPORTED (0x4E37)
Extended SSP not supported.
#define
SL_STATUS_SI91X_HOST_BUSY_PAIRING (0X4E38)
#define
SL_STATUS_SI91X_PINCODE_REPLY_FOR_WRONG_BD_ADDRESS (0x4E39)
#define
SL_STATUS_SI91X_CONNECTION_FAILED_ESTABLISHED (0x4E3E)
Connection Failed to be Establish.
#define
SL_STATUS_SI91X_INVALID_GAIN_TABLE_PAYLOAD_LENGTH (0x4F01)
Invalid Gain table payload length.
#define
SL_STATUS_SI91X_INVALID_REGION (0x4F02)
#define
SL_STATUS_SI91X_INVALID_GAIN_TABLE_OFFSET_REQUEST_TYPE (0x4F03)
Invalid Gain Table offset request type.
#define
SL_STATUS_SI91X_INVALID_NODE_ID (0x4F04)
#define
SL_STATUS_SI91X_BT_INVALID_COMMAND (0x4FF8)
#define
SL_STATUS_SI91X_INVALID_ARGS (0x0101)
#define
SL_STATUS_SI91X_UNKNOWN (0x0102)
#define
SL_STATUS_SI91X_FIRMWARE_TIMEOUT (0x0103)
#define
SL_STATUS_SI91X_MEMORY_ALLOC_FAIL (0x0104)
#define
SL_STATUS_SI91X_IO_FAIL (0x0106)
#define
SL_STATUS_SI91X_UNSUPPORTED (0x0108)
#define
SL_STATUS_SI91X_SHORT_BUF (0x0109)
#define
SL_STATUS_SI91X_BUF_OVERFLOW (0x010A)
#define
SL_STATUS_SI91X_TOO_LARGE_BUF (0x010B)
#define
SL_STATUS_SI91X_I_O_ABORT (0x010C)
#define
SL_STATUS_SI91X_OPEN_FAIL (0x010D)
#define
SL_STATUS_SI91X_OS_TASK_INVALID_PRIORITY (0x1010)
OS task invalid priority.
#define
SL_STATUS_SI91X_OS_TASK_PRIO_EXISTS (0x1011)
#define
SL_STATUS_SI91X_OS_TASK_NOT_STOPPED (0x1012)
#define
SL_STATUS_SI91X_OS_SEM_MAX_VALUE (0x1020)
#define
SL_STATUS_SI91X_OS_SEM_NOT_AVAILABLE (0x1021)
#define
SL_STATUS_SI91X_OS_SEM_RESET (0x1022)
#define
SL_STATUS_SI91X_OS_MUTEX_NOT_OWNER (0x1030)
#define
SL_STATUS_SI91X_OS_MUTEX_NOT_LOCKED (0x1031)
#define
SL_STATUS_SI91X_OS_MUTEX_LOCK_FAILED (0x1032)
#define
SL_STATUS_SI91X_OS_MUTEX_TRY_LOCK_FAILED (0x1033)
OS mutex try lock failed.
#define
SL_STATUS_SI91X_OS_MSG_QUEUE_FULL (0x1040)
#define
SL_STATUS_SI91X_OS_MESSAGE_QUEUE_EMPTY (0x1041)
#define
SL_STATUS_SI91X_PIPE_EMPTY (0x1050)
#define
SL_STATUS_SI91X_PIPE_FULL (0x1051)
#define
SL_STATUS_SI91X_INVALID_LEN (0x1052)
#define
SL_STATUS_SI91X_PIPE_READ_IN_USE (0x1053)
#define
SL_STATUS_SI91X_PIPE_WRITE_IN_USE (0x1054)
#define
SL_STATUS_SI91X_OS_TIMER_EXPIRED (0x1060)
#define
SL_STATUS_SI91X_OS_TIMER_STATE_RUNNING (0x1061)
#define
SL_STATUS_SI91X_OS_CANNOT_WAIT (0x1070)
#define
SL_STATUS_SI91X_OS_MEM_POOL_EMPTY (0x1080)
#define
SL_STATUS_SI91X_OS_MEM_POOL_SIZE_SHORT (0x1081)
#define
SL_STATUS_SI91X_ERR_BT_INVALID_ARGS (0x4046)
#define
SL_STATUS_SI91X_DIRECTED_ADVERTISING_TIMEOUT (0x4E3C)
Directed Advertising Timeout.
#define
SL_STATUS_SI91X_CONNECTION_TERMINATED_DUE_TO_MIC_FAILURE (0x4E3D)
Connection terminated due to MIC failure.
#define
SL_STATUS_SI91X_INVALID_HANDLE_RANGE (0x4E60)
#define
SL_STATUS_SI91X_MEMORY_IS_NOT_SUFFICIENT (0x4E61)
Memory is not sufficient.
#define
SL_STATUS_SI91X_INVALID_PARAMETERS (0x4E62)
#define
SL_STATUS_SI91X_BLE_BUFFER_COUNT_EXCEEDED (0x4E63)
BLE Buffer Count Exceeded.
#define
SL_STATUS_SI91X_BLE_BUFFER_ALREADY_IN_USE (0x4E64)
BLE Buffer already in use.
#define
SL_STATUS_SI91X_INVALID_ATTRIBUTE_LENGTH (0x4E65)
Invalid Attribute Length When Small Buffer Mode is Configured.
#define
SL_STATUS_SI91X_INVALID_NAME_LENGTH (0x4E66)
Invalid Name length when set to more than 16 bytes.
#define
SL_STATUS_SI91X_INVALID_HANDLE (0x4A01)
#define
SL_STATUS_SI91X_READ_NOT_PERMITTED (0x4A02)
#define
SL_STATUS_SI91X_WRITE_NOT_PERMITTED (0x4A03)
#define
SL_STATUS_SI91X_INVALID_PDU (0x4A04)
#define
SL_STATUS_SI91X_INSUFFICIENT_AUTHENTICATION (0x4A05)
Insufficient authentication.
#define
SL_STATUS_SI91X_REQUEST_NOT_SUPPORTED (0x4A06)
#define
SL_STATUS_SI91X_INVALID_OFFSET (0x4A07)
#define
SL_STATUS_SI91X_INSUFFICIENTA_UTHORIZATION (0x4A08)
Insufficient authorization.
#define
SL_STATUS_SI91X_PREPARE_QUEUE_FULL (0x4A09)
#define
SL_STATUS_SI91X_ATTRIBUTE_NOT_FOUND (0x4A0A)
#define
SL_STATUS_SI91X_ATTRIBUTE_NOT_LONG (0x4A0B)
#define
SL_STATUS_SI91X_INSUFFICIENT_ENCRYPTION_KEY_SIZE (0x4A0C)
Insufficient encryption key size.
#define
SL_STATUS_SI91X_INVALID_ATTRIBUTE_VALUE_LENGTH (0x4A0D)
Invalid attribute value length.
#define
SL_STATUS_SI91X_UNLIKELY_ERROR (0x4A0E)
#define
SL_STATUS_SI91X_INSUFFICIENT_ENCRYPTION (0x4A0F)
#define
SL_STATUS_SI91X_UNSUPPORTED_GROUP_TYPE (0x4A10)
#define
SL_STATUS_SI91X_INSUFFICIENT_RESOURCES (0x4A11)
#define
SL_STATUS_SI91X_GATT_TIMEOUT (0x4A80)
#define
SL_STATUS_SI91X_DATA_MAINTAINED_IN_HOST (0x4AFF)
#define
SL_STATUS_SI91X_SMP_PASSKEY_ENTRY_FAILED (0x4B01)
SMP Passkey entry failed.
#define
SL_STATUS_SI91X_SMP_OOB_NOT_AVAILABLE (0x4B02)
#define
SL_STATUS_SI91X_SMP_AUTHENTICATION_REQUIREMENTS (0x4B03)
SMP Authentication Requirements.
#define
SL_STATUS_SI91X_SMP_CONFIRM_VALUE_FAILED (0x4B04)
SMP confirm value failed.
#define
SL_STATUS_SI91X_SMP_PAIRING_NOT_SUPPORTED (0x4B05)
SMP Pairing not supported.
#define
SL_STATUS_SI91X_SMP_ENCRYPTION_KEY_SIZE_INSUFFICIENT (0x4B06)
SMP Encryption key size insufficient.
#define
SL_STATUS_SI91X_SMP_COMMAND_NOT_SUPPORTED (0x4B07)
SMP command not supported.
#define
SL_STATUS_SI91X_SMP_PAIRING_FAILED (0x4B08)
#define
SL_STATUS_SI91X_SMP_REPEATED_ATTEMPTS (0x4B09)
#define
SL_STATUS_SI91X_SMP_INVALID_PARAMETERS (0x4B0A)
#define
SL_STATUS_SI91X_SMP_DH_KEY_CHECK_FAILED (0x4B0B)
#define
SL_STATUS_SI91X_SMP_NUMERIC_COMPARISON_FAILED (0x4B0C)
SMP Numeric Comparison Failed.
#define
SL_STATUS_SI91X_SMP_INVALID_KEYS_GENERATED (0x4BFD)
SMP Invalid Keys Generated.
#define
SL_STATUS_SI91X_SMP_IDENTICAL_PUBLIC_KEY (0x4BFE)
SMP Identical Public Key.
#define
SL_STATUS_SI91X_PSM_CONN_FAILED (0x4C02)
#define
SL_STATUS_SI91X_BLE_REMOTE_DEVICE_FOUND (0x4D00)
#define
SL_STATUS_SI91X_BLE_REMOTE_DEVICE_NOT_FOUND (0x4D01)
BLE Remote device not found.
#define
SL_STATUS_SI91X_BLE_REMOTE_DEVICE_STRUCTURE_FULL (0x4D02)
BLE Remote device structure full.
#define
SL_STATUS_SI91X_UNABLE_TO_CHANGE_STATE (0x4D03)
#define
SL_STATUS_SI91X_BLE_NOT_CONNECTED (0x4D04)
#define
SL_STATUS_SI91X_BLE_SOCKET_NOT_AVAILABLE (0x4D05)
BLE socket not available.
#define
SL_STATUS_SI91X_ATTRIBUTE_RECORD_NOT_FOUND (0x4D06)
Attribute record not found.
#define
SL_STATUS_SI91X_ATTRIBUTE_ENTRY_NOT_FOUND (0x4D07)
Attribute entry not found.
#define
SL_STATUS_SI91X_PROFILE_RECORD_FULL (0x4D08)
#define
SL_STATUS_SI91X_ATTRIBUTE_RECORD_FULL (0x4D09)
#define
SL_STATUS_SI91X_BLE_PROFILE_HANDLER_INVALID (0x4D0A)
BLE profile not found(profile handler invalid).
#define
SL_STATUS_SI91X_BLE_ATTRIBUTE_BUFFER_FULL (0x4D0B)
BLE Attribute Buffer Full .
#define
SL_STATUS_SI91X_BLE_CONNECTION_SOCK_NOT_AVAILABLE (0x4D10)
BLE Connection Sock not Available.
#define
SL_STATUS_SI91X_BLE_REMOTE_CREDITS_NOT_AVAILABLE (0x4D11)
BLE Remote Credits not Available.
#define
SL_STATUS_SI91X_PARAMETER_OUTOFF_MANADATORY_RANGE (0x4D14)
Parameter is outoff the manadatory range.
#define
SL_STATUS_SI91X_ERROR_BLE_HW_BUF_OVERFLOW (0x4D16)
Sufficient buffers are not available in TA.
#define
SL_STATUS_SI91X_ERROR_BLE_SAPI_CMD_NOT_ALLOWED (0x4D17)
SAPI command not allowed when Stack Bypass feature is enabled.