Wi-Fi Scan and Connect Initialization and Configuration#

This section describes how to initialize the Wi-Fi subsystem and bring up the interface before performing scans or connections. It covers the startup sequence and prerequisites for scan and connect operations.

This section also describes the main configuration structures and options for Wi-Fi scanning and connection. These structures are typically filled by the application and passed to the scan and connect APIs.

For detailed information on how these parameters affect scan duration, connection latency, roaming behaviour, and power consumption, see Scan and Connect Parameter Tuning.

Startup Sequence#

When the application starts, the Wi-Fi stack must be initialized and the client interface brought up before any scan or connect operation. The following flowchart illustrates the startup sequence.

Startup sequenceStartup sequence

  1. Initialize WiFi – Call sl_wifi_init. This initializes the Wi-Fi subsystem and network processor (NWP).

  2. Check interface – Call sl_wifi_is_interface_up(SL_WIFI_CLIENT_2_4GHZ_INTERFACE) (or the interface you use) — see sl_wifi_is_interface_up.

  3. Bring interface up if needed – If the interface is not up, call sl_wifi_set_interface_up(SL_WIFI_CLIENT_2_4GHZ_INTERFACE) — see sl_wifi_set_interface_up.

  4. Optional: Configure scan timeouts – Configure scan channel timeouts based on application requirements: To set global scan timeouts before init, use sl_si91x_set_timeout before sl_wifi_init. To configure timeouts after init, use sl_wifi_configure_timeout.

Prerequisites for Scanning and Connection#

Before using Wi-Fi scan or connect APIs:

Initialization Example#

#include "sl_wifi.h"

void wifi_init_sequence(void)
{
  sl_status_t status = sl_wifi_init();
  if (status != SL_STATUS_OK) {
    // Handle initialization failure
    return;
  }

  sl_wifi_interface_t interface = SL_WIFI_CLIENT_2_4GHZ_INTERFACE;
  if (!sl_wifi_is_interface_up(interface)) {
    status = sl_wifi_set_interface_up(interface);
    if (status != SL_STATUS_OK) {
      // Handle interface bring-up failure
      return;
    }
  }

  // Wi-Fi is ready for scan and connect operations
}

Note:

  • Client interfaces: SL_WIFI_CLIENT_2_4GHZ_INTERFACE, SL_WIFI_CLIENT_5GHZ_INTERFACE – used to connect to access points.

  • AP interface: SL_WIFI_AP_INTERFACE – used when the device operates as an access point. Scanning in AP mode is supported only as Active scan after sl_wifi_start_ap is called.

Use the client interface for typical scan-and-connect flows.

Configuration Overview#

The following diagram shows where each configuration type is used in the scan and connect flow.

Configuration overviewConfiguration overview

Scan Configuration#

sl_wifi_scan_configuration_t#

Field

Description

type

SL_WIFI_SCAN_TYPE_ACTIVE, PASSIVE, EXTENDED, or ADV_SCAN.

channel_bitmap_2g4

2.4 GHz channels (bits 0–13 = channels 1–14). Use 0 for all channels.

periodic_scan_interval

For Advanced scan only: interval in milliseconds between periodic scan cycles.

lp_mode

1 = enable low-power mode for passive scan.

flags

Reserved; set to 0.

channel_bitmap_5g

5 GHz; not supported; set to 0.

Default: use default_wifi_scan_configuration and set type and other fields as needed.

sl_wifi_advanced_scan_configuration_t#

Used for channel times (all scan types) and for Advanced-scan-specific parameters:

Field

Description

active_channel_time

Dwell time per channel for active scan (ms). Default 100. Used for standard and internal scans.

passive_channel_time

Dwell time per channel for passive scan (ms). Advanced scan only; default 400.

trigger_level

RSSI (dBm) below which Advanced scan triggers. Advanced scan only.

trigger_level_change

RSSI delta (dB) that triggers background scan when connected RSSI drops by this amount. Advanced scan only.

enable_instant_scan

1 = start Advanced scan immediately and deliver one result set. Advanced scan only.

enable_multi_probe

Advanced scan only; multiple probes.

Configure with sl_wifi_set_advanced_scan_configuration before starting a scan or before calling sl_wifi_connect if you want to influence internal scan channel time.

Timeout Configuration#

Global timeouts#

Use sl_wifi_timeout_t with sl_si91x_set_timeout. Must be called before sl_wifi_init.

  • active_chan_scan_timeout_value – Active scan channel time (ms).

  • passive_scan_timeout_value – Passive scan channel time (ms).

Per-timeout#

Use sl_si91x_configure_timeout with:

  • SL_SI91X_CHANNEL_ACTIVE_SCAN_TIMEOUT – Active channel time (ms).

  • SL_SI91X_CHANNEL_PASSIVE_SCAN_TIMEOUT – Passive channel time (ms).

Extended Scan Result Filters#

When calling sl_wifi_get_stored_scan_results, use sl_wifi_extended_scan_result_parameters_t:

  • scan_results – Array to store results.

  • array_length – Size of array.

  • result_count – Output: number of results.

  • channel_filter – Optional; filter by channel.

  • rssi_filter – Optional; minimum RSSI (dBm).

  • security_mode_filter – Optional; filter by security.

  • network_type_filter – Optional; filter by network type.

Set filter pointers to NULL to disable filtering.

Scan Transmit Power#

Use sl_wifi_set_max_tx_power with sl_wifi_max_tx_power_t:

  • scan_tx_power – Transmit power during scan (1–31 dBm). Applies to all scans.

  • join_tx_power – Transmit power during join (1–31 dBm).

Optional: Global Scan Timeout#

If you need to set global active and passive scan channel times before Wi-Fi init:

sl_wifi_timeout_t timeout_config = {
  .active_chan_scan_timeout_value  = 150,   // ms
  .passive_scan_timeout_value      = 500,   // ms
  .auth_assoc_timeout_value        = SL_WIFI_DEFAULT_AUTH_ASSOCIATION_TIMEOUT,
  .keep_alive_timeout_value       = SL_WIFI_DEFAULT_KEEP_ALIVE_TIMEOUT
};
sl_si91x_set_timeout(&timeout_config);

// Then initialize WiFi
sl_wifi_init();

Note: sl_si91x_set_timeout must be called before sl_wifi_init. To change scan timeouts after init, use sl_si91x_configure_timeout with SL_SI91X_CHANNEL_ACTIVE_SCAN_TIMEOUT or SL_SI91X_CHANNEL_PASSIVE_SCAN_TIMEOUT.

Connect Configuration#

sl_wifi_client_configuration_t#

Field

Required

Description

ssid

Yes

Target network SSID.

security

Yes

Security type (WPA, WPA2, WPA3, Enterprise, OPEN).

credential_id

Yes*

Credential ID; use SL_NET_NO_CREDENTIAL_ID for open.

channel

No

Specific channel.

bssid

No

AP MAC; requires SL_WIFI_JOIN_FEAT_BSSID_BASED.

channel_bitmap

No

Limits internal scan to selected channels. Set channel_bitmap.channel_bitmap_2_4 for 2.4 GHz (same bit layout as scan channel_bitmap_2g4).

encryption

No

Default SL_WIFI_DEFAULT_ENCRYPTION.

bss_type

No

Not currently supported; infrastructure is used.

client_options

No

Not currently supported.

* Required for secured networks.

Join Feature Bitmap#

Configure join behavior with sl_wifi_set_join_configuration:

  • SL_WIFI_JOIN_FEAT_LISTEN_INTERVAL_VALID – Use listen interval from join (default).

  • SL_WIFI_JOIN_FEAT_QUICK_JOIN – Quick join; scan_interval in advanced client config is not used.

  • SL_WIFI_JOIN_FEAT_BSSID_BASED – Required when connecting by BSSID.

  • SL_WIFI_JOIN_FEAT_MFP_CAPABLE_ONLY / SL_WIFI_JOIN_FEAT_MFP_CAPABLE_REQUIRED – MFP behavior.

Use sl_wifi_set_listen_interval_v2 when the listen interval is taken from the join command.

Advanced Client Configuration#

Use sl_wifi_set_advanced_client_configuration to set:

  • max_retry_attempts – Retries after first connection (0 = forever, 20 = default).

  • beacon_missed_count – Missed beacons before triggering rejoin (e.g., 40).

  • scan_interval – Active scan interval in seconds during rejoin (ignored if quick join is enabled).

  • first_time_retry_enable – Retry on first join failure.

Configure before connecting so that initial connection and rejoin use the desired behavior.

Connection with BSSID#

When connecting to a specific AP by MAC address:

  1. Set access_point.bssid to the AP MAC.

  2. Set join feature bitmap to include SL_WIFI_JOIN_FEAT_BSSID_BASED and call sl_wifi_set_join_configuration.

  3. Call sl_wifi_connect.

Without the BSSID join feature flag, the BSSID in the join command may be ignored.