Socket Configuration#
This section provides a reference for the socket configuration API functions.
These functions enable various socket-related configurations, including ciphers used for secure communication.
Modules#
sl_si91x_socket_type_length_value_t
SiWx91x Socket Extended Ciphers
Functions#
Configures SiWx91x specific socket settings.
Sets the list of standard TLS ciphers (TLSv1.0 / TLSv1.1 / TLSv1.2) to be used when creating secure sockets on the SiWx91x.
Sets the list of extended TLS ciphers (including TLSv1.3) to be used when creating secure sockets on the SiWx91x.
Function Documentation#
sl_si91x_config_socket#
sl_status_t sl_si91x_config_socket (sl_si91x_socket_config_t socket_config)
Configures SiWx91x specific socket settings.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_si91x_socket_config_t | [in] | socket_config | Socket configuration of type sl_si91x_socket_config_t. Field values must satisfy the constraints documented in sl_si91x_socket_config_t (for example, |
This function sets up the socket configuration specific to the SiWx91x. It must be called before invoking any socket-creation API. The configuration includes setting parameters such as socket type, protocol, and other options specific to the SiWx91x series.
Applies to all socket families. The configuration values (TCP/UDP/TLS slot counts, MSS, RX/TX buffer sizes, TLS extensions) are applied to the underlying SiWx91x network stack and therefore affect all three socket families — BSD sockets (socket), IoT sockets (iotSocketCreate), and native SiWx91x sockets (sl_si91x_socket / sl_si91x_socket_async) — because they share the same firmware resources.
Pre-conditions:
The Wi-Fi/Net stack must be initialized.
This API must be called before creating any socket using socket, iotSocketCreate, sl_si91x_socket, or sl_si91x_socket_async.
Post-conditions:
On success the supplied configuration is applied to the SiWx91x socket pool and all subsequent socket-creation calls (regardless of family) observe the new limits.
On failure the firmware configuration is unchanged.
Returns
sl_status_t. See https://docs.silabs.com/gecko-platform/latest/platform-common/status for details.
Return values
SL_STATUS_OK: Configuration applied successfully.
SL_STATUS_NOT_INITIALIZED: Wi-Fi/Net stack is not initialized.
SL_STATUS_INVALID_PARAMETER: One of the fields in
SL_STATUS_SI91X_INVALID_CONFIG: Firmware rejected the configuration (for example, MSS/buffer sizes out of range).
SL_STATUS_BUSY: A previous socket-configuration request is still in progress.
Note
Thread safety:
Not thread-safe. Must be invoked by a single thread at initialization time, before any socket is created.
Side effects:
Allocates/releases firmware buffers used by the SiWx91x socket pool.
Affects every subsequent socket-creation call across BSD, IoT, and SiWx91x families.
See Also
Example
Example#
Configure the SiWx91x socket pool before creating application sockets:
sl_si91x_socket_config_t socket_cfg = { .total_sockets = 3, .total_tcp_sockets = 2, .total_udp_sockets = 1, .tcp_tx_only_sockets = 1, .tcp_rx_only_sockets = 1, .udp_tx_only_sockets = 1, .udp_rx_only_sockets = 0, .tcp_rx_high_performance_sockets = 1, .tcp_rx_window_size_cap = 10, .tcp_rx_window_div_factor = 0, }; sl_status_t status = sl_si91x_config_socket(socket_cfg); if (status != SL_STATUS_OK) { printf("sl_si91x_config_socket() failed, 0x%lx\r\n", (unsigned long)status); return status; }
sl_si91x_set_socket_cipherlist#
void sl_si91x_set_socket_cipherlist (uint32_t cipher_list)
Sets the list of standard TLS ciphers (TLSv1.0 / TLSv1.1 / TLSv1.2) to be used when creating secure sockets on the SiWx91x.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | cipher_list | A bitmap of the selected ciphers from SiWx91x Socket Ciphers. Multiple ciphers can be OR-ed together. |
This function stores the cipher-suite bitmap in an internal global (sl_si91x_socket_selected_ciphers). When a secure socket is subsequently created, the SiWx91x socket layer copies this bitmap into the socket-create command sent to the firmware (see ssl_ciphers_bitmap in sli_create_and_send_socket_request()), and the firmware uses it during the TLS handshake.
Applicability by socket family#
BSD sockets (socket) — Applies whenever TLS is enabled on the socket (e.g., via setsockopt with the SiWx91x TLS option before connect). This is the primary use case.
SiWx91x (proprietary) sockets (sl_si91x_socket, sl_si91x_socket_async) — Applies whenever TLS is enabled on the socket.
IoT sockets (iotSocketCreate) — The IoT Socket API surface itself does not expose TLS enablement (
iotSocketCreateaccepts onlyIOT_SOCKET_IPPROTO_TCP/IOT_SOCKET_IPPROTO_UDP, andiotSocketSetOpthas no TLS options). The cipher configuration therefore has no effect on a pure IoT-Socket-API usage.
Pre-conditions:
The Wi-Fi / network stack must be initialized.
Must be called before creating the secure socket(s) that need to use the selected ciphers. Existing secure sockets are not updated retroactively.
Post-conditions:
The supplied cipher bitmap is stored and applied to every secure socket created afterwards until the cipher list is changed again.
Note
Thread safety: Not thread-safe — the cipher list is held in an unsynchronized process-global. Call once from an initialization thread before any secure socket is created.
For TLSv1.3 ciphers use sl_si91x_set_extended_socket_cipherlist.
See Also
sl_si91x_set_extended_socket_cipherlist, sl_si91x_config_socket, socket, sl_si91x_socket, sl_si91x_socket_async
Example
Example#
Select a set of TLSv1.2 ciphers for every subsequent secure socket (BSD or SiWx91x family):
sl_si91x_set_socket_cipherlist(BIT(SL_SI91X_TLS_RSA_WITH_AES_256_CBC_SHA256) | BIT(SL_SI91X_TLS_RSA_WITH_AES_128_CBC_SHA256));
sl_si91x_set_extended_socket_cipherlist#
void sl_si91x_set_extended_socket_cipherlist (uint32_t extended_cipher_list)
Sets the list of extended TLS ciphers (including TLSv1.3) to be used when creating secure sockets on the SiWx91x.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | extended_cipher_list | A bitmap of the selected extended ciphers from SiWx91x Socket Extended Ciphers. Multiple ciphers can be OR-ed together. |
This function stores the extended cipher-suite bitmap in an internal global (sl_si91x_socket_selected_extended_ciphers). When a secure socket is subsequently created, the SiWx91x socket layer copies this bitmap into the socket-create command sent to the firmware (see ssl_ext_ciphers_bitmap in sli_create_and_send_socket_request(), under SLI_SI917), and the firmware uses it during the TLS handshake. Extended ciphers include the TLSv1.3 suites and other suites not covered by sl_si91x_set_socket_cipherlist.
Applicability by socket family#
BSD sockets (socket) — Applies whenever TLS is enabled on the socket. Primary use case.
SiWx91x (proprietary) sockets (sl_si91x_socket, sl_si91x_socket_async) — Applies whenever TLS is enabled on the socket.
IoT sockets (iotSocketCreate) — No effect when using the IoT Socket API in isolation, because that API does not expose TLS enablement.
Pre-conditions:
The Wi-Fi / network stack must be initialized.
Must be called before creating the secure socket(s) that need to use the selected ciphers. Existing secure sockets are not updated retroactively.
Post-conditions:
The supplied extended cipher bitmap is stored and applied to every secure socket created afterwards until the extended cipher list is changed again.
Note
Thread safety: Not thread-safe — the extended cipher list is held in an unsynchronized process-global. Call once from an initialization thread before any secure socket is created.
See Also
sl_si91x_set_socket_cipherlist, sl_si91x_config_socket, socket, sl_si91x_socket, sl_si91x_socket_async
Example
Example#
Enable the TLSv1.3 AES-128-GCM-SHA256 suite for every subsequent secure socket (BSD or SiWx91x family):
sl_si91x_set_extended_socket_cipherlist(BIT(SL_SI91X_TLS13_AES_128_GCM_SHA256));