Documentation Revision History#
Revision 4.1.2 released Sep, 2026#
SoC only#
Updated the
bt_stack_bypassSoC application README with instructions for obtaining RTT logs after a board reset.Documented
SL_SI91X_RETAINED_DATAandSL_SI91X_RETAINED_BSSmacros, which retain PSRAM-related sleep and wake state in internal RAM.Added BRD2605B to the supported hardware lists for Wi-Fi, BLE, and platform SoC examples.
Removed internal-only BRD4343S references from SoC example hardware requirements.
Added PSRAM build-variant guidance for the Power Save Deep Sleep, TWT TCP Client, and Wi-Fi Station BLE Throughput examples.
Removed unused SoC crypto example information of AES, ECDH, ECDSA, GCM-CMAC, HMAC, and SHA from documentation.
Added combined-image firmware fallback OTA instructions for the Slot A and Slot B SoC examples.
NCP only#
Standardized supported host MCU and SPI/UART interface requirements and corrected EFR32xG25 naming across NCP example READMEs.
SoC and NCP#
Clarified when the
rsi_ble_get_att_valueandrsi_ble_get_att_value_asynccallbacks are triggered.Updated the
wifi_concurrent_nat_ble_provisioning_socREADME with BLE-disconnection guidance.Removed the BRD2605B hyperlink from the example documentation.
Clarified HTTP POST and PUT transfer modes,
end_of_datastatus values, and the fixed NWP HTTP timeout.Documented MQTT error-event status information and updated error-handling instructions for the Embedded MQTT Client example.
Clarified remote-termination callback parameters as the BSD socket descriptor and remote peer port.
Documented the GATT Client synchronous-API requirement to disable
SL_SI91X_BLE_GATT_ASYNC_ENABLE.Updated BRD4002A references to BRD4002B across Wi-Fi, BLE, and platform example documentation.
Documented the SNTP prerequisite for Azure IoT MQTT SAS-token generation and troubleshooting guidance.
Added
sl_paho_network_connect()API documentation for explicit IPv4 or IPv6 MQTT TCP connections.Clarified that
SL_WIFI_FEAT_SECURITY_OPENsupports both client and AP modes.Updated function header for
rsi_ble_enableandrsi_ble_disableto reflect API reference in docs.silabs.com.
Revision 4.1.1 released Jul 29, 2026#
SoC only#
None
NCP only#
None
SoC and NCP#
Documentation release aligned with WiSeConnect SDK v4.1.1, including refresh of public examples index and getting-started links to the v4.1.1 example README content.
Added Migrating from v4.1.0 guide covering newly introduced APIs, updated timeout behavior, and newly documented structures, fields, macros, and enums for the 4.1.1 release.
Expanded the Wi-Fi Scan and Connect Developer Guide with clearer API descriptions, initialization flow, channel-bitmap guidance, configuration structure usage, parameter-tuning links, and usage-scenario coverage.
Updated application-debugging documentation to clarify how to enable additional host/NWP logs in Simplicity Studio and how to interpret
H TX->/H RX->logging output.Refreshed AT command and API reference content for HTTP client, IP management, network credentials, network interfaces, network profiles, UART, file system, and Wi-Fi common/debugging/radio/scanning topics so descriptions and header/source links align with the v4.1.1 SDK content.
Updated public documentation references for supported boards and examples, including formatting cleanups and refreshed links for BRD4343C-related hardware text and public example README pages.
Revision 4.1.0 released Jun, 2026#
SoC only#
Added BRD4343C radio board support and UG641 BRD4343C User Guide to the documentation menu.
NCP only#
Refreshed NCP getting-started guide images and workflow for EFR32 hosts.
Added support for the BRD4357C Radio Board in the SiWx917 NCP Manufacturing Utility User Guide (UG575) and the EFR32 and STM32 getting started guides.
SoC and NCP#
Documentation release aligned with WiSeConnect SDK v4.1.0.
Added Migrating from v4.0.2 guide covering CMSIS 6.2, HAL thread priorities, and v4.1.0 API, AT command, and component deprecations.
Updated Enable Additional Logs section for the Log Backend I/O Stream component and
SL_DEBUG_LOG_V2host/NWP command logging.Documented deprecated
at+wifi-net-info?AT command and itsat+net-info=<interface>replacement.Updated README documentation for the Wi-Fi Concurrent Mode and Wi-Fi Concurrent HTTP Server examples to resolve the app-vs-documentation mismatch, including removal of inaccurate 5 GHz channel information from the Concurrent HTTP Server README.
Updated the SNTP Client example README to match the application's actual NTP server configuration behavior in Wi-Fi concurrent mode.
Added README and supporting resource images for the Wi-Fi - AWS IoT MQTT Client (LwIP TLS) example
Fixed numerous spelling mistakes across WLAN components and developer documentation.
Documented in the
sl_si91x_select()API reference that multiple file descriptors are not supported in a singleselectcall.Updated the Wi-Fi Client BLE Provisioning with AWS (Devkit) README to address reported documentation issues for the Coex example.
Added the missing AWS configuration details to the Wi-Fi Client BLE Provisioning with AWS (Devkit) README for Si Connect App v3.2.0 and above.
Updated API documentation to mark the
sl_wifi_twt_selection_tstructure andsl_wifi_target_wake_time_auto_selection()API as deprecated in favor of the v2 variants (sl_wifi_twt_selection_v2_t/sl_wifi_target_wake_time_auto_selection_v2()).
Revision 4.0.2 released April, 2026#
SoC only#
Updated the note for the
SL_SI91X_EXT_FEAT_FRONT_END_SWITCH_PINS_ULP_GPIO_4_5_0.
NCP only#
None
SoC and NCP#
Documented listen_interval prerequisites for sl_wifi_set_performance_profile() and sl_wifi_set_performance_profile_v2() — requires SL_WIFI_JOIN_FEAT_PS_CMD_LISTEN_INTERVAL_VALID to be set via sl_wifi_set_join_configuration() before AP connection, must not exceed the value set by sl_wifi_set_listen_interval_v2(), and defaults to 1000 ms.
Updated sl_wifi_set_max_tx_power API documentation to clearly state that a Wi-Fi join operation must be completed before invoking this API, ensuring developers configure transmit power in the correct call sequence.
Updated sl_net_dns_resolve_hostname() API documentation to reflect that the user-configured DNS_TIMEOUT is now propagated to the NWP firmware (previously the firmware used a fixed ~70-second timeout regardless of the SDK setting).
Updated the OPN gain-table values and inline documentation.
Revision 4.0.1 released March, 2026#
SoC only#
Improved software component documentation to clarify that "No External Flash" must be selected when using on-module flash.
NCP only#
None
SoC and NCP#
Enhanced sl_si91x_select() API documentation to clarify that the API is designed for connected sockets, not listening sockets. This helps developers avoid errors (such as 0xfffd) when using the API before accept() and provides clearer usage guidelines.
Enhanced HTTP OTAF README documentation with detailed combined image (NWP+M4) generation steps. This provides clearer guidance for creating firmware update packages and helps customers implement over-the-air firmware updates more effectively.
Revision 4.0.0 released December, 2025#
SoC only#
Updated the documentation note section of the
sl_si91x_get_socket_info()API.Updated README documentation for the Wi-Fi Commander example.
NCP only#
Updated README documentation for the WLAN throughput example.
SoC and NCP#
Updated README documentation for HTTP client and AWS MQTT examples.
Added NWP Watchdog Timer configuration support in UC Development.
Added deinitialization support for the Wi-Fi client interface when the power-save profile is set to DEEP_SLEEP_WITHOUT_RAM_RETENTION.
Updated the use of SiWx91x Async Sockets in the HTTP server for consistency.
Replaced debug breakpoints with proper error status returns to improve error handling.
Updated README documentation for station ping example.
Fixed formatting issue in
sl_wifi_region_code_tAPI docs.Updated stack size of Network Manager thread.
Added encryption types "PEAPSAFE1" and "PEAPSAFE2".
Renamed the command engine callback type from
sl_wifi_command_engine_status_handler_ttosl_wifi_command_engine_status_callback_t.Updated IPv6 throughput values in README documentation.
Updated station ping IPv6 README documentation.
Updated README documentation for the wireless test example.
Added configurable maximum retransmission timeout via the AWS_IOT_MAX_RETRANSMISSION_TIMEOUT macro in
aws_iot_config.h.Updated Wi-Fi Coex - Wi-Fi Client HTTPS BLE Dual Role README documentation.
Updated the documentation for SL_SI91X_CUSTOM_FEAT_HTTP_HTTPS_AUTH macro to indicate that HTTP/HTTPS authentication is currently not supported.
Updated README documentation for the concurrent HTTP server example.
Updated README documentation for the Wi-Fi Coex – Wi-Fi BLE Power Save example.
Added documentation for the newly added timeout indication macros.
Updated the note section of the
sl_wifi_ap_configuration_tstructure.Enabled the WLAN RX low-power chain in both NCP and SoC modes and added new APIs with updated documentation for usage and configuration.
Updated the notes section to document the usage and configuration of the WLAN RX low-power chain APIs.
Added APIs to retrieve Wireless Statistics for Concurrent Wi-Fi Interfaces.
Added support for the LwIP stack in the Paho embedded MQTT library.
Integrated mbedTLS changes for the Paho MQTT library.
Updated Embedded MQTT Client TWT README documentation.
Updated README documentation for the firmware update bootloader XModem example.
Updated README documentation for the LwIP MQTT over TCP example.
Updated the maximum number of supported clients from 15 to 8.
Added new APIs for Wi-Fi set and get join configuration.
Updated README documentation for Wi-Fi Coex - Wi-Fi Concurrent NAT with BLE Provisioning.
Updated README documentation for the Wi-Fi concurrent NAT BLE Provisioning example
Updated scan and join documentation.
Enhanced Vendor Specific IE requirement handling with improvements and updated documentation.
Added support for dynamically configuring hidden SSID in P2P mode.
Improved the
sl_si91x_recvfromDoxygen documentation for UDP datagram continuation and sizing constant.Refactored PER mode APIs.
Added new APIs in the Wi-Fi SDK to support SNI parameters for the embedded MQTT feature.
Added an opermode bit to configure the LDO.
Revision 3.5.3 released October, 2025#
SoC only#
None
NCP only#
None
SoC and NCP#
Added
SL_SI91X_CONFIG_FEAT_BLE_ONLY_LOW_POWER_MODEconfiguration bit in config_feature_bit_map for memory optimization.
Revision 3.5.2 released September, 2025#
SoC only#
Updated applications prints for Wi-Fi M4 firmware update.
Updated README documentation for various SoC peripheral examples including PS2 wireless event monitor, LittleFS common flash, eFuse, QEI, HSPI primary/secondary, PCM primary/secondary, I2C driver follower/leader non-blocking, OpAmp, ADC static mode, ULP I2S, DAC, ULP DAC, BJT temperature sensor, PWM, GSPI, memory manager, watchdog timer manager, and M4 updater examples.
Enhanced documentation for peripheral drivers and system components including eFuse, clock manager, GSPI, OpAmp, GPIO driver, GPDMA, system RTC, BJT temperature sensor, configuration timer, memory manager, SDIO secondary, and firmware fallback modules.
Improved PSRAM core component documentation.
Corrected the supported instances displayed in UC screens for proper component configuration.
NCP only#
None
SoC and NCP#
Updated readme of Wi-Fi - Azure IoT MQTT client application.
Marked internal Wi-Fi transceiver mode configurations as unsupported for the current release.
Updated the readme for WLAN TCP TX on periodic wakeup example.
Updated readme of Wi-Fi - Embedded MQTT client example correcting the units of Keepalive timer as seconds.
Updated readme of Crypto - AES example.
Removed incorrect HTTPS server references from documentation.
Added documentation for the TLS_EXTENSION_ENABLE macro in the TLS client example.
Added recommendation settings as a note in example applications.
Update Flash Read Write readme to include note on flash memory erasure before write operations.
Added readme for NAT application, Wi-Fi - Dual Network Stack NWP + M4.
Updated application prints for Wi-Fi Firmware update example.
Updated the error code for SL_STATUS_SI91X_HOST_VOLTAGE_OUT_OF_RANGE.
Updated the readme of Wi-Fi Coex - Wi-Fi Client BLE Provisioning with AWS (Devkit) example.
Updated
sl_wifi_update_su_gain_tableAPI documentation to improve clarity.Updated
sl_si91x_rsp_wireless_info_tstructure documentation to improve clarity.Updated
SL_WIFI_FEAT_DISABLE_SHORT_GIdocumentation with a note on it's impact on 802.11n and 802.11ax data rates.
Revision 3.5.0 released June, 2025#
SoC only#
Updated README documentation with output images in Wi-Fi - NWP Or Combined (NWP & M4) Firmware Update via TCP example.
Updated the Wi-Fi – AWS IoT MQTT Client example README to include the latest application print images.
NCP only#
Updated the API description for
sl_http_server_init()and updated the README for the multithreading application.
SoC and NCP#
Updated the README documentation with the path to scripts to be used in Wi-Fi - HTTP Client and Wi-Fi - HTTP Server examples.
Updated the README documentation for the Wi-Fi - Concurrent HTTP Server Provisioning as per new flow.
Updated the README documentation with the steps to update the user gain table for the Wireless Test example.
Updated the
sl_wifi_stats_callback_tdocumentation to include a note directing users to the reference section for Access Point (AP) deauthentication reason codes.Updated documentation for
sl_wifi_bss_type_tto specify supported and unsupported BSS types.Updated documentation for NWP UART baud rate and steps to capture RAM dump details.
Revised the documentation to specify that
sl_wifi_send_raw_data_frame()usage is supported only after the module is in connected state.Updated README documentation with alarm-based wakeup information in Wi-Fi - AWS IoT MQTT Client example.
Updated documentation in the note section
sl_net_deinit()to explain that this function should not be called after an M4 OTA firmware upgrade.Updated type variable documentation in
sl_si91x_socket_type_length_value_tstructure.Updated README with images aligned to the mobile application interface.
Updated interface usage recommendation note in the
sl_net_deinit()API documentation.Updated
option_nameandoption_valuedocumentation for the TLS feature insl_si91x_setsockopt()API.Updated connection timeout recommendations in
sl_wifi_connect()for different security modes.Updated usage notes to clarify correct sequencing of sl_wifi_* and sl_net_* API functions, helping prevent undefined behavior during Wi-Fi/Network interface.
Updated the error code for SL_STATUS_SI91X_HOST_VOLTAGE_OUT_OF_RANGE.
Updated the
sl_si91x_gcmAPI documentation to specify the maximum supported message length.Added a note for configuring crystal good time using the
sl_si91x_set_nwp_config_requestAPI.