IP Management#
Functions#
Configure IP address of given interface.
This function retrieves the IP address of the specified network interface.
Enables Network Address Translation (NAT) on the specified network interface in concurrent mode.
Disables Network Address Translation (NAT) on the specified network interface in concurrent mode.
Function Documentation#
sl_net_configure_ip#
sl_status_t sl_net_configure_ip (sl_net_interface_t interface, const sl_net_ip_configuration_t * ip_config, uint32_t timeout)
Configure IP address of given interface.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_net_interface_t | [in] | interface | Interface identified by sl_net_interface_t |
| const sl_net_ip_configuration_t * | [in] | ip_config | Multicast IP address of type sl_net_ip_configuration_t |
| uint32_t | [in] | timeout | The maximum time to wait for the IP address Configuration, in milliseconds. |
Pre-conditions:
sl_net_up should be called before this API.
Returns
sl_status_t. See https://docs.silabs.com/gecko-platform/latest/platform-common/status for details.
Note
This API doesn't support async mode operation, so passing 0 in timeout parameter leads to an error.
sl_net_get_ip_address#
sl_status_t sl_net_get_ip_address (sl_net_interface_t interface, sl_net_ip_address_t * ip_address, uint32_t timeout)
This function retrieves the IP address of the specified network interface.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_net_interface_t | [in] | interface | Interface identified by sl_net_interface_t |
| sl_net_ip_address_t * | [in] | ip_address | IP address of type sl_net_ip_address_t |
| uint32_t | [in] | timeout | The maximum time to wait for the IP address retrieval, in milliseconds. |
Pre-conditions:
sl_net_up should be called before this API.
Returns
sl_status_t. See https://docs.silabs.com/gecko-platform/latest/platform-common/status for details.
Note
This API doesn't support async mode operation, so passing 0 in timeout parameter leads to an error.
If the interface is setup in SL_IP_MANAGEMENT_STATIC_IP mode, this API only returns its mode and doesn't return ip address.
sl_net_nat_enable#
sl_status_t sl_net_nat_enable (const sl_net_nat_config_t * nat_config)
Enables Network Address Translation (NAT) on the specified network interface in concurrent mode.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const sl_net_nat_config_t * | [in] | nat_config | Pointer to the NAT configuration structure of type sl_net_nat_config_t. |
This function enables NAT on the given network interface. This is a blocking API.
Pre-conditions:
sl_net_init should be called before this API on AP and STA interfaces. sl_net_up should be called before this API on AP and STA interfaces.
Returns
status of the operation.
SL_STATUS_OK: On successful completion of the operation.
SL_STATUS_FAIL: If the operation fails.
SL_STATUS_INVALID_PARAMETER: If the nat_config parameter is NULL.
Note
NAT feature is internal test feature only, not recommended for Production.
sl_net_nat_disable#
sl_status_t sl_net_nat_disable (const sl_net_interface_t interface)
Disables Network Address Translation (NAT) on the specified network interface in concurrent mode.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const sl_net_interface_t | [in] | interface | The network interface on which to disable NAT. (This parameter is currently unused.) |
This function disables NAT on the given network interface. This is a blocking API.
Pre-conditions:
sl_net_nat_enable should be called before this API.
Returns
Status of the operation.
SL_STATUS_OK: On successful completion of the operation.
SL_STATUS_FAIL: If the operation fails.
Note
NAT feature is internal test feature only, not recommended for Production.