LED#
Introduction#
The SI91x LED driver is a platform-level software module designed to manage LED control. All LED functions are accessed through the generic driver, which then internally calls the LED-specific functions.
Configuration#
All LED instances are configured with an sl_led_t struct. This struct along with a function definition for initializing LED is automatically generated when an LED is set up using Simplicity Studio's wizard. This struct sl_led_t struct is automatically generated into the following files sl_si91x_led_instances.h and sl_si91x_led_instances.c. The samples below are for a single instance called "led0".
// sl_si91x_led_instances.c
#include "sl_si91x_led.h"
#include "sl_si91x_led_config.h"
#include "sl_si91x_led_instances.h"
sl_led_t const led_led0 = {
.port = SL_LED_LED0_PORT,
.pin = SL_LED_LED0_PIN,
.led_number = SL_LED_LED0_NUMBER,
};
void led_init_instances(void)
{
sl_si91x_led_init(&led_led0);
}
Note
The sl_si91x_led_instances.c file is shown with only one instance, but if more were in use they would all appear in this .c file.
// sl_si91x_led_instances.h
#ifndef SL_SI91x_LED_INSTANCES_H
#define SL_SI91x_LED_INSTANCES_H
#include "sl_si91x_led.h"
extern const sl_led_t led_led0;
void led_init_instances(void);
#endif // SL_SI91x_LED_INSTANCES_H
Note
The sl_si91x_led_instances.h file is shown with only one instance, but if more were in use they would all appear in this .h file.
For more information on configuring available parameters, see the respective peripheral example readme document and Peripheral Configuration.
Usage#
After the LED structures are defined, the LED functions can be called by passing an instance of sl_led_t, which will internally redirect to the type-specific version of the function. The commonly used functions include the following:
It configure GPIOs pertaining to the control of LEDs and to initialize the selected LED GPIO and mode: sl_si91x_led_init
This atomically wraps an XOR or a similar operation for a single GPIO pin connected to an LED to toggle the LED: sl_si91x_led_toggle
To set a GPIO pin connected to an LED to turn the LED on: sl_si91x_led_set
To clear a GPIO pin connected to an LED to turn the LED off: sl_si91x_led_clear
sl_si91x_led_init initialises the specific LED. This function is called automatically when the application is run.
sl_si91x_led_toggle can be implemented by the application, if required. This function is used to toggle the state of the LED. sl_si91x_led_set and sl_si91x_led_clear both can be implemented by the application. These functions are used to turn the LED on and off resectively.
Functions#
To configure GPIOs pertaining to the control of LEDs and initializes the selected LED GPIO and mode.
To toggle the state of an LED connected to a specified GPIO pin.
To set the state of an LED connected to a specified GPIO pin to ON.
To clear the state of an LED connected to a specified GPIO pin to OFF.
To indicate radio activity for both transmission and reception.
Function Documentation#
sl_si91x_led_init#
void sl_si91x_led_init (const sl_led_t * handle)
To configure GPIOs pertaining to the control of LEDs and initializes the selected LED GPIO and mode.
Type | Direction | Argument Name | Description |
---|---|---|---|
const sl_led_t * | [in] | handle | The pointer to an sl_led_t structure that contains the specific LED information. |
This API initializes the selected GPIOs, sets their operation modes, and configures them for controlling the LEDs. It ensures that the GPIOs are properly configured to drive the LEDs as per the specified settings in the handle.
The GPIO peripheral must be enabled and clocked before calling this function.
The specified GPIO pin will be configured and set to the initial state as defined in the handle.
sl_si91x_led_toggle#
void sl_si91x_led_toggle (uint8_t pin)
To toggle the state of an LED connected to a specified GPIO pin.
Type | Direction | Argument Name | Description |
---|---|---|---|
uint8_t | [in] | pin | GPIO pin connected to the LED to be toggled. |
This API toggles the state of an LED connected to a specified GPIO pin by performing an XOR operation. The function identifies the GPIO port corresponding to a given pin number for a specific development board/opn.
The GPIO peripheral must be enabled and clocked before calling this function.
The state of the specified GPIO pin will be toggled, effectively turning the connected LED on or off.
sl_si91x_led_set#
void sl_si91x_led_set (uint8_t pin)
To set the state of an LED connected to a specified GPIO pin to ON.
Type | Direction | Argument Name | Description |
---|---|---|---|
uint8_t | [in] | pin | GPIO pin connected to the LED to be turned on. |
This API sets the specified GPIO pin to a high state, which turns on the LED connected to that pin. The function determines the GPIO port based on the pin number and the development kit being used.
The GPIO peripheral must be enabled and clocked before calling this function.
The specified GPIO pin will be set to the appropriate state to turn on the LED.
sl_si91x_led_clear#
void sl_si91x_led_clear (uint8_t pin)
To clear the state of an LED connected to a specified GPIO pin to OFF.
Type | Direction | Argument Name | Description |
---|---|---|---|
uint8_t | [in] | pin | GPIO pin connected to the LED to be turned off. |
This API sets the specified GPIO pin to a low state, which turns off the LED connected to that pin. The function determines the GPIO port based on the pin number and the development kit being used.
The GPIO peripheral must be enabled and clocked before calling this function.
The specified GPIO pin will be set to the appropriate state to turn off the LED.
sl_si91x_led_StackIndicateActivity#
void sl_si91x_led_StackIndicateActivity (bool turnOn)
To indicate radio activity for both transmission and reception.
Type | Direction | Argument Name | Description |
---|---|---|---|
bool | [in] | turnOn | A boolean value indicating the radio activity state. |
This function is called by the stack to indicate activity over the radio. It is called once with turnOn
set to true to indicate the start of activity, and shortly thereafter with turnOn
set to false to indicate the end of activity. Typically, this function changes the state of an LED to reflect the radio activity.
The LED or other indicator should be properly configured before calling this function.
The state of the LED or other indicator will be updated based on the radio activity.