Types#

This section provides a reference to the SNTP API data types.

Modules#

SL_ATTRIBUTE_PACKED

sl_sntp_client_response_t

sl_sntp_client_config_t

Typedefs#

typedef void(*
sl_sntp_client_event_handler_t)(sl_sntp_client_response_t *response, uint8_t *user_data, uint16_t user_data_length)

Callback type for handling SNTP client responses.

typedef void(*
sl_sntp_set_time_sync_notification_handler_t)(const uint8_t cmd_type, sl_status_t status, const uint8_t *buffer)

Callback type for handling SNTP time synchronization notifications.

Typedef Documentation#

sl_sntp_client_event_handler_t#

sl_sntp_client_event_handler_t )(sl_sntp_client_response_t *response, uint8_t *user_data, uint16_t user_data_length)

Callback type for handling SNTP client responses.

Parameters
TypeDirectionArgument NameDescription
[in]response

Pointer to the SNTP client response of type sl_sntp_client_response_t.

[in]user_data

Pointer to user data passed in the APIs sl_sntp_client_get_time(), sl_sntp_client_get_time_date(), and sl_sntp_client_get_server_info().

[in]user_data_length

Length of the user data passed in the APIs sl_sntp_client_get_time(), sl_sntp_client_get_time_date(), and sl_sntp_client_get_server_info().

This callback is invoked to handle responses from the SNTP client. It provides the response data, user data, and the length of the user data.


sl_sntp_set_time_sync_notification_handler_t#

sl_sntp_set_time_sync_notification_handler_t )(const uint8_t cmd_type, sl_status_t status, const uint8_t *buffer)

Callback type for handling SNTP time synchronization notifications.

Parameters
TypeDirectionArgument NameDescription
[in]cmd_type

Command type indicating the type of SNTP operation.

[in]status

Status of the SNTP operation. See https://docs.silabs.com/gecko-platform/latest/platform-common/status for details.

[in]buffer

Pointer to the data buffer containing additional information related to the SNTP operation.

This callback is invoked to handle notifications related to SNTP time synchronization. It provides the command type, status of the operation, and a data buffer.

Note

  • This feature is currently not supported in SiWx91x chipsets.