BSD Sockets#
This section provides a reference to BSD Socket API functions.
The BSD socket implementation tries to emulate the standards library to the extent possible for embedded offerings from Silabs. There are substantial limitation/exceptions however, and those are mentioned under Note section in the subsequent API documentation of BSD sockets.
Note
BSD Sockets support only synchronous socket operations. For asynchronous operations, refer to the SiWx91x sockets.
sl_si91x_get_saved_firmware_status() needs to be called to fetch the error code returned by the firmware if the API returns -1 and errno is 0.
Modules#
Typedefs#
Socket Length is internal type.
Public type for socket length.
Internal type for sockaddr address family.
Public type for sockaddr address family.
Functions#
Create an endpoint for communication.
Bind a name to a socket.
Listen for connections on a socket.
Accept a connection on a socket.
Initiate a connection on a socket.
Receive a message from a socket.
Receive a message from a socket.
Send a message on a socket.
Send a message on a socket.
Set options on a socket.
Get options on a socket.
Get the name of the connected peer socket.
Get the current address assigned to a socket.
Close a socket.
Typedef Documentation#
__socklen_t#
__socklen_t
Socket Length is internal type.
It represents the length of a socket address that is used internally within network system calls to specify the size of address structures.
socklen_t#
socklen_t
Public type for socket length.
It is a public alias for the internal __socklen_t type. You can use it to specify the length of socket addresses in the network system calls.
__sa_family_t#
__sa_family_t
Internal type for sockaddr address family.
The address family of a socket address is used internally within the system to specify the address type (for example, IPv4 and IPv6).
sa_family_t#
sa_family_t
Public type for sockaddr address family.
It is a public alias for the internal ___sa_family_t. It specifies the address family of a socket address in user applications.
Function Documentation#
socket#
int socket (int domain, int type, int protocol)
Create an endpoint for communication.
Type | Direction | Argument Name | Description |
---|---|---|---|
int | [in] | domain | Specifies a communication domain, selecting the protocol family to be used for communication. Must be one of the values from Socket Address Family. |
int | [in] | type | Specifies the semantics of communication for the socket. Must be one of the values from BSD_SOCKET_TYPES. Currently defined types are SOCK_STREAM, SOCK_DGRAM, SOCK_RAW, SOCK_RDM, and SOCK_SEQPACKET. |
int | [in] | protocol | Specifies a particular protocol to be used with the socket. Normally, only a single protocol exists to support a particular socket type within a given protocol family. However, if multiple protocols exist, a specific protocol must be specified. The protocol number to use is specific to the communication domain. Must be one of the values from Socket Protocol. |
The socket()
function creates an endpoint for communication and returns a file descriptor that refers to that endpoint. The file descriptor returned by a successful call would be the lowest-numbered file descriptor not currently open for the process.
Returns
Returns the socket ID or file descriptor that references the socket upon success. Returns -1 if an error occurs.
Note
The
type
supports SOCK_STREAM and SOCK_DGRAM only.
bind#
int bind (int socket_id, const struct sockaddr * addr, socklen_t addr_len)
Bind a name to a socket.
Type | Direction | Argument Name | Description |
---|---|---|---|
int | [in] | socket_id | The socket ID or file descriptor for the specified socket. |
const struct sockaddr * | [in] | addr | Pointer to a sockaddr structure containing the address to be assigned to the socket. |
socklen_t | [in] | addr_len | The |
When a socket is created with socket()
, it exists in a namespace (address family) but, has no address assigned to it. The bind()
function assigns the address specified by addr
to the socket referred to by the file descriptor socket_id
.
Traditionally, this operation is called "assigning a name to a socket".
It is normally necessary to assign a local address using bind()
before a SOCK_STREAM
socket may receive connections.
Returns
Returns 0 if successful. Otherwise, returns -1 and sets the global variable
errno
to indicate the error.
listen#
int listen (int socket_id, int backlog)
Listen for connections on a socket.
Type | Direction | Argument Name | Description |
---|---|---|---|
int | [in] | socket_id | The socket ID or file descriptor for the specified socket. |
int | [in] | backlog | The backlog argument defines the maximum number of pending connections that can be queued. |
The listen()
function marks the socket referred to by socket_id
as a passive socket, that is, as a socket that would be used to accept incoming connection requests using accept()
. This function applies only to sockets of type SOCK_STREAM
or SOCK_SEQPACKET
.
To accept connections, a socket must first be created with socket(). A willingness to accept incoming connections and a queue limit for incoming connections must be specified with listen(), and then the connections can be accepted with accept().
Returns
Returns 0 if successful. Otherwise, returns -1 and sets the global variable
errno
to indicate the error.
accept#
int accept (int socket_id, struct sockaddr * addr, socklen_t * addr_len)
Accept a connection on a socket.
Type | Direction | Argument Name | Description |
---|---|---|---|
int | [in] | socket_id | Socket identification number of the socket to accept. This socket must have been created with socket(), bound to an address with bind(), and set to listen for connections with listen(). |
struct sockaddr * | [out] | addr | Pointer to a |
socklen_t * | [inout] | addr_len | Pointer to a |
The accept()
system call is used with connection-based socket types (for example, SOCK_STREAM
, SOCK_SEQPACKET
). It extracts the first connection request on the queue of pending connections for the listening socket (socket_id
), creates a new connected socket, and returns a new file descriptor referring to that socket. The newly created socket is not in the listening state. The original socket (socket_id
) is unaffected by this call.
If no pending connections are present on the queue and the original socket is not marked as non-blocking, this function blocks the caller until a connection is present. If the original socket is marked non-blocking and no pending connections are present on the queue, accept() returns an error. The accepted socket may not be used to accept more connections. The original socket (socket_id
) remains open.
Returns
Returns a non-negative integer that is a descriptor for the accepted socket if successful. Returns -1 on error and sets the global variable
errno
to indicate the error.
Note
The accept() system call only supports blocking mode.
connect#
int connect (int socket_id, const struct sockaddr * addr, socklen_t addr_len)
Initiate a connection on a socket.
Type | Direction | Argument Name | Description |
---|---|---|---|
int | [in] | socket_id | The socket ID or file descriptor for the specified socket. |
const struct sockaddr * | [in] | addr | The addr argument of type sockaddr is the address is that to which datagrams are to be sent. |
socklen_t | [in] | addr_len | The addr_len argument of type socklen_t indicates the amount of space pointed to by address, in bytes. |
The connect() system call connects the socket referred to by the file descriptor socket_id
to the address specified by addr
.
The addr_len
argument specifies the size of addr
. The format of the address in addr
is determined by the address space of the socket socket_id
; see socket() for further details.
If socket_id
is of type SOCK_DGRAM
, the connect() system call specifies the peer with which the socket is to be associated. If the socket is of type SOCK_STREAM
, the connect() system call attempts to make a connection to another socket. The other socket is specified by addr
, which is an address in the communications space of the socket. Each communications space interprets the addr
argument in its own way. Generally, stream sockets may successfully connect() only once; datagram sockets can use connect() multiple times to change their association.
Returns
Returns 0 if successful. Otherwise, returns -1 and sets the global variable
errno
to indicate the error.
Note
Connecting to an invalid address, such as a null address, will result in an
EFAULT
error.
recv#
ssize_t recv (int socket_id, void * buf, size_t buf_len, int flags)
Receive a message from a socket.
Type | Direction | Argument Name | Description |
---|---|---|---|
int | [in] | socket_id | The socket ID or file descriptor for the specified socket. |
void * | [out] | buf | Pointer to the buffer that receives the data. |
size_t | [in] | buf_len | Length of the buffer pointed to by the |
int | [in] | flags | Controls the reception of the data. Currently, no flags are supported and this parameter should be set to 0. |
The recv() function is normally used only on a connected socket. It receives messages from a socket and returns the length of the message on successful completion. If a message is too long to fit in the supplied buffer, excess bytes may be discarded depending on the type of socket the message is received from. By default, recv() is a blocking API. To use it in a non-blocking manner, you can set the socket to non-blocking mode using setsockopt()
.
Returns
ssize_t
Note
The recv() system call does not support any flags.
recvfrom#
ssize_t recvfrom (int socket_id, void * buf, size_t buf_len, int flags, struct sockaddr * from_addr, socklen_t * from_addr_len)
Receive a message from a socket.
Type | Direction | Argument Name | Description |
---|---|---|---|
int | [in] | socket_id | The socket ID or file descriptor for the specified socket. |
void * | [out] | buf | Pointer to the buffer that receives the data. |
size_t | [in] | buf_len | The length of the buffer pointed to by the |
int | [in] | flags | Controls the reception of the data. Currently, no flags are supported and this parameter should be set to 0. |
struct sockaddr * | [out] | from_addr | Pointer to a socket address structure of type sockaddr that will be filled with the source address of the received message. If the source address is not required, this parameter can be NULL. |
socklen_t * | [inout] | from_addr_len | A value-result argument of type socklen_t. Initially, it should contain the size of the buffer associated with |
The recvfrom() system call is used to receive messages from a socket and can be used to receive data on a socket whether or not it is connection-oriented. If from_addr
is not a null pointer and the socket is not connection-oriented, the source address of the message is filled in.
Returns
Returns the length of the message on successful completion. Returns -1 on error and sets the global variable
errno
to indicate the error.
Note
The recvfrom() system call does not support any flags.
send#
ssize_t send (int socket_id, const void * buf, size_t buf_len, int flags)
Send a message on a socket.
Type | Direction | Argument Name | Description |
---|---|---|---|
int | [in] | socket_id | The socket ID or file descriptor for the specified socket. |
const void * | [in] | buf | Pointer to the buffer containing the message to transmit. |
size_t | [in] | buf_len | The length of the message in bytes. |
int | [in] | flags | Controls the transmission of the data. Currently, no flags are supported and this parameter should be set to 0. |
The send() function is used to transmit a message on a socket. This function can only be used when the socket is in a connected state. If the socket is connection-oriented, the protocol must support implied connect or the socket must be explicitly connected before use. No indication of failure to deliver is implicit in a send(). Locally detected errors are indicated by a return value of -1. If no message space is available at the socket to hold the message to be transmitted, then send() normally blocks, unless the socket has been placed in non-blocking I/O mode.
Returns
Returns the number of bytes sent on success. Returns -1 on error and sets the global variable
errno
to indicate the error.
Note
The send() system call currently supports only blocking mode.
The send() system call does not guarantee that the packets are transmitted to the remote node; they are enqueued in the local queue.
The send() system call does not support any flags.
The send() system call can send a maximum of 1460 bytes in the case of plain TCP/UDP. For TLS, the maximum buffer length is 1370 bytes.
sendto#
ssize_t sendto (int socket_id, const void * buf, size_t buf_len, int flags, const struct sockaddr * to_addr, socklen_t to_addr_len)
Send a message on a socket.
Type | Direction | Argument Name | Description |
---|---|---|---|
int | [in] | socket_id | The socket ID or file descriptor for the specified socket. |
const void * | [in] | buf | Pointer to the buffer containing the message to transmit. |
size_t | [in] | buf_len | The length of the message in bytes. |
int | [in] | flags | Controls the transmission of the data. Due to firmware limitations, sendto() does not support any flags and this parameter should be set to 0. |
const struct sockaddr * | [in] | to_addr | Pointer to a |
socklen_t | [in] | to_addr_len | Size of the address structure pointed to by |
The sendto() function is used to transmit a message on a socket. This function can be used at any time if the socket is in connectionless mode. If the socket is in connection mode, the protocol must support implied connect or the socket must be in a connected state before use. The address of the target is specified by to_addr
with to_addr_len
indicating its size. If the socket is in a connected state, the target address passed to sendto() is ignored. If the message is too long to pass atomically through the protocol, the error EMSGSIZE
is returned, and the message is not transmitted.
Returns
The number of octets sent. If an error occurred, a value of -1 is returned.
Note
setsockopt#
int setsockopt (int socket_id, int option_level, int option_name, const void * option_value, socklen_t option_length)
Set options on a socket.
Type | Direction | Argument Name | Description | ||||||||||||||||||||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
int | [in] | socket_id | The socket ID or file descriptor for the specified socket. | ||||||||||||||||||||||||||||||
int | [in] | option_level | The level at which the option is being set. One of the values from Socket Option Level. | ||||||||||||||||||||||||||||||
int | [in] | option_name | The option to be configured. Accepts values from Socket Option Name. Currently, following options are supported: | ||||||||||||||||||||||||||||||
const void * | [in] | option_value | A pointer to the buffer containing the value for the option. Most socket-level options utilize an
| ||||||||||||||||||||||||||||||
socklen_t | [in] | option_length | The length of the option data, in bytes, pointed to by |
The setsockopt() system call manipulates the options associated with a socket. Options may exist at multiple protocol levels; they are always present at the uppermost "socket" level. When manipulating socket options, the level at which the option resides and the name of the option must be specified. To manipulate options at the socket level, option_level
is specified as SOL_SOCKET
. To manipulate options at any other level, the protocol number of the appropriate protocol controlling the option is supplied. For example, to indicate that an option is to be interpreted by the TCP protocol, option_level
should be set to the protocol number of TCP. The option_value
and option_length
arguments are used to access option values for setsockopt().
Returns
Returns 0 on successful completion. Returns -1 on error and sets the global variable
errno
to indicate the error.
Note
The options
SL_SO_CERT_INDEX
,SL_SO_HIGH_PERFORMANCE_SOCKET
,SL_SO_TLS_SNI
, andSL_SO_TLS_ALPN
are Silicon Labs specific options. This function is used before the socket is connected.
getsockopt#
int getsockopt (int socket_id, int option_level, int option_name, void * option_value, socklen_t * option_length)
Get options on a socket.
Type | Direction | Argument Name | Description |
---|---|---|---|
int | [in] | socket_id | The socket ID or file descriptor for the specified socket. |
int | [in] | option_level | The level at which the option is defined. One of the values from Socket Option Level. |
int | [in] | option_name | The name of the option to retrieve. One of the values from Socket Option Name. The |
void * | [out] | option_value | Pointer to a buffer where the retrieved option value will be stored. |
socklen_t * | [inout] | option_length | A value-result argument of type socklen_t. Initially, it should contain the size of the buffer pointed to by |
The getsockopt() system call retrieves the options associated with a socket. Options may exist at multiple protocol levels; they are always present at the uppermost "socket" level. When retrieving socket options, the level at which the option resides and the name of the option must be specified. To retrieve options at the socket level, option_level
is specified as SOL_SOCKET
. To retrieve options at any other level, the protocol number of the appropriate protocol controlling the option is supplied. For example, to indicate that an option is to be interpreted by the TCP protocol, option_level
should be set to the protocol number of TCP. The option_value
and option_length
arguments identify a buffer in which the value for the requested options are to be returned.
Returns
Returns 0 on successful completion. Returns -1 on error and sets the global variable
errno
to indicate the error.
Note
The following options are currently supported:
SO_RCVTIMEO
: Receive timeout.SO_KEEPALIVE
: Keep connections alive.TCP_ULP
: TCP upper layer protocol.SO_MAX_RETRANSMISSION_TIMEOUT_VALUE
: Maximum retransmission timeout value.IP_TOS
: Type of service.
getpeername#
int getpeername (int socket_id, struct sockaddr * name, socklen_t * name_len)
Get the name of the connected peer socket.
Type | Direction | Argument Name | Description |
---|---|---|---|
int | [in] | socket_id | The socket ID or file descriptor for the specified socket. |
struct sockaddr * | [out] | name | Pointer to a |
socklen_t * | [inout] | name_len | A value-result argument of type socklen_t. Initially, it should contain the size of the buffer pointed to by |
The getpeername() system call returns the address of the peer connected to the socket specified by socket_id
. The address is returned in the buffer pointed to by name
, and the actual size of the address is returned in the variable pointed to by name_len
. If the buffer provided is too small, the address is truncated.
Returns
Returns 0 on success. Returns -1 on error and sets the global variable
errno
to indicate the error.
getsockname#
int getsockname (int socket_id, struct sockaddr * name, socklen_t * name_len)
Get the current address assigned to a socket.
Type | Direction | Argument Name | Description |
---|---|---|---|
int | [in] | socket_id | The socket ID or file descriptor for the specified socket. |
struct sockaddr * | [out] | name | Pointer to a |
socklen_t * | [inout] | name_len | A value-result argument of type socklen_t. Initially, it should contain the size of the buffer pointed to by |
The getsockname() system call returns the current address to which the socket socket_id
is bound. The address is returned in the buffer pointed to by name
, and the actual size of the address is returned in the variable pointed to by name_len
. If the buffer provided is too small, the address is truncated.
Returns
Returns 0 on success. Returns -1 on error and sets the global variable
errno
to indicate the error.
close#
int close (int socket_id)
Close a socket.
Type | Direction | Argument Name | Description |
---|---|---|---|
int | [in] | socket_id | The socket ID or file descriptor for the specified socket. |
The close() function closes a socket identified by socket_id
, so that it no longer refers to any file and can be reused. This function releases the resources associated with the socket and makes the socket descriptor available for reuse.
Returns
Returns 0 on success. Returns -1 on error and sets the global variable
errno
to indicate the error.
Note