Functions#
This section provides a reference to the WebSocket Client API functions.
Functions#
Initialize the WebSocket client.
Connect to a WebSocket server.
Send a WebSocket frame.
Close the WebSocket connection.
Deinitialize the WebSocket client.
Configures advanced TCP/TLS options for a WebSocket client.
Sets the Origin header value for a WebSocket client.
Extracts the WebSocket opcode from a given socket ID.
Function Documentation#
sl_websocket_init#
sl_websocket_error_t sl_websocket_init (sl_websocket_client_t * handle, const sl_websocket_config_t * config)
Initialize the WebSocket client.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_websocket_client_t * | [out] | handle | Pointer to the WebSocket client structure. Must not be NULL. |
| const sl_websocket_config_t * | [in] | config | Pointer to the WebSocket client configuration constant structure. Must not be NULL. |
This function initializes the WebSocket client with the provided configuration. It allocates necessary resources and sets up the client for connection.
Returns
sl_websocket_error_t - Error code indicating the result of the operation.
sl_websocket_connect#
sl_websocket_error_t sl_websocket_connect (sl_websocket_client_t * handle)
Connect to a WebSocket server.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_websocket_client_t * | [in] | handle | Pointer to the WebSocket client structure. Must not be NULL. |
This function creates a socket, binds it, and connects to the specified WebSocket server.
The WebSocket handle should be initialized using sl_websocket_init before calling this function.
Returns
sl_websocket_error_t - Error code indicating the result of the operation.
sl_websocket_send_frame#
sl_websocket_error_t sl_websocket_send_frame (sl_websocket_client_t * handle, const sl_websocket_send_request_t * send_request)
Send a WebSocket frame.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_websocket_client_t * | [in] | handle | Pointer to the WebSocket client structure. Must not be NULL. |
| const sl_websocket_send_request_t * | [in] | send_request | Pointer to the send request constant structure containing the frame details. Must not be NULL. |
This function sends a WebSocket frame to the server. Masking is taken care of by the firmware.
The WebSocket handle should be initialized using sl_websocket_init and connected using sl_websocket_connect before calling this function.
Returns
sl_websocket_error_t - Error code indicating the result of the operation.
Note
Masking refers to applying a random 32-bit mask to the data sent to the server to ensure data integrity and security.
The following table lists the maximum individual chunk of data that can be sent over each supported protocol. The length of the payload is specified in the
lengthfield of thesl_websocket_send_request_tstructure.
Protocol | Maximum data chunk (bytes) |
|---|---|
WebSocket | 1450 bytes |
WebSocket over SSL | 1362 bytes |
sl_websocket_close#
sl_websocket_error_t sl_websocket_close (sl_websocket_client_t * handle)
Close the WebSocket connection.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_websocket_client_t * | [in] | handle | Pointer to the WebSocket client structure. Must not be NULL. |
This function closes the WebSocket connection and cleans up resources.
The WebSocket handle should be initialized using sl_websocket_init and connected using sl_websocket_connect before calling this function.
Returns
sl_websocket_error_t - Error code indicating the result of the operation.
sl_websocket_deinit#
sl_websocket_error_t sl_websocket_deinit (sl_websocket_client_t * handle)
Deinitialize the WebSocket client.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_websocket_client_t * | [in] | handle | Pointer to the WebSocket client structure. Must not be NULL. |
This function deinitializes the WebSocket client by freeing allocated resources and resetting the state. It should be called only after the WebSocket connection has been closed because it also attempts to close the socket as part of its cleanup process if the socket remains open after the sl_websocket_close is invoked. Therefore, calling this function is mandatory whenever a WebSocket connection is terminated, ensuring proper cleanup.
The WebSocket handle should be initialized using sl_websocket_init before calling this function.
Returns
sl_websocket_error_t - Error code indicating the result of the operation.
sl_websocket_set_tcp_tls_advanced_configuration#
sl_websocket_error_t sl_websocket_set_tcp_tls_advanced_configuration (sl_websocket_client_t * handle, const sl_websocket_tcp_tls_advanced_options_t * options)
Configures advanced TCP/TLS options for a WebSocket client.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_websocket_client_t * | [in] | handle | Pointer to the WebSocket client structure. Must not be NULL. |
| const sl_websocket_tcp_tls_advanced_options_t * | [in] | options | Pointer to an sl_websocket_tcp_tls_advanced_options_t structure containing the TCP/TLS options. Must not be NULL. |
This function stores the provided advanced TCP and TLS configuration options in the WebSocket client handle. The options are applied automatically when the client connects via sl_websocket_connect. Call this function after sl_websocket_init and before connecting.
sl_websocket_init should be called before this function.
Returns
sl_websocket_error_t - Error code indicating the result of the operation.
sl_websocket_set_origin#
sl_websocket_error_t sl_websocket_set_origin (sl_websocket_client_t * handle, const char * origin)
Sets the Origin header value for a WebSocket client.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_websocket_client_t * | [in] | handle | Pointer to the WebSocket client structure. Must not be NULL. |
| const char * | [in] | origin | Null-terminated Origin header value (for example, "https://example.com"). Must not be NULL or an empty string. Maximum length is SL_SI91X_WEBSOCKET_MAX_ORIGIN_LENGTH - 1 characters (excluding the null terminator). |
Stores the Origin header value in the WebSocket client handle. The value is sent to the NWP during sl_websocket_connect as part of the HTTP upgrade handshake. Call after sl_websocket_init and before connecting.
sl_websocket_init should be called before this function.
Returns
SL_WEBSOCKET_SUCCESS on success.
SL_WEBSOCKET_ERR_INVALID_PARAMETER if
handleis NULL,originis NULL or empty, or if the client is not in SL_WEBSOCKET_STATE_DISCONNECTED.SL_WEBSOCKET_ERR_MAX_LENGTH_EXCEEDED if
originlength is greater than or equal to SL_SI91X_WEBSOCKET_MAX_ORIGIN_LENGTH.
sl_si91x_get_opcode_from_socket_id#
sl_websocket_opcode_t sl_si91x_get_opcode_from_socket_id (uint16_t socket_id)
Extracts the WebSocket opcode from a given socket ID.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | socket_id | The 16-bit socket ID from which to extract the opcode. |
This function determines the opcode of the WebSocket from the socket ID. The socket_id is obtained from the recv_data_callback from the sl_si91x_socket_metadata_t parameter.
Returns
sl_websocket_opcode_t - The extracted WebSocket opcode.