Wi-SUN Util#
Functions#
sl_status_t
sl_wisun_util_get_rf_settings(uint8_t *reg_domain, uint8_t *op_class, uint16_t *op_mode)
Get frequency band settings from RAIL config.
sl_status_t
sl_wisun_util_connect(const uint8_t *network_name)
Connect to a Wi-SUN network.
Function Documentation#
sl_wisun_util_get_rf_settings#
sl_status_t sl_wisun_util_get_rf_settings (uint8_t * reg_domain, uint8_t * op_class, uint16_t * op_mode)
Get frequency band settings from RAIL config.
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t * | [out] | reg_domain | Regulatory domain of the Wi-SUN network |
| uint8_t * | [out] | op_class | Operational class of the Wi-SUN network |
| uint16_t * | [out] | op_mode | Operational mode of the Wi-SUN network |
Returns
SL_STATUS_OK if successful, an error code otherwise
sl_wisun_util_connect#
sl_status_t sl_wisun_util_connect (const uint8_t * network_name)
Connect to a Wi-SUN network.
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const uint8_t * | [in] | network_name | Name of the Wi-SUN network as a zero-terminated string |
Wi-SUN frequency band settings are deduced from RAIL config. Returns
SL_STATUS_OK if successful, an error code otherwise