You are viewing documentation for version:1.10.2Indication message body. Public Attributes#uint32_tstatusStatus of the indication. uint64_ttimestamp_usTimestamp in microseconds. uint16_tlengthFrame length in bytes. uint8_tframeReceived frame. Public Attribute Documentation#status#uint32_t sl_wisun_msg_rx_frame_ind_body_t::statusStatus of the indication. timestamp_us#uint64_t sl_wisun_msg_rx_frame_ind_body_t::timestamp_usTimestamp in microseconds. length#uint16_t sl_wisun_msg_rx_frame_ind_body_t::lengthFrame length in bytes. frame#uint8_t sl_wisun_msg_rx_frame_ind_body_t::frame[]Received frame.