Socket API#

Modules#

sockaddr

in6_addr

sockaddr_in6

Protocol levels used for socket_setsockopt.#

#define

Socket option level.

#define

Application socket option level.

#define

IPV6 socket option level.

application level socket options#

application level socket options summaryopt_name data type set/get sendmsg recvmsg SO_EVENT_MODE int16_t Set only No Yes SO_NONBLOCK int16_t Set only Yes Yes

#define

Specify event mode of a socket. When set, optval must point to an uint32_t.

Possible values are:

#define
SOCKET_EVENT_MODE SO_EVENT_MODE

Specify event mode of a socket. When set, optval must point to an uint32_t.

Possible values are:

#define

Enable/disable nonblocking mode.

socket level options#

socket level options summaryopt_name data type set/get sendmsg recvmsg SO_RCVBUF int32_t Set/Get No Yes SO_SNDBUF int32_t Set/Get Yes No SO_SNDLOWAT int32_t Set/Get Yes No

#define

Specify receive buffer size in payload bytes. When set, optval must point to an int32_t.

0 means unread data are dropped, unless read in data callback.

#define

Specify send buffer size in payload bytes.

#define

Specify send low water mark in payload bytes.

IPv6 socket options#

IPv6 socket options summaryopt_name Data type set/getsockopt sendmsg recvmsg IPV6_UNICAST_HOPS int16_t Set/Get Yes No IPV6_MULTICAST_HOPS int16_t Set/Get Yes No IPV6_JOIN_GROUP ns_ipv6_mreq_t Set only Yes Yes IPV6_LEAVE_GROUP ns_ipv6_mreq_t Set only Yes Yes SO_EDFE_MODE uint32_t Set only Yes No

#define

Set the unicast hop limit for the socket. When set, optval must point to an int16_t.

-1 in the value means use the route default, otherwise it should be between 0 and 255.

#define

Set the multicast hop limit for the socket.

#define

Join a multicast group.

#define

Leave a multicast group.

#define

Experimental: Enable Extended Directed Frame Exchange mode.

#define
SOCKET_EDFE_MODE SO_EDFE_MODE

Set the unicast hop limit for the socket. When set, optval must point to an int16_t.

-1 in the value means use the route default, otherwise it should be between 0 and 255.

Enumerations#

enum
SL_WISUN_SOCKET_EVENT_MODE_INDICATION = 0
SL_WISUN_SOCKET_EVENT_MODE_POLLING = 1
}

Enumerations for socket event mode.

enum
AF_INET6 = 0
}

Supported address families.

enum
SOCK_STREAM = 1
SOCK_DGRAM = 2
SOCK_RAW = 3
}

Socket types.

enum
IPPROTO_IP = 0
IPPROTO_ICMP = 1
IPPROTO_TCP = 2
IPPROTO_UDP = 3
}

IP protocols.

Typedefs#

typedef uint32_t

Socket address length type definition.

typedef int32_t
typedef enum socket_domain

Supported address families.

typedef enum socket_type

Socket types.

typedef enum socket_protocol

IP protocols.

typedef struct in6_addr

IPv6 Internet address.

typedef struct sockaddr_in6

IPv6 address format.

Variables#

IPv6 wildcard address.

Functions#

int32_t
socket(int32_t domain, int32_t type, int32_t protocol)

Creates an endpoint for communication and returns an Id that refers to that endpoint.

int32_t
close(int32_t sockid)

Close a socket.

int32_t
bind(int32_t sockid, const struct sockaddr *addr, socklen_t addrlen)

Bind a name to a socket.

int32_t
send(int32_t sockid, const void *buff, uint32_t len, int32_t flags)

Send a message on a socket.

int32_t
sendto(int32_t sockid, const void *buff, uint32_t len, int32_t flags, const struct sockaddr *dest_addr, socklen_t addr_len)

Send a message to a given address.

int32_t
recvfrom(int32_t sockid, void *buf, uint32_t len, int32_t flags, struct sockaddr *src_addr, socklen_t *addrlen)

Receive messages from a socket.

int32_t
recv(int32_t sockid, void *buf, uint32_t len, int32_t flags)

Receive a message from a socket.

int32_t
accept(int32_t sockid, struct sockaddr *addr, socklen_t *addrlen)

Accept a connection on a socket.

int32_t
connect(int32_t sockid, const struct sockaddr *addr, socklen_t addrlen)

Initiate a connection on a socket.

int32_t
listen(int32_t sockid, int32_t backlog)

Listen for connections on a socket.

int32_t
setsockopt(int32_t sockid, int32_t level, int32_t optname, const void *optval, socklen_t optlen)

Set socket option designated by optname at a given protocol level to the value pointed by optval.

int32_t
getsockopt(int32_t sockid, int32_t level, int32_t optname, void *optval, socklen_t *optlen)

Get socket option.

__STATIC_INLINE uint32_t
htonl(uint32_t hostlong)

Convert the long host byte order to network order.

__STATIC_INLINE uint16_t
htons(uint16_t hostshort)

Convert the short host byte order to network order.

__STATIC_INLINE uint32_t
ntohl(uint32_t netlong)

Convert the long network byte order to host byte order.

__STATIC_INLINE uint16_t
ntohs(uint16_t netshort)

Convert the short network byte order to host byte order.

int32_t
inet_pton(int32_t af, const char *src, void *dst)

Convert the IPv4 and IPv6 addresses from text to binary form.

const char *
inet_ntop(int32_t af, const void *src, char *dst, socklen_t size)

Convert IPv6 addresses from binary to text form.

Macros#

#define
APP_LEVEL_SOCKET SOL_APPLICATION
#define

Size of an IPv6 address.

#define
SOCK_NONBLOCK 0X00010000

When bitwise ored with socket's type, it sets the O_NONBLOCK status flag on the opened socket file description.

Protocol levels used for socket_setsockopt. Documentation#

SOL_SOCKET#

#define SOL_SOCKET
Value:
0

Socket option level.


SOL_APPLICATION#

#define SOL_APPLICATION
Value:
1

Application socket option level.


IPPROTO_IPV6#

#define IPPROTO_IPV6
Value:
41

IPV6 socket option level.


application level socket options Documentation#

SO_EVENT_MODE#

#define SO_EVENT_MODE
Value:
10

Specify event mode of a socket. When set, optval must point to an uint32_t.

Possible values are:


SOCKET_EVENT_MODE#

#define SOCKET_EVENT_MODE
Value:
SO_EVENT_MODE

Specify event mode of a socket. When set, optval must point to an uint32_t.

Possible values are:


SO_NONBLOCK#

#define SO_NONBLOCK
Value:
11

Enable/disable nonblocking mode.

This option takes an uint32_t value.

Possible values are:

  • (1) enables nonblocking mode

  • (0) disables nonblocking mode


socket level options Documentation#

SO_RCVBUF#

#define SO_RCVBUF
Value:
1

Specify receive buffer size in payload bytes. When set, optval must point to an int32_t.

0 means unread data are dropped, unless read in data callback.


SO_SNDBUF#

#define SO_SNDBUF
Value:
2

Specify send buffer size in payload bytes.

When set, optval must point to an int32_t.

Used only for stream sockets.


SO_SNDLOWAT#

#define SO_SNDLOWAT
Value:
4

Specify send low water mark in payload bytes.

When set, optval must point to an int32_t.


IPv6 socket options Documentation#

IPV6_UNICAST_HOPS#

#define IPV6_UNICAST_HOPS
Value:
2

Set the unicast hop limit for the socket. When set, optval must point to an int16_t.

-1 in the value means use the route default, otherwise it should be between 0 and 255.


IPV6_MULTICAST_HOPS#

#define IPV6_MULTICAST_HOPS
Value:
3

Set the multicast hop limit for the socket.

When set, optval must point to an int16_t.

-1 in the value means use the route default, otherwise it should be between 0 and 255.


IPV6_JOIN_GROUP#

#define IPV6_JOIN_GROUP
Value:
15

Join a multicast group.

When set, optval must point to an in6_addr_t.


IPV6_LEAVE_GROUP#

#define IPV6_LEAVE_GROUP
Value:
16

Leave a multicast group.

When set, optval must point to an in6_addr_t.


SO_EDFE_MODE#

#define SO_EDFE_MODE
Value:
0xfb

Experimental: Enable Extended Directed Frame Exchange mode.

When set, optval must point to an uint32_t.


SOCKET_EDFE_MODE#

#define SOCKET_EDFE_MODE
Value:
SO_EDFE_MODE

Set the unicast hop limit for the socket. When set, optval must point to an int16_t.

-1 in the value means use the route default, otherwise it should be between 0 and 255.


Enumeration Documentation#

sl_wisun_socket_event_mode_t#

sl_wisun_socket_event_mode_t

Enumerations for socket event mode.

Enumerator
SL_WISUN_SOCKET_EVENT_MODE_INDICATION

SL_WISUN_MSG_SOCKET_DATA_IND_ID is sent to the app with the packet contained in the indication.

SL_WISUN_SOCKET_EVENT_MODE_POLLING

SL_WISUN_MSG_SOCKET_DATA_AVAILABLE_IND_ID is sent to the app indicating the amount of data received recv() or recvfrom() should be invoked after indication reception to retrieve data This is the default socket event mode option.


socket_domain#

socket_domain

Supported address families.

Enumerator
AF_INET6

IP version 6.


socket_type#

socket_type

Socket types.

Enumerator
SOCK_STREAM

stream (connection) socket (TCP)

SOCK_DGRAM

datagram (connectionless ) socket (UDP)

SOCK_RAW

raw socket


socket_protocol#

socket_protocol

IP protocols.

Enumerator
IPPROTO_IP

Dummy protocol.

IPPROTO_ICMP

Internet Control Message Protocol.

IPPROTO_TCP

Transmission Control Protocol.

IPPROTO_UDP

User Datagram Protocol.


Typedef Documentation#

socklen_t#

typedef uint32_t socklen_t

Socket address length type definition.


sl_wisun_socket_id_t#

typedef int32_t sl_wisun_socket_id_t

Socket id.


sl_socket_domain_t#

typedef enum socket_domain sl_socket_domain_t

Supported address families.


sl_socket_type_t#

typedef enum socket_type sl_socket_type_t

Socket types.


sl_socket_protocol_t#

typedef enum socket_protocol sl_socket_protocol_t

IP protocols.


in6_addr_t#

typedef struct in6_addr in6_addr_t

IPv6 Internet address.


sockaddr_in6_t#

typedef struct sockaddr_in6 sockaddr_in6_t

IPv6 address format.


Variable Documentation#

in6addr_any#

const in6_addr_t in6addr_any

IPv6 wildcard address.


Function Documentation#

socket#

int32_t socket (int32_t domain, int32_t type, int32_t protocol)

Creates an endpoint for communication and returns an Id that refers to that endpoint.

Parameters
TypeDirectionArgument NameDescription
int32_t[in]domain

Specifies a communication domain. It selects the protocol family which will be used for communication. Must be set to AF_INET6 (IPv6 network socket)

int32_t[in]type

The communication semantics It can be:

int32_t[in]protocol

Specifies the particular protocol to be used. It can be:

Returns

  • The socket's id on success, (-1) on failure.


close#

int32_t close (int32_t sockid)

Close a socket.

Parameters
TypeDirectionArgument NameDescription
int32_t[in]sockid

socket id

Returns

  • 0 on success, -1 on failure.

Close a socket and remove from the socket handler storage.


bind#

int32_t bind (int32_t sockid, const struct sockaddr * addr, socklen_t addrlen)

Bind a name to a socket.

Parameters
TypeDirectionArgument NameDescription
int32_t[in]sockid

socket id

const struct sockaddr *[in]addr

address structure ptr

socklen_t[in]addrlen

address structure size

Returns

  • 0 on success, -1 on failure.

Assigns the address to the socket, referred to by the socket ID, as specified by addr. It is normally necessary to assign a local address using bind() before a SOCK_STREAM socket may receive connections.


send#

int32_t send (int32_t sockid, const void * buff, uint32_t len, int32_t flags)

Send a message on a socket.

Parameters
TypeDirectionArgument NameDescription
int32_t[in]sockid

socket descriptor.

const void *[in]buff

pointer to data buffer to send.

uint32_t[in]len

length of data buffer to send.

int32_t[in]flags

flags to select send options. Ignored in our implementation.

Returns

  • The number of bytes sent on success, -1 if an error occurred.

Preferred with connection-oriented sockets (TCP).


sendto#

int32_t sendto (int32_t sockid, const void * buff, uint32_t len, int32_t flags, const struct sockaddr * dest_addr, socklen_t addr_len)

Send a message to a given address.

Parameters
TypeDirectionArgument NameDescription
int32_t[in]sockid

socket descriptor.

const void *[in]buff

pointer to data buffer to send.

uint32_t[in]len

length of data buffer to send.

int32_t[in]flags

flags to select send options. Ignored in our implementation.

const struct sockaddr *[in]dest_addr

pointer to destination address buffer; Required for datagram sockets.

socklen_t[in]addr_len

length of destination address buffer.

Returns

  • The number of bytes sent on success, -1 if an error occurred.

Preferred in datagram mode (UDP).


recvfrom#

int32_t recvfrom (int32_t sockid, void * buf, uint32_t len, int32_t flags, struct sockaddr * src_addr, socklen_t * addrlen)

Receive messages from a socket.

Parameters
TypeDirectionArgument NameDescription
int32_t[in]sockid

descriptor of socket to receive the message from.

void *[out]buf

pointer to destination data buffer.

uint32_t[in]len

length of destination data buffer.

int32_t[in]flags

flags to select type of message reception. Ignored in our implementation.

struct sockaddr *[in]src_addr

pointer to a sockaddr structure in which the sending address is to be stored.

socklen_t *[in]addrlen

length of the supplied sockaddr structure.

Returns

  • The number of bytes received on success, -1 if an error occurred.

Receives data on a socket whether or not it is connection-oriented.


recv#

int32_t recv (int32_t sockid, void * buf, uint32_t len, int32_t flags)

Receive a message from a socket.

Parameters
TypeDirectionArgument NameDescription
int32_t[in]sockid

descriptor of socket to receive the message from.

void *[out]buf

pointer to destination data buffer.

uint32_t[in]len

length of destination data buffer.

int32_t[in]flags

flags to select type of message reception. Ignored in our implementation.

Returns

  • The number of bytes received on success, -1 if an error occurred.

Should be used for connection-oriented protocol (TCP)


accept#

int32_t accept (int32_t sockid, struct sockaddr * addr, socklen_t * addrlen)

Accept a connection on a socket.

Parameters
TypeDirectionArgument NameDescription
int32_t[in]sockid

socket descriptor

struct sockaddr *[inout]addr

A pointer to sockaddr structure filled in with the address of the peer (remote) socket. When addr is NULL, nothing is filled in; in this case, addrlen is not used, and should also be NULL.

socklen_t *[inout]addrlen

The caller must initialize it to contain the size (in bytes) of the structure pointed to by addr. On return it will contain the actual size of the peer address.

Returns

  • The socket id of the accepted socket on success, -1 if an error occurred.

Used with connection-based socket types (TCP). It extracts the first connection request on the queue of pending connections for the listening socket.


connect#

int32_t connect (int32_t sockid, const struct sockaddr * addr, socklen_t addrlen)

Initiate a connection on a socket.

Parameters
TypeDirectionArgument NameDescription
int32_t[in]sockid

socket descriptor.

const struct sockaddr *[in]addr

If the socket sockid is of type SOCK_DGRAM, addr is the address to which datagrams are sent by default and the only address from which datagrams are received. If the socket is of type SOCK_STREAM, this call attempts to make a connection to the socket that is bound to the address specified by addr.

socklen_t[in]addrlen

length of the supplied sockaddr structure.

Returns

  • 0 on connection or binding success, -1 if an error occurred.

Connects the socket referred to by the sockid to the address specified by address.


listen#

int32_t listen (int32_t sockid, int32_t backlog)

Listen for connections on a socket.

Parameters
TypeDirectionArgument NameDescription
int32_t[in]sockid

socket id

int32_t[in]backlog

Argument defines the maximum length to which the queue of pending connections for sockid may grow. Not implemented for Wi-SUN, the connection queue size is always 1

Returns

  • 0 on success, -1 if an error occurred.

Marks the socket referred to by sockid as a passive socket, that is, as a socket that will be used to accept incoming connection requests using accept.


setsockopt#

int32_t setsockopt (int32_t sockid, int32_t level, int32_t optname, const void * optval, socklen_t optlen)

Set socket option designated by optname at a given protocol level to the value pointed by optval.

Parameters
TypeDirectionArgument NameDescription
int32_t[in]sockid

socket ID

int32_t[in]level

protocol level at which the option resides. it could be:

int32_t[in]optname

option name. it could be:

const void *[in]optval

Pointer to the socket option new value. The type of variable pointed by optval depends level and optname values.

socklen_t[in]optlen

Must be the size of the symbol pointed by optval.

Returns

  • 0 on success, -1 if an error occurred.

This function can set socket properties.


getsockopt#

int32_t getsockopt (int32_t sockid, int32_t level, int32_t optname, void * optval, socklen_t * optlen)

Get socket option.

Parameters
TypeDirectionArgument NameDescription
int32_t[in]sockid

socket descriptor.

int32_t[in]level

socket protocol level.

int32_t[in]optname

Option name. Supported options:

void *[out]optval

option value structure pointer.

socklen_t *[in]optlen

size of the option value structure.

Returns

  • 0 on success, -1 if an error occurred.

The function gets socket option by optname, and copies option data to optval ptr.


htonl#

__STATIC_INLINE uint32_t htonl (uint32_t hostlong)

Convert the long host byte order to network order.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]hostlong

Long host integer

Returns

  • Long network integer

This function converts the unsigned integer hostlong from host byte order to network byte order. For Wi-SUN, the conversion is not needed. Dummy implementation


htons#

__STATIC_INLINE uint16_t htons (uint16_t hostshort)

Convert the short host byte order to network order.

Parameters
TypeDirectionArgument NameDescription
uint16_t[in]hostshort

Short host integer

Returns

  • Short network integer

This function converts the unsigned short integer hostshort from host byte order to network byte order. For Wi-SUN, the conversion is not needed. Dummy implementation


ntohl#

__STATIC_INLINE uint32_t ntohl (uint32_t netlong)

Convert the long network byte order to host byte order.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]netlong

Long network integer

Returns

  • Long host integer

This function converts the unsigned integer netlong from network byte order to host byte order. For Wi-SUN, the conversion is not needed. Dummy implementation


ntohs#

__STATIC_INLINE uint16_t ntohs (uint16_t netshort)

Convert the short network byte order to host byte order.

Parameters
TypeDirectionArgument NameDescription
uint16_t[in]netshort

Returns

  • Short host integer

This function converts the unsigned short integer netshort from the network byte order to host byte order.For Wi-SUN, the conversion is not needed. Dummy implementation.


inet_pton#

int32_t inet_pton (int32_t af, const char * src, void * dst)

Convert the IPv4 and IPv6 addresses from text to binary form.

Parameters
TypeDirectionArgument NameDescription
int32_t[in]af

The address family. Only AF_INET6 is supported by our implementation.

const char *[in]src

Source string

void *[out]dst

Destination address pointer

Returns

  • 1 on succes, -1 if an error occurred. (POSIX described the 0 value too)

This function converts the character string src into a network address structure in the af address family, then copies the network address structure to dst. AF_INET (IPv4) case not supported.


inet_ntop#

const char * inet_ntop (int32_t af, const void * src, char * dst, socklen_t size)

Convert IPv6 addresses from binary to text form.

Parameters
TypeDirectionArgument NameDescription
int32_t[in]af

- Address family.

  • Only AF_INET6 is supported

const void *[in]src

Source address in byte form

char *[out]dst

Destination buffer ptr

socklen_t[in]size

Size of the destination buffer.

Returns

  • It returns a non-null pointer to dst. NULL if an error occurred.

Converts the network address structure src in the af address family into a character string. The resulting string is copied to the buffer pointed to by dst, which must be a non-null pointer. The caller specifies the number of bytes available in this buffer in the argument size. AF_INET (IPv4) case not supported.


Macro Definition Documentation#

APP_LEVEL_SOCKET#

#define APP_LEVEL_SOCKET
Value:
SOL_APPLICATION

IPV6_ADDR_SIZE#

#define IPV6_ADDR_SIZE
Value:
16

Size of an IPv6 address.


SOCK_NONBLOCK#

#define SOCK_NONBLOCK
Value:
0X00010000

When bitwise ored with socket's type, it sets the O_NONBLOCK status flag on the opened socket file description.