RPL neighbor information.

Public Attributes#

ULA/GUA address (unspecified address :: if unknown)

uint32_t

Neighbor type.

uint32_t

Remaining lifetime (Link lifetime for parents, ARO lifetime for children)

uint32_t

MAC TX packet count.

uint32_t

MAC TX failed count.

uint16_t

RPL Rank value for parents (0xffff if unknown or child)

uint16_t

Measured ETX value if known (0xffff if unknown)

uint8_t
uint8_t

Public Attribute Documentation#

link_local_address#

sl_wisun_ip_address_t sl_wisun_neighbor_info_t::link_local_address

Link-local address.


global_address#

sl_wisun_ip_address_t sl_wisun_neighbor_info_t::global_address

ULA/GUA address (unspecified address :: if unknown)


type#

uint32_t sl_wisun_neighbor_info_t::type

Neighbor type.


lifetime#

uint32_t sl_wisun_neighbor_info_t::lifetime

Remaining lifetime (Link lifetime for parents, ARO lifetime for children)


mac_tx_count#

uint32_t sl_wisun_neighbor_info_t::mac_tx_count

MAC TX packet count.


mac_tx_failed_count#

uint32_t sl_wisun_neighbor_info_t::mac_tx_failed_count

MAC TX failed count.


rpl_rank#

uint16_t sl_wisun_neighbor_info_t::rpl_rank

RPL Rank value for parents (0xffff if unknown or child)


etx#

uint16_t sl_wisun_neighbor_info_t::etx

Measured ETX value if known (0xffff if unknown)


rsl_out#

uint8_t sl_wisun_neighbor_info_t::rsl_out

Parent RSSI Out measured RSSI value (0xff if unknown) Calculated using EWMA specified by Wi-SUN from range of -174 (0) to +80 (254) dBm.


rsl_in#

uint8_t sl_wisun_neighbor_info_t::rsl_in

Parent RSSI In measured RSSI value (0xff if unknown) Calculated using EWMA specified by Wi-SUN from range of -174 (0) to +80 (254) dBm.