Util Functions#
The Util Functions component provides helper functions to inform the application about the Wi-SUN PHY configured in the RAIL configuration file.
Functions#
Get frequency band settings of the first RAIL configuration listed in RAIL's channelConfigs array.
Connect to a Wi-SUN network.
Function Documentation#
sl_wisun_util_get_rf_settings#
sl_status_t sl_wisun_util_get_rf_settings (uint8_t * reg_domain, uint8_t * op_class, uint16_t * op_mode)
Get frequency band settings of the first RAIL configuration listed in RAIL's channelConfigs array.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t * | [out] | reg_domain | Regulatory domain of the Wi-SUN network |
| uint8_t * | [out] | op_class | Operational class of the Wi-SUN network |
| uint16_t * | [out] | op_mode | Operational mode of the Wi-SUN network |
Returns
SL_STATUS_OK if successful, an error code otherwise
sl_wisun_util_connect#
sl_status_t sl_wisun_util_connect (const uint8_t * network_name)
Connect to a Wi-SUN network.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const uint8_t * | [in] | network_name | Name of the Wi-SUN network as a zero-terminated string |
Since Wi-SUN frequency band settings are deduced from first RAIL configuration listed in RAIL's channelConfigs array, using this function is not recommended if more than one RAIL configuration is described. Returns
SL_STATUS_OK if successful, an error code otherwise