Indication message body.
Public Attributes#
uint32_t
Status of the indication.
uint32_t
Sum of transmission durations during last hour in milliseconds.
uint8_t
Transmission level, one value of sl_wisun_regulation_tx_level_t.
uint8_t
Reserved.
Public Attribute Documentation#
status#
uint32_t sl_wisun_msg_regulation_tx_level_ind_body_t::status
Status of the indication.
Definition at line
415
of file /mnt/raid/workspaces/ws.fy2OGuDyK/overlay/super/protocol/wisun/stack/inc/sl_wisun_events.h
tx_duration_ms#
uint32_t sl_wisun_msg_regulation_tx_level_ind_body_t::tx_duration_ms
Sum of transmission durations during last hour in milliseconds.
Definition at line
417
of file /mnt/raid/workspaces/ws.fy2OGuDyK/overlay/super/protocol/wisun/stack/inc/sl_wisun_events.h
tx_level#
uint8_t sl_wisun_msg_regulation_tx_level_ind_body_t::tx_level
Transmission level, one value of sl_wisun_regulation_tx_level_t.
Definition at line
419
of file /mnt/raid/workspaces/ws.fy2OGuDyK/overlay/super/protocol/wisun/stack/inc/sl_wisun_events.h
reserved#
uint8_t sl_wisun_msg_regulation_tx_level_ind_body_t::reserved[3]
Reserved.
Definition at line
421
of file /mnt/raid/workspaces/ws.fy2OGuDyK/overlay/super/protocol/wisun/stack/inc/sl_wisun_events.h