MAC statistics.
Public Attributes#
Current number of frames in the MAC transmission queue.
Highest number of frames in the MAC transmission queue.
Number of successfully received MAC frames.
Number of transmitted MAC frames.
Number of successfully received broadcast MAC frames.
Number of transmitted broadcast MAC frames.
Number of successfully received MAC frames discarded during processing.
Amount of transmitted MAC data in bytes. FCS is not included.
Amount of successfully received MAC data in bytes. FCS is not included.
Number of failed MAC transmissions.
Number of retried MAC transmissions.
Number of MAC CCA attempts.
Number of failed MAC transmissions due to CCA.
Number of successfully received MAC frames using mode_switch.
Number of transmitted MAC frames using mode switch.
Number of failed reception using mode switch (no data after PHR or MDR Command).
Number of failed MAC frames transmission using mode switch.
Public Attribute Documentation#
tx_queue_size#
uint16_t sl_wisun_statistics_mac_t::tx_queue_size
Current number of frames in the MAC transmission queue.
296
of file /mnt/raid/workspaces/ws.fy2OGuDyK/overlay/super/protocol/wisun/stack/inc/sl_wisun_types.h
tx_queue_peak#
uint16_t sl_wisun_statistics_mac_t::tx_queue_peak
Highest number of frames in the MAC transmission queue.
298
of file /mnt/raid/workspaces/ws.fy2OGuDyK/overlay/super/protocol/wisun/stack/inc/sl_wisun_types.h
rx_count#
uint32_t sl_wisun_statistics_mac_t::rx_count
Number of successfully received MAC frames.
300
of file /mnt/raid/workspaces/ws.fy2OGuDyK/overlay/super/protocol/wisun/stack/inc/sl_wisun_types.h
tx_count#
uint32_t sl_wisun_statistics_mac_t::tx_count
Number of transmitted MAC frames.
302
of file /mnt/raid/workspaces/ws.fy2OGuDyK/overlay/super/protocol/wisun/stack/inc/sl_wisun_types.h
bc_rx_count#
uint32_t sl_wisun_statistics_mac_t::bc_rx_count
Number of successfully received broadcast MAC frames.
304
of file /mnt/raid/workspaces/ws.fy2OGuDyK/overlay/super/protocol/wisun/stack/inc/sl_wisun_types.h
bc_tx_count#
uint32_t sl_wisun_statistics_mac_t::bc_tx_count
Number of transmitted broadcast MAC frames.
306
of file /mnt/raid/workspaces/ws.fy2OGuDyK/overlay/super/protocol/wisun/stack/inc/sl_wisun_types.h
rx_drop_count#
uint32_t sl_wisun_statistics_mac_t::rx_drop_count
Number of successfully received MAC frames discarded during processing.
308
of file /mnt/raid/workspaces/ws.fy2OGuDyK/overlay/super/protocol/wisun/stack/inc/sl_wisun_types.h
tx_bytes#
uint32_t sl_wisun_statistics_mac_t::tx_bytes
Amount of transmitted MAC data in bytes. FCS is not included.
310
of file /mnt/raid/workspaces/ws.fy2OGuDyK/overlay/super/protocol/wisun/stack/inc/sl_wisun_types.h
rx_bytes#
uint32_t sl_wisun_statistics_mac_t::rx_bytes
Amount of successfully received MAC data in bytes. FCS is not included.
312
of file /mnt/raid/workspaces/ws.fy2OGuDyK/overlay/super/protocol/wisun/stack/inc/sl_wisun_types.h
tx_failed_count#
uint32_t sl_wisun_statistics_mac_t::tx_failed_count
Number of failed MAC transmissions.
314
of file /mnt/raid/workspaces/ws.fy2OGuDyK/overlay/super/protocol/wisun/stack/inc/sl_wisun_types.h
retry_count#
uint32_t sl_wisun_statistics_mac_t::retry_count
Number of retried MAC transmissions.
316
of file /mnt/raid/workspaces/ws.fy2OGuDyK/overlay/super/protocol/wisun/stack/inc/sl_wisun_types.h
cca_attempts_count#
uint32_t sl_wisun_statistics_mac_t::cca_attempts_count
Number of MAC CCA attempts.
318
of file /mnt/raid/workspaces/ws.fy2OGuDyK/overlay/super/protocol/wisun/stack/inc/sl_wisun_types.h
failed_cca_count#
uint32_t sl_wisun_statistics_mac_t::failed_cca_count
Number of failed MAC transmissions due to CCA.
320
of file /mnt/raid/workspaces/ws.fy2OGuDyK/overlay/super/protocol/wisun/stack/inc/sl_wisun_types.h
rx_ms_count#
uint32_t sl_wisun_statistics_mac_t::rx_ms_count
Number of successfully received MAC frames using mode_switch.
322
of file /mnt/raid/workspaces/ws.fy2OGuDyK/overlay/super/protocol/wisun/stack/inc/sl_wisun_types.h
tx_ms_count#
uint32_t sl_wisun_statistics_mac_t::tx_ms_count
Number of transmitted MAC frames using mode switch.
324
of file /mnt/raid/workspaces/ws.fy2OGuDyK/overlay/super/protocol/wisun/stack/inc/sl_wisun_types.h
rx_ms_failed_count#
uint32_t sl_wisun_statistics_mac_t::rx_ms_failed_count
Number of failed reception using mode switch (no data after PHR or MDR Command).
326
of file /mnt/raid/workspaces/ws.fy2OGuDyK/overlay/super/protocol/wisun/stack/inc/sl_wisun_types.h
tx_ms_failed_count#
uint32_t sl_wisun_statistics_mac_t::tx_ms_failed_count
Number of failed MAC frames transmission using mode switch.
328
of file /mnt/raid/workspaces/ws.fy2OGuDyK/overlay/super/protocol/wisun/stack/inc/sl_wisun_types.h