Indication message body.

Public Attributes#

uint32_t

Status of the indication.

uint32_t

Sum of transmission durations during last hour in milliseconds.

uint8_t

Transmission level, one value of sl_wisun_regulation_tx_level_t.

uint8_t

Reserved.

Public Attribute Documentation#

status#

uint32_t sl_wisun_msg_regulation_tx_level_ind_body_t::status

Status of the indication.


Definition at line 417 of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_events.h

tx_duration_ms#

uint32_t sl_wisun_msg_regulation_tx_level_ind_body_t::tx_duration_ms

Sum of transmission durations during last hour in milliseconds.


Definition at line 419 of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_events.h

tx_level#

uint8_t sl_wisun_msg_regulation_tx_level_ind_body_t::tx_level

Transmission level, one value of sl_wisun_regulation_tx_level_t.


Definition at line 421 of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_events.h

reserved#

uint8_t sl_wisun_msg_regulation_tx_level_ind_body_t::reserved[3]

Reserved.


Definition at line 423 of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_events.h