Indication message body.
Public Attributes#
uint32_t
Status of the indication.
uint32_t
ID of the socket.
uint32_t
Amount of free space in the transmission buffer.
Public Attribute Documentation#
status#
uint32_t sl_wisun_msg_socket_data_sent_ind_body_t::status
Status of the indication.
Definition at line
336
of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_events.h
socket_id#
uint32_t sl_wisun_msg_socket_data_sent_ind_body_t::socket_id
ID of the socket.
Definition at line
338
of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_events.h
socket_space_left#
uint32_t sl_wisun_msg_socket_data_sent_ind_body_t::socket_space_left
Amount of free space in the transmission buffer.
Definition at line
340
of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_events.h