Statistic ping type definition.

Public Attributes#

Wi-SUN remote address.

uint16_t

Packet count.

uint16_t

Packet length.

uint16_t

Lost packet count.

uint32_t

Minimum echo time millisecond.

uint32_t

Maximum echo time millisecond.

uint32_t

Average echo time millisecond.

Public Attribute Documentation#

remote_addr#

wisun_addr_t sl_wisun_ping_stat::remote_addr

Wi-SUN remote address.


Definition at line 129 of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/app/wisun/component/ping/sl_wisun_ping.h

packet_count#

uint16_t sl_wisun_ping_stat::packet_count

Packet count.


Definition at line 131 of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/app/wisun/component/ping/sl_wisun_ping.h

packet_length#

uint16_t sl_wisun_ping_stat::packet_length

Packet length.


Definition at line 133 of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/app/wisun/component/ping/sl_wisun_ping.h

lost#

uint16_t sl_wisun_ping_stat::lost

Lost packet count.


Definition at line 135 of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/app/wisun/component/ping/sl_wisun_ping.h

min_time_ms#

uint32_t sl_wisun_ping_stat::min_time_ms

Minimum echo time millisecond.


Definition at line 137 of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/app/wisun/component/ping/sl_wisun_ping.h

max_time_ms#

uint32_t sl_wisun_ping_stat::max_time_ms

Maximum echo time millisecond.


Definition at line 139 of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/app/wisun/component/ping/sl_wisun_ping.h

avg_time_ms#

uint32_t sl_wisun_ping_stat::avg_time_ms

Average echo time millisecond.


Definition at line 141 of file /mnt/raid/workspaces/ws.VedEDj2Fn/overlay/gsdk/app/wisun/component/ping/sl_wisun_ping.h