iPerf Client Header extended
Public Attributes#
int32_t
Type.
int32_t
Length.
int16_t
Upper flags.
int16_t
Lower flags.
uint32_t
Upper version.
uint32_t
Lower version.
uint16_t
Reserved.
uint16_t
Tos.
uint32_t
Lower rate.
uint32_t
Upper rate.
uint32_t
TCP write prefetch.
Public Attribute Documentation#
type#
int32_t sl_iperf_clnt_hdr_ext::type
Type.
Definition at line
356
of file /mnt/raid/workspaces/ws.Mae4JfP9d/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h
length#
int32_t sl_iperf_clnt_hdr_ext::length
Length.
Definition at line
358
of file /mnt/raid/workspaces/ws.Mae4JfP9d/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h
u_flags#
int16_t sl_iperf_clnt_hdr_ext::u_flags
Upper flags.
Definition at line
360
of file /mnt/raid/workspaces/ws.Mae4JfP9d/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h
l_flags#
int16_t sl_iperf_clnt_hdr_ext::l_flags
Lower flags.
Definition at line
362
of file /mnt/raid/workspaces/ws.Mae4JfP9d/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h
u_version#
uint32_t sl_iperf_clnt_hdr_ext::u_version
Upper version.
Definition at line
364
of file /mnt/raid/workspaces/ws.Mae4JfP9d/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h
l_version#
uint32_t sl_iperf_clnt_hdr_ext::l_version
Lower version.
Definition at line
366
of file /mnt/raid/workspaces/ws.Mae4JfP9d/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h
reserved#
uint16_t sl_iperf_clnt_hdr_ext::reserved
Reserved.
Definition at line
368
of file /mnt/raid/workspaces/ws.Mae4JfP9d/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h
tos#
uint16_t sl_iperf_clnt_hdr_ext::tos
Tos.
Definition at line
370
of file /mnt/raid/workspaces/ws.Mae4JfP9d/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h
l_rate#
uint32_t sl_iperf_clnt_hdr_ext::l_rate
Lower rate.
Definition at line
372
of file /mnt/raid/workspaces/ws.Mae4JfP9d/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h
u_rate#
uint32_t sl_iperf_clnt_hdr_ext::u_rate
Upper rate.
Definition at line
374
of file /mnt/raid/workspaces/ws.Mae4JfP9d/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h
tcp_write_prefetch#
uint32_t sl_iperf_clnt_hdr_ext::tcp_write_prefetch
TCP write prefetch.
Definition at line
376
of file /mnt/raid/workspaces/ws.Mae4JfP9d/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h