Socket API#
Modules#
Protocol levels used for socket_setsockopt.#
Socket option level.
Application socket option level.
IPV6 socket option level.
application level socket options#
application level socket options summaryopt_name data type set/get sendmsg recvmsg SO_EVENT_MODE int16_t Set only No Yes SO_NONBLOCK int16_t Set only Yes Yes
Specify event mode of a socket. When set, optval must point to an uint32_t.
Possible values are:
SL_WISUN_SOCKET_EVENT_MODE_INDICATION: received data is included in SL_WISUN_MSG_SOCKET_DATA_IND_ID indication
SL_WISUN_SOCKET_EVENT_MODE_POLLING: only the amount of received data is included SL_WISUN_MSG_SOCKET_DATA_AVAILABLE_IND_ID indication. recv() or recvfrom() shouldbe invoked after indication reception to retrieve data
Specify event mode of a socket. When set, optval must point to an uint32_t.
Possible values are:
SL_WISUN_SOCKET_EVENT_MODE_INDICATION: received data is included in SL_WISUN_MSG_SOCKET_DATA_IND_ID indication
SL_WISUN_SOCKET_EVENT_MODE_POLLING: only the amount of received data is included SL_WISUN_MSG_SOCKET_DATA_AVAILABLE_IND_ID indication. recv() or recvfrom() shouldbe invoked after indication reception to retrieve data
Enable/disable nonblocking mode.
socket level options#
socket level options summaryopt_name data type set/get sendmsg recvmsg SO_RCVBUF int32_t Set/Get No Yes SO_SNDBUF int32_t Set/Get Yes No SO_SNDLOWAT int32_t Set/Get Yes No
Specify receive buffer size in payload bytes. When set, optval must point to an int32_t.
0 means unread data are dropped, unless read in data callback.
Specify send buffer size in payload bytes.
Specify send low water mark in payload bytes.
IPv6 socket options#
IPv6 socket options summaryopt_name Data type set/getsockopt sendmsg recvmsg IPV6_UNICAST_HOPS int16_t Set/Get Yes No IPV6_MULTICAST_HOPS int16_t Set/Get Yes No IPV6_JOIN_GROUP ns_ipv6_mreq_t Set only Yes Yes IPV6_LEAVE_GROUP ns_ipv6_mreq_t Set only Yes Yes SO_EDFE_MODE uint32_t Set only Yes No
Set the unicast hop limit for the socket. When set, optval must point to an int16_t.
-1 in the value means use the route default, otherwise it should be between 0 and 255.
Set the multicast hop limit for the socket.
Join a multicast group.
Leave a multicast group.
Experimental: Enable Extended Directed Frame Exchange mode.
Set the unicast hop limit for the socket. When set, optval must point to an int16_t.
-1 in the value means use the route default, otherwise it should be between 0 and 255.
Enumerations#
Enumerations for socket event mode.
Typedefs#
Socket address length type definition.
Socket id.
Supported address families.
Socket types.
IP protocols.
IPv6 Internet address.
IPv6 address format.
Variables#
IPv6 wildcard address.
Functions#
Creates an endpoint for communication and returns an Id that refers to that endpoint.
Close a socket.
Bind a name to a socket.
Send a message on a socket.
Send a message to a given address.
Receive messages from a socket.
Receive a message from a socket.
Accept a connection on a socket.
Initiate a connection on a socket.
Listen for connections on a socket.
Set socket option designated by optname at a given protocol level to the value pointed by optval.
Get socket option.
Convert the long host byte order to network order.
Convert the short host byte order to network order.
Convert the long network byte order to host byte order.
Convert the short network byte order to host byte order.
Convert the IPv4 and IPv6 addresses from text to binary form.
Convert IPv6 addresses from binary to text form.
Macros#
Size of an IPv6 address.
When bitwise ored with socket's type, it sets the O_NONBLOCK status flag on the opened socket file description.
Protocol levels used for socket_setsockopt. Documentation#
application level socket options Documentation#
socket level options Documentation#
IPv6 socket options Documentation#
Enumeration Documentation#
sl_wisun_socket_event_mode_t#
sl_wisun_socket_event_mode_t
Enumerations for socket event mode.
| Enumerator | |
|---|---|
| SL_WISUN_SOCKET_EVENT_MODE_INDICATION | SL_WISUN_MSG_SOCKET_DATA_IND_ID is sent to the app with the packet contained in the indication. |
| SL_WISUN_SOCKET_EVENT_MODE_POLLING | SL_WISUN_MSG_SOCKET_DATA_AVAILABLE_IND_ID is sent to the app indicating the amount of data received recv() or recvfrom() should be invoked after indication reception to retrieve data This is the default socket event mode option. |
socket_type#
socket_type
Socket types.
| Enumerator | |
|---|---|
| SOCK_STREAM | stream (connection) socket (TCP) |
| SOCK_DGRAM | datagram (connectionless ) socket (UDP) |
| SOCK_RAW | raw socket |
socket_protocol#
socket_protocol
IP protocols.
| Enumerator | |
|---|---|
| IPPROTO_IP | Dummy protocol. |
| IPPROTO_ICMP | Internet Control Message Protocol. |
| IPPROTO_TCP | Transmission Control Protocol. |
| IPPROTO_UDP | User Datagram Protocol. |
Typedef Documentation#
Function Documentation#
socket#
int32_t socket (int32_t domain, int32_t type, int32_t protocol)
Creates an endpoint for communication and returns an Id that refers to that endpoint.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| int32_t | [in] | domain | Specifies a communication domain. It selects the protocol family which will be used for communication. Must be set to AF_INET6 (IPv6 network socket) |
| int32_t | [in] | type | The communication semantics It can be:
|
| int32_t | [in] | protocol | Specifies the particular protocol to be used. It can be:
|
Returns
The socket's id on success, (-1) on failure.
close#
int32_t close (int32_t sockid)
Close a socket.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| int32_t | [in] | sockid | socket id |
Returns
0 on success, -1 on failure.
Close a socket and remove from the socket handler storage.
bind#
int32_t bind (int32_t sockid, const struct sockaddr * addr, socklen_t addrlen)
Bind a name to a socket.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| int32_t | [in] | sockid | socket id |
| const struct sockaddr * | [in] | addr | address structure ptr |
| socklen_t | [in] | addrlen | address structure size |
Returns
0 on success, -1 on failure.
Assigns the address to the socket, referred to by the socket ID, as specified by addr. It is normally necessary to assign a local address using bind() before a SOCK_STREAM socket may receive connections.
send#
int32_t send (int32_t sockid, const void * buff, uint32_t len, int32_t flags)
Send a message on a socket.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| int32_t | [in] | sockid | socket descriptor. |
| const void * | [in] | buff | pointer to data buffer to send. |
| uint32_t | [in] | len | length of data buffer to send. |
| int32_t | [in] | flags | flags to select send options. Ignored in our implementation. |
Returns
The number of bytes sent on success, -1 if an error occurred.
Preferred with connection-oriented sockets (TCP).
sendto#
int32_t sendto (int32_t sockid, const void * buff, uint32_t len, int32_t flags, const struct sockaddr * dest_addr, socklen_t addr_len)
Send a message to a given address.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| int32_t | [in] | sockid | socket descriptor. |
| const void * | [in] | buff | pointer to data buffer to send. |
| uint32_t | [in] | len | length of data buffer to send. |
| int32_t | [in] | flags | flags to select send options. Ignored in our implementation. |
| const struct sockaddr * | [in] | dest_addr | pointer to destination address buffer; Required for datagram sockets. |
| socklen_t | [in] | addr_len | length of destination address buffer. |
Returns
The number of bytes sent on success, -1 if an error occurred.
Preferred in datagram mode (UDP).
recvfrom#
int32_t recvfrom (int32_t sockid, void * buf, uint32_t len, int32_t flags, struct sockaddr * src_addr, socklen_t * addrlen)
Receive messages from a socket.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| int32_t | [in] | sockid | descriptor of socket to receive the message from. |
| void * | [out] | buf | pointer to destination data buffer. |
| uint32_t | [in] | len | length of destination data buffer. |
| int32_t | [in] | flags | flags to select type of message reception. Ignored in our implementation. |
| struct sockaddr * | [in] | src_addr | pointer to a sockaddr structure in which the sending address is to be stored. |
| socklen_t * | [in] | addrlen | length of the supplied sockaddr structure. |
Returns
The number of bytes received on success, -1 if an error occurred.
Receives data on a socket whether or not it is connection-oriented.
recv#
int32_t recv (int32_t sockid, void * buf, uint32_t len, int32_t flags)
Receive a message from a socket.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| int32_t | [in] | sockid | descriptor of socket to receive the message from. |
| void * | [out] | buf | pointer to destination data buffer. |
| uint32_t | [in] | len | length of destination data buffer. |
| int32_t | [in] | flags | flags to select type of message reception. Ignored in our implementation. |
Returns
The number of bytes received on success, -1 if an error occurred.
Should be used for connection-oriented protocol (TCP)
accept#
int32_t accept (int32_t sockid, struct sockaddr * addr, socklen_t * addrlen)
Accept a connection on a socket.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| int32_t | [in] | sockid | socket descriptor |
| struct sockaddr * | [inout] | addr | A pointer to sockaddr structure filled in with the address of the peer (remote) socket. When addr is NULL, nothing is filled in; in this case, addrlen is not used, and should also be NULL. |
| socklen_t * | [inout] | addrlen | The caller must initialize it to contain the size (in bytes) of the structure pointed to by addr. On return it will contain the actual size of the peer address. |
Returns
The socket id of the accepted socket on success, -1 if an error occurred.
Used with connection-based socket types (TCP). It extracts the first connection request on the queue of pending connections for the listening socket.
connect#
int32_t connect (int32_t sockid, const struct sockaddr * addr, socklen_t addrlen)
Initiate a connection on a socket.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| int32_t | [in] | sockid | socket descriptor. |
| const struct sockaddr * | [in] | addr | If the socket sockid is of type SOCK_DGRAM, addr is the address to which datagrams are sent by default and the only address from which datagrams are received. If the socket is of type SOCK_STREAM, this call attempts to make a connection to the socket that is bound to the address specified by addr. |
| socklen_t | [in] | addrlen | length of the supplied sockaddr structure. |
Returns
0 on connection or binding success, -1 if an error occurred.
Connects the socket referred to by the sockid to the address specified by address.
listen#
int32_t listen (int32_t sockid, int32_t backlog)
Listen for connections on a socket.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| int32_t | [in] | sockid | socket id |
| int32_t | [in] | backlog | Argument defines the maximum length to which the queue of pending connections for sockid may grow. Not implemented for Wi-SUN, the connection queue size is always 1 |
Returns
0 on success, -1 if an error occurred.
Marks the socket referred to by sockid as a passive socket, that is, as a socket that will be used to accept incoming connection requests using accept.
setsockopt#
int32_t setsockopt (int32_t sockid, int32_t level, int32_t optname, const void * optval, socklen_t optlen)
Set socket option designated by optname at a given protocol level to the value pointed by optval.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| int32_t | [in] | sockid | socket ID |
| int32_t | [in] | level | protocol level at which the option resides. it could be: |
| int32_t | [in] | optname | option name. it could be: |
| const void * | [in] | optval | Pointer to the socket option new value. The type of variable pointed by optval depends level and optname values. |
| socklen_t | [in] | optlen | Must be the size of the symbol pointed by optval. |
Returns
0 on success, -1 if an error occurred.
This function can set socket properties.
getsockopt#
int32_t getsockopt (int32_t sockid, int32_t level, int32_t optname, void * optval, socklen_t * optlen)
Get socket option.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| int32_t | [in] | sockid | socket descriptor. |
| int32_t | [in] | level | socket protocol level. |
| int32_t | [in] | optname | Option name. Supported options:
|
| void * | [out] | optval | option value structure pointer. |
| socklen_t * | [in] | optlen | size of the option value structure. |
Returns
0 on success, -1 if an error occurred.
The function gets socket option by optname, and copies option data to optval ptr.
htonl#
__STATIC_INLINE uint32_t htonl (uint32_t hostlong)
Convert the long host byte order to network order.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | hostlong | Long host integer |
Returns
Long network integer
This function converts the unsigned integer hostlong from host byte order to network byte order. For Wi-SUN, the conversion is not needed. Dummy implementation
htons#
__STATIC_INLINE uint16_t htons (uint16_t hostshort)
Convert the short host byte order to network order.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | hostshort | Short host integer |
Returns
Short network integer
This function converts the unsigned short integer hostshort from host byte order to network byte order. For Wi-SUN, the conversion is not needed. Dummy implementation
ntohl#
__STATIC_INLINE uint32_t ntohl (uint32_t netlong)
Convert the long network byte order to host byte order.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | netlong | Long network integer |
Returns
Long host integer
This function converts the unsigned integer netlong from network byte order to host byte order. For Wi-SUN, the conversion is not needed. Dummy implementation
ntohs#
__STATIC_INLINE uint16_t ntohs (uint16_t netshort)
Convert the short network byte order to host byte order.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | netshort |
Returns
Short host integer
This function converts the unsigned short integer netshort from the network byte order to host byte order.For Wi-SUN, the conversion is not needed. Dummy implementation.
inet_pton#
int32_t inet_pton (int32_t af, const char * src, void * dst)
Convert the IPv4 and IPv6 addresses from text to binary form.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| int32_t | [in] | af | The address family. Only AF_INET6 is supported by our implementation. |
| const char * | [in] | src | Source string |
| void * | [out] | dst | Destination address pointer |
Returns
1 on succes, -1 if an error occurred. (POSIX described the 0 value too)
This function converts the character string src into a network address structure in the af address family, then copies the network address structure to dst. AF_INET (IPv4) case not supported.
inet_ntop#
const char * inet_ntop (int32_t af, const void * src, char * dst, socklen_t size)
Convert IPv6 addresses from binary to text form.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| int32_t | [in] | af | - Address family.
|
| const void * | [in] | src | Source address in byte form |
| char * | [out] | dst | Destination buffer ptr |
| socklen_t | [in] | size | Size of the destination buffer. |
Returns
It returns a non-null pointer to dst. NULL if an error occurred.
Converts the network address structure src in the af address family into a character string. The resulting string is copied to the buffer pointed to by dst, which must be a non-null pointer. The caller specifies the number of bytes available in this buffer in the argument size. AF_INET (IPv4) case not supported.