iPerf Client header extended FQ start time

Public Attributes#

uint32_t

Reserved.

uint32_t

Start sec.

uint32_t

Start usec.

uint32_t

Lower FQ rate.

uint32_t

Upper FQ rate.

Public Attribute Documentation#

reserved#

uint32_t sl_iperf_clnt_hdr_ext_starttime_fq::reserved

Reserved.


Definition at line 405 of file /mnt/raid/workspaces/ws.x49WyIS5n/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h

start_tv_sec#

uint32_t sl_iperf_clnt_hdr_ext_starttime_fq::start_tv_sec

Start sec.


Definition at line 407 of file /mnt/raid/workspaces/ws.x49WyIS5n/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h

start_tv_usec#

uint32_t sl_iperf_clnt_hdr_ext_starttime_fq::start_tv_usec

Start usec.


Definition at line 409 of file /mnt/raid/workspaces/ws.x49WyIS5n/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h

l_fq_rate#

uint32_t sl_iperf_clnt_hdr_ext_starttime_fq::l_fq_rate

Lower FQ rate.


Definition at line 411 of file /mnt/raid/workspaces/ws.x49WyIS5n/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h

u_fq_rate#

uint32_t sl_iperf_clnt_hdr_ext_starttime_fq::u_fq_rate

Upper FQ rate.


Definition at line 413 of file /mnt/raid/workspaces/ws.x49WyIS5n/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h