Ping info structure type definition.
Public Attributes#
uint16_t
Identifier.
uint16_t
Sequence number.
uint16_t
ICMPv6 packet length including header.
uint32_t
Response time millisecond.
Wi-SUN remote address.
uint32_t
Start time stamp.
uint32_t
Stop time stamp.
bool
Lost packet flag.
Public Attribute Documentation#
identifier#
uint16_t sl_wisun_ping_info::identifier
Identifier.
Definition at line
109
of file /mnt/raid/workspaces/ws.x49WyIS5n/overlay/gsdk/app/wisun/component/ping/sl_wisun_ping.h
sequence_number#
uint16_t sl_wisun_ping_info::sequence_number
Sequence number.
Definition at line
111
of file /mnt/raid/workspaces/ws.x49WyIS5n/overlay/gsdk/app/wisun/component/ping/sl_wisun_ping.h
packet_length#
uint16_t sl_wisun_ping_info::packet_length
ICMPv6 packet length including header.
Definition at line
113
of file /mnt/raid/workspaces/ws.x49WyIS5n/overlay/gsdk/app/wisun/component/ping/sl_wisun_ping.h
response_time_ms#
uint32_t sl_wisun_ping_info::response_time_ms
Response time millisecond.
Definition at line
115
of file /mnt/raid/workspaces/ws.x49WyIS5n/overlay/gsdk/app/wisun/component/ping/sl_wisun_ping.h
remote_addr#
sockaddr_in6_t sl_wisun_ping_info::remote_addr
Wi-SUN remote address.
Definition at line
117
of file /mnt/raid/workspaces/ws.x49WyIS5n/overlay/gsdk/app/wisun/component/ping/sl_wisun_ping.h
start_time_stamp#
uint32_t sl_wisun_ping_info::start_time_stamp
Start time stamp.
Definition at line
119
of file /mnt/raid/workspaces/ws.x49WyIS5n/overlay/gsdk/app/wisun/component/ping/sl_wisun_ping.h
stop_time_stamp#
uint32_t sl_wisun_ping_info::stop_time_stamp
Stop time stamp.
Definition at line
121
of file /mnt/raid/workspaces/ws.x49WyIS5n/overlay/gsdk/app/wisun/component/ping/sl_wisun_ping.h
lost#
bool sl_wisun_ping_info::lost
Lost packet flag.
Definition at line
123
of file /mnt/raid/workspaces/ws.x49WyIS5n/overlay/gsdk/app/wisun/component/ping/sl_wisun_ping.h