Wi-SUN event definitions.
This structure contains a Wi-SUN API event and its associated data.
Public Attribute Documentation#
connected#
sl_wisun_msg_connected_ind_body_t sl_wisun_evt_t::connected
SL_WISUN_MSG_CONNECTED_IND_ID event data
connection_lost#
sl_wisun_msg_connection_lost_ind_body_t sl_wisun_evt_t::connection_lost
SL_WISUN_MSG_CONNECTION_LOST_IND_ID event data
dhcp_vendor_data#
sl_wisun_msg_dhcp_vendor_data_ind_body_t sl_wisun_evt_t::dhcp_vendor_data
SL_WISUN_MSG_DHCP_VENDOR_DATA_IND_ID event data
disconnected#
sl_wisun_msg_disconnected_ind_body_t sl_wisun_evt_t::disconnected
SL_WISUN_MSG_DISCONNECTED_IND_ID event data
evt#
union sl_wisun_evt_t::@0 sl_wisun_evt_t::evt
Event-specific data.
This structure contains the event-specific data.
header#
sl_wisun_msg_header_t sl_wisun_evt_t::header
Common event header.
This structure contains common information for all events. ID of the event is stored in the sl_wisun_msg_header_t.id field and is one of the values of sl_wisun_msg_ind_id_t. The other fields can be ignored.
join_state#
sl_wisun_msg_join_state_ind_body_t sl_wisun_evt_t::join_state
SL_WISUN_MSG_JOIN_STATE_IND_ID event data
lfn_multicast_reg#
sl_wisun_msg_lfn_multicast_reg_ind_body_t sl_wisun_evt_t::lfn_multicast_reg
SL_WISUN_MSG_LFN_MULTICAST_REG_IND_ID event data
lfn_wake_up#
sl_wisun_msg_lfn_wake_up_ind_body_t sl_wisun_evt_t::lfn_wake_up
SL_WISUN_MSG_LFN_WAKE_UP_IND_ID event data
mode_switch_fallback#
sl_wisun_msg_mode_switch_fallback_ind_body_t sl_wisun_evt_t::mode_switch_fallback
SL_WISUN_MSG_MODE_SWITCH_FALLBACK_IND_ID event data
network_update#
sl_wisun_msg_network_update_ind_body_t sl_wisun_evt_t::network_update
SL_WISUN_MSG_NETWORK_UPDATE_IND_ID event data
regulation_tx_level#
sl_wisun_msg_regulation_tx_level_ind_body_t sl_wisun_evt_t::regulation_tx_level
SL_WISUN_MSG_REGULATION_TX_LEVEL_IND_ID event data
rx_frame#
sl_wisun_msg_rx_frame_ind_body_t sl_wisun_evt_t::rx_frame
SL_WISUN_MSG_RX_FRAME_IND_ID event data
socket_closing#
sl_wisun_msg_socket_closing_ind_body_t sl_wisun_evt_t::socket_closing
SL_WISUN_MSG_SOCKET_CLOSING_IND_ID event data
socket_connected#
sl_wisun_msg_socket_connected_ind_body_t sl_wisun_evt_t::socket_connected
SL_WISUN_MSG_SOCKET_CONNECTED_IND_ID event data
socket_connection_available#
sl_wisun_msg_socket_connection_available_ind_body_t sl_wisun_evt_t::socket_connection_available
SL_WISUN_MSG_SOCKET_CONNECTION_AVAILABLE_IND_ID event data
socket_data#
sl_wisun_msg_socket_data_ind_body_t sl_wisun_evt_t::socket_data
SL_WISUN_MSG_SOCKET_DATA_IND_ID event data
socket_data_available#
sl_wisun_msg_socket_data_available_ind_body_t sl_wisun_evt_t::socket_data_available
SL_WISUN_MSG_SOCKET_DATA_AVAILABLE_IND_ID event data
socket_data_sent#
sl_wisun_msg_socket_data_sent_ind_body_t sl_wisun_evt_t::socket_data_sent
SL_WISUN_MSG_SOCKET_DATA_SENT_IND_ID event data