Wi-SUN OTA DFU download error context definition.

Public Attributes#

uint16_t

Data size.

uint32_t

Offset of GBL file.

int32_t

Return value of API call.

Public Attribute Documentation#

data_size#

uint16_t sl_wisun_ota_dfu_error_ctx_fw_download::data_size

Data size.


Definition at line 113 of file /mnt/raid/workspaces/ws.z1SfSYxIV/overlay/gsdk/app/wisun/component/ota_dfu/sl_wisun_ota_dfu.h

offset#

uint32_t sl_wisun_ota_dfu_error_ctx_fw_download::offset

Offset of GBL file.


Definition at line 111 of file /mnt/raid/workspaces/ws.z1SfSYxIV/overlay/gsdk/app/wisun/component/ota_dfu/sl_wisun_ota_dfu.h

ret_val#

int32_t sl_wisun_ota_dfu_error_ctx_fw_download::ret_val

Return value of API call.


Definition at line 109 of file /mnt/raid/workspaces/ws.z1SfSYxIV/overlay/gsdk/app/wisun/component/ota_dfu/sl_wisun_ota_dfu.h