Ping echo request packed structure type definitions.
Public Attributes#
uint16_t
Checksum.
uint8_t
Code.
uint16_t
Identifier.
uint8_t
Payload array.
uint16_t
Sequence number.
uint8_t
type
Public Attribute Documentation#
checksum#
uint16_t sl_wisun_ping_echo_request::checksum
Checksum.
Definition at line
93
of file /mnt/raid/workspaces/ws.z1SfSYxIV/overlay/gsdk/app/wisun/component/ping/sl_wisun_ping.h
code#
uint8_t sl_wisun_ping_echo_request::code
Code.
Definition at line
91
of file /mnt/raid/workspaces/ws.z1SfSYxIV/overlay/gsdk/app/wisun/component/ping/sl_wisun_ping.h
identifier#
uint16_t sl_wisun_ping_echo_request::identifier
Identifier.
Definition at line
95
of file /mnt/raid/workspaces/ws.z1SfSYxIV/overlay/gsdk/app/wisun/component/ping/sl_wisun_ping.h
payload#
uint8_t sl_wisun_ping_echo_request::payload[SL_WISUN_PING_MAX_PAYLOAD_LENGTH]
Payload array.
Definition at line
99
of file /mnt/raid/workspaces/ws.z1SfSYxIV/overlay/gsdk/app/wisun/component/ping/sl_wisun_ping.h
sequence_number#
uint16_t sl_wisun_ping_echo_request::sequence_number
Sequence number.
Definition at line
97
of file /mnt/raid/workspaces/ws.z1SfSYxIV/overlay/gsdk/app/wisun/component/ping/sl_wisun_ping.h
type#
uint8_t sl_wisun_ping_echo_request::type
type
Definition at line
89
of file /mnt/raid/workspaces/ws.z1SfSYxIV/overlay/gsdk/app/wisun/component/ping/sl_wisun_ping.h