Wi-SUN Overview#

 

Wi-SUN Stack#

The Wi-SUN stack API is the primary Application Programming Interface (API) for applications running on Silicon Labs EFR32 Wireless Gecko SoCs to interact with the Silicon Labs Wi-SUN FAN wireless stack. It allows the application to manage the connection to a Wi-SUN FAN network as well as to communicate with other devices in the network using a socket-based communication interface.

See the Wi-SUN Stack API for more details.

Stack Plugins#

Wi-SUN stack plugin components are software modules tightly linked to the stack that provide means to customize it: debug, manufacturing or Wi-SUN specific optional features. They can have significant impact on key capabilities and footprint.

Service Components#

The following software components are provided to help and accelerate Wi-SUN application developments by offering common functionalities. They can easily be added to an existing Wi-SUN application through Simplicity Studio graphical interface. The components are shared in source code in the Gecko SDK.

Versioning#

Silicon Labs Wi-SUN solution follows the Semantic Versioning guidelines for release cycle transparency and to maintain backward compatibility.