Deprecated List#
Global sl_wisun_app_status_get_remote_address (void) SL_DEPRECATED_API_SDK_2025_6
This function is not thread-safe, use sl_wisun_app_status_get_remote_addr instead.
Global sl_wisun_br_set_network_size (sl_wisun_network_size_t size) SL_DEPRECATED_API_SDK_2026_6
This function will be removed in the future versions of the Wi-SUN stack, use sl_wisun_br_set_connection_parameters() instead.
Global sl_wisun_coap_free (void *addr) SL_DEPRECATED_API_SDK_2025_6
Global sl_wisun_coap_malloc (uint16_t size) SL_DEPRECATED_API_SDK_2025_6
Global sl_wisun_set_channel_mask (const sl_wisun_channel_mask_t *channel_mask)
This function is an alias for sl_wisun_set_allowed_channel_mask(). It is maintained for backward compatibility.
Global sl_wisun_set_neighbor_table_size (uint8_t size) SL_DEPRECATED_API_SDK_2025_6
This function will be removed in the future versions of the Wi-SUN stack, use sl_wisun_config_neighbor_table() instead.
Global sl_wisun_set_regulation (sl_wisun_regulation_t regulation) SL_DEPRECATED_API_SDK_2025_12
This function will be removed in the future versions of the Wi-SUN stack, use sl_wisun_set_regulation_parameters() instead.
Global sl_wisun_set_tx_power (int8_t tx_power) SL_DEPRECATED_API_SDK_2024_6
This function will be removed in the future versions of the Wi-SUN stack, use sl_wisun_set_tx_power_ddbm() instead.
Global sl_wisun_util_connect (const uint8_t *network_name) SL_DEPRECATED_API_SDK_2024_6
This function will be removed in the future versions of the Wi-SUN stack.
Global sl_wisun_util_get_phy_config (sl_wisun_phy_config_t *phy_config) SL_DEPRECATED_API_SDK_2024_6
This function will be removed in the future versions of the Wi-SUN stack.