Border Router API#
Wi-SUN Border Router API contains functions for Border Router specific functionality.
The API is an extension, not a replacement of Wi-SUN Stack API. An application implementing Border Router capability may utilize functions from both APIs. See API availability for further information.
Functions#
Get Group AES Key.
Get the unicast IPv6 addresses configured in the Border Router.
Get the Routing Table.
Get the Routing Table Size.
Get the Routing Table starting from a specific index.
Get the Border Router state.
Forward an IPv6 packet to Wi-SUN network.
Check if the IPv6 destination address is routable in the Wi-SUN network.
Start or stop PAN Defect advertisement.
Revoke (LFN) Group Transient Keys and installs a new key.
Remove pairwise keys associated with a node.
Set advanced Border Router connection parameters.
Set broadcast settings.
Configure the Border Router parameter set.
Set the Border Router device certificate.
Set Group Transient Key.
Set IPv6 prefix for the Wi-SUN network.
Register a function to handle IPv6 packets received from Wi-SUN network.
Configure LFN parenting parameter set.
Configure LFN parenting support.
Set the size of the Wi-SUN network.
Start the Border Router.
Stop the Border Router.
Trigger a global repair process from the Border Router.
Macros#
Define sl_wisun_set_br_device_certificate for legacy.
Function Documentation#
sl_wisun_br_get_gak#
sl_status_t sl_wisun_br_get_gak (uint8_t index, uint8_t * gak)
Get Group AES Key.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | index | Index of the key from 0 to 3 for GAKs and 4 to 6 for LFN GAKs |
| uint8_t * | [out] | gak | Pointer to Group AES Key |
Returns
SL_STATUS_OK if successful, an error code otherwise
This function exports (L)GAK as a plaintext key.
Note
This functionality is only available when using the debug library.
sl_wisun_br_get_ip_addresses#
sl_status_t sl_wisun_br_get_ip_addresses (uint8_t * addr_ll, uint8_t * addr_gua, uint8_t * addr_dodagid)
Get the unicast IPv6 addresses configured in the Border Router.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t * | [out] | addr_ll | Pointer to Link-Local address |
| uint8_t * | [out] | addr_gua | Pointer to Unique Local Address or Global Unicast Address |
| uint8_t * | [out] | addr_dodagid | Pointer to DODAG ID |
Returns
SL_STATUS_OK if successful, an error code otherwise
sl_wisun_br_get_routing_table#
sl_status_t sl_wisun_br_get_routing_table (uint16_t * entry_count, sl_wisun_br_routing_table_entry_t * table)
Get the Routing Table.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t * | [inout] | entry_count | Maximum number of entries to read on input, number of entries read on output |
| sl_wisun_br_routing_table_entry_t * | [out] | table | Pointer to the application allocated memory where the routing table is written |
Returns
SL_STATUS_OK if successful, an error code otherwise
The routing table is unordered and only contains the parent-child relationship between the nodes. The table is in the format: | Node GUA/ULA 16 bytes | parent GUA/ULA 16 bytes |
Note
This function should be called after sl_wisun_br_get_routing_table_entry_count() to get the number of entries in the routing table.
sl_wisun_br_get_routing_table_entry_count#
sl_status_t sl_wisun_br_get_routing_table_entry_count (uint16_t * entry_count)
Get the Routing Table Size.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t * | [out] | entry_count | Number of entries in the routing table |
Returns
SL_STATUS_OK if successful, an error code otherwise
This function retrieves the number of entries in the routing table. This allows for allocation before calling sl_wisun_br_get_routing_table(). The allocated memory should be at least equal to: sizeof(sl_wisun_br_routing_table_entry_t) * entry_count.
sl_wisun_br_get_routing_table_from_index#
sl_status_t sl_wisun_br_get_routing_table_from_index (uint16_t start_index, uint16_t * entry_count, sl_wisun_br_routing_table_entry_t * entries)
Get the Routing Table starting from a specific index.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | start_index | Index to start reading the routing table from |
| uint16_t * | [inout] | entry_count | Maximum number of entries to read on input, number of entries read on output |
| sl_wisun_br_routing_table_entry_t * | [out] | entries | Pointer to the application allocated memory where the routing table is written |
Returns
SL_STATUS_OK if successful, an error code otherwise
This function retrieves entry_count entries from the routing table, starting from a specific index. This allows the caller to get any number of entries from the routing table without having to allocate a large buffer. The allocated memory should be at least equal to: sizeof(sl_wisun_br_routing_table_entry_t) * entry_count.
Note
This function should be called after sl_wisun_br_get_routing_table_entry_count() to get the number of entries in the routing table.
Warnings
If the application does not retrieve the entire routing table in a single read, it may miss updates or changes in the network topology.
sl_wisun_br_get_state#
sl_status_t sl_wisun_br_get_state (sl_wisun_br_state_t * state)
Get the Border Router state.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_wisun_br_state_t * | [out] | state | Pointer to state
|
Returns
SL_STATUS_OK if successful, an error code otherwise
sl_wisun_br_ipv6_down#
sl_status_t sl_wisun_br_ipv6_down (const uint8_t * data, size_t data_length)
Forward an IPv6 packet to Wi-SUN network.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const uint8_t * | [in] | data | Pointer to IPv6 header |
| size_t | [out] | data_length | Length of IPv6 packet data in bytes |
Returns
SL_STATUS_OK if successful, an error code otherwise
This function forwards an IPv6 packet to Wi-SUN network. The destination address must belong to the DODAG prefix. This function is used for handling downlink packets from the backhaul interface, see sl_wisun_br_set_ipv6_up_handler() for uplink. It's recommended to use sl_wisun_br_ipv6_route_exists() before forwarding a packet.
sl_wisun_br_ipv6_route_exists#
sl_status_t sl_wisun_br_ipv6_route_exists (const uint8_t * ipv6_address, bool * exists)
Check if the IPv6 destination address is routable in the Wi-SUN network.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const uint8_t * | [in] | ipv6_address | Pointer to IPv6 destination address |
| bool * | [out] | exists | Whether the address is routable
|
Returns
SL_STATUS_OK if successful, an error code otherwise
This function checks if the given IPv6 address is a valid destination in the Wi-SUN network. The destination address must belong to the Border Router or one of the connected nodes.
sl_wisun_br_pan_defect_advertise#
sl_status_t sl_wisun_br_pan_defect_advertise (bool defect_advertise, uint32_t min_scan_duration_s, uint32_t max_scan_duration_s)
Start or stop PAN Defect advertisement.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| bool | [in] | defect_advertise | True to start PAN Defect procedure, false to stop it. |
| uint32_t | [in] | min_scan_duration_s | Minimum duration after which devices are allowed to switch their PAN if an alternative one is available. |
| uint32_t | [in] | max_scan_duration_s | Duration after which devices should systemically switch to the alternative PAN if one is available. |
Returns
SL_STATUS_OK if successful, an error code otherwise.
Note
The values for
min_scan_duration_sandmax_scan_duration_sshould be chosen based on the estimated performance of the backup power source. Specifically,max_scan_duration_sshould be set to a value smaller than the estimated lifetime of the backup power source to ensure a seamless transition to the alternative PAN without long connection interruptions.
sl_wisun_br_revoke_gtks#
sl_status_t sl_wisun_br_revoke_gtks (bool revoke_lgtks, const uint8_t * gtk)
Revoke (LFN) Group Transient Keys and installs a new key.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| bool | [in] | revoke_lgtks | True to revoke LGTKs, false to revoke GTKs |
| const uint8_t * | [in] | gtk | (LFN) Group Transient Key |
Returns
SL_STATUS_OK if successful, an error code otherwise
Destroy all (L)GTKs except the current active one (and potentially the next key), reduce the current (or next) key's lifetime, and add a new key, as described in the Wi-SUN FAN specification section 6.5.2.5.
Note
The gtk parameter is provided for test and debug purposes: setting a specific key in production is not recommended. Set to NULL to generate a random key.
sl_wisun_br_revoke_pairwise_keys#
sl_status_t sl_wisun_br_revoke_pairwise_keys (const sl_wisun_mac_address_t * address)
Remove pairwise keys associated with a node.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const sl_wisun_mac_address_t * | [in] | address | EUI-64 of the target node |
Returns
SL_STATUS_OK if successful, an error code otherwise
Remove the Pairwise Transient Key (PTK) and Pairwise Master Key (PMK) associated with a node as described in the Wi-SUN FAN specification section 6.5.2.5.
Note
To permanently revoke access to the node, its certificate must be banned at the authentication authority (e.g. RADIUS server).
sl_wisun_br_set_advanced_parameters#
sl_status_t sl_wisun_br_set_advanced_parameters (const sl_wisun_br_advanced_parameters_t * params)
Set advanced Border Router connection parameters.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const sl_wisun_br_advanced_parameters_t * | [in] | params | Pointer to the advanced parameter structure |
Returns
SL_STATUS_OK on success.
SL_STATUS_INVALID_STATE if the border router is started, or if sl_wisun_br_set_connection_parameters has been called previously.
SL_STATUS_INVALID_PARAMETER if one or more parameters are invalid.
By default, the stack automatically adapts its behavior based on the PAN Size advertised in the Wi-SUN PAN-IE.
This function overrides that automatic adjustment with explicit values.
This function and sl_wisun_br_set_connection_parameters are mutually exclusive. If sl_wisun_br_set_connection_parameters has been called, any subsequent call to this function will fail with SL_STATUS_INVALID_STATE.
This restriction remains in effect even if the border router is later stopped. To switch back to auto mode and allow this function again, call sl_wisun_reset_parameters.
A later call to sl_wisun_br_set_connection_parameters also overrides any overlapping settings previously applied with this function.
This function can be used together with sl_wisun_set_option.
This function must be called before starting the border router.
sl_wisun_br_set_broadcast_settings#
sl_status_t sl_wisun_br_set_broadcast_settings (uint32_t interval_ms, uint8_t dwell_interval_ms)
Set broadcast settings.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | interval_ms | Broadcast Interval (BDI < BI <= 16777215 ms) (default: 1020 ms) |
| uint8_t | [in] | dwell_interval_ms | Broadcast Dwell Interval (100-255 ms) (default: 255 ms) |
Returns
SL_STATUS_OK if successful, an error code otherwise
This function sets the broadcast channel hopping schedule. The Broadcast Interval is the duration, between Broadcast Dwell Intervals within the advertising node’s broadcast schedule. Its resolution is limited to 24 bits (16777215 ms). The Broadcast Dwell Interval specifies the duration during which the node may transmit a broadcast message. It is recommended a BI value of 4.0 times the maximum of (UDI, BDI). These values affect the whole PAN, since they are propagated from parent to children. This function must be called before starting the Border Router.
sl_wisun_br_set_connection_parameters#
sl_status_t sl_wisun_br_set_connection_parameters (const sl_wisun_br_connection_params_t * params)
Configure the Border Router parameter set.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const sl_wisun_br_connection_params_t * | [in] | params | Parameter set to use |
Returns
SL_STATUS_OK if successful, an error code otherwise
This functions sets the Border Router parameter set. These parameters impact connection time, bandwidth usage, and latency. Use of a predefined parameter set is recommended (Predefined BR parameter sets). Small profile will be used by default for all missing configurations. This function must be called before starting the Border Router.
sl_wisun_br_set_device_certificate#
sl_status_t sl_wisun_br_set_device_certificate (uint16_t certificate_options, uint16_t certificate_length, const uint8_t * certificate)
Set the Border Router device certificate.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | certificate_options | Options for the certificate. |
| uint16_t | [in] | certificate_length | Size of the certificate data |
| const uint8_t * | [in] | certificate | Pointer to the certificate data |
Returns
SL_STATUS_OK if successful, an error code otherwise
sl_wisun_br_set_gtk#
sl_status_t sl_wisun_br_set_gtk (const uint8_t * gtk, uint8_t index)
Set Group Transient Key.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const uint8_t * | [in] | gtk | Group Transient Key |
| uint8_t | [in] | index | Index of the key from 0 to 3 for GTKs and 4 to 6 for LGTKs |
Note
This API is provided for test and debug purposes: setting a specific key in production is not recommended. The keys set using this API are saved to NVM, and subsequent calls to this API are ignored until the NVM is cleared using sl_wisun_clear_credential_cache.
Returns
SL_STATUS_OK if successful, SL_STATUS_ALREADY_EXISTS when ignored, an error code otherwise
sl_wisun_br_set_ipv6_prefix#
sl_status_t sl_wisun_br_set_ipv6_prefix (const uint8_t * ipv6_prefix, uint8_t prefix_length)
Set IPv6 prefix for the Wi-SUN network.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const uint8_t * | [in] | ipv6_prefix | IPv6 prefix |
| uint8_t | [in] | prefix_length | Prefix length. Currently, only 64 bit prefixes are supported. |
Note
Must not be called after the border router is started
Returns
SL_STATUS_OK if successful, an error code otherwise
This function sets the prefix used to generate IP addresses for RPL traffic (DODAGID will derive from it). This function must be called before starting the Border Router.
sl_wisun_br_set_ipv6_up_handler#
sl_status_t sl_wisun_br_set_ipv6_up_handler (sl_wisun_ipv6_up_handler_t handler)
Register a function to handle IPv6 packets received from Wi-SUN network.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_wisun_ipv6_up_handler_t | [in] | handler | Pointer to handler function |
Returns
SL_STATUS_OK if successful, an error code otherwise
This function registers a handler function that will be called when the destination address of a received IPv6 packet is outside the DODAG prefix. Setting the handler function to NULL disables the forwarding. This function is used for handling uplink packets towards the backhaul interface, see sl_wisun_br_ipv6_down() for downlink.
sl_wisun_br_set_lfn_parameters#
sl_status_t sl_wisun_br_set_lfn_parameters (const sl_wisun_br_lfn_params_t * params)
Configure LFN parenting parameter set.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const sl_wisun_br_lfn_params_t * | [in] | params | Parameter set to use |
Returns
SL_STATUS_OK if successful, an error code otherwise
This function sets the LFN parenting parameter set. These parameters impact battery life of all LFNs in the PAN. Use of a predefined parameter set is recommended (Predefined BR LFN-parenting parameter sets). This function must be called before starting the Border Router.
sl_wisun_br_set_lfn_support#
sl_status_t sl_wisun_br_set_lfn_support (uint8_t lfn_limit, bool lfn_support_pan)
Configure LFN parenting support.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | lfn_limit | Maximum number of LFN children
|
| bool | [in] | lfn_support_pan | LFN parenting support in the PAN
|
Returns
SL_STATUS_OK if successful, an error code otherwise
This function configures LFN parenting support in the Border Router and in the PAN. Set sl_wisun_config_neighbor_table accordingly.
sl_wisun_br_set_network_size#
sl_status_t sl_wisun_br_set_network_size (sl_wisun_network_size_t size)
Set the size of the Wi-SUN network.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_wisun_network_size_t | [in] | size | Size of the network |
Returns
SL_STATUS_OK if successful, an error code otherwise
This function sets the size of the network. The size is used to set various stack parameters, such as timing parameters to optimize device behavior in regards to node count. The device will function with any setting but may exhibit non-optimal behavior. Setting the size too large may cause slow connection speed and increased latency. Conversely, a value too small may cause increased network traffic.
DeprecatedThis function will be removed in the future versions of the Wi-SUN stack, use sl_wisun_br_set_connection_parameters() instead.
sl_wisun_br_start#
sl_status_t sl_wisun_br_start (const uint8_t * name, const sl_wisun_phy_config_t * phy_config)
Start the Border Router.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const uint8_t * | [in] | name | Name of the Wi-SUN network as a zero-terminated string |
| const sl_wisun_phy_config_t * | [in] | phy_config | Pointer to PHY configuration |
Returns
SL_STATUS_OK if successful, an error code otherwise
sl_wisun_br_stop#
sl_status_t sl_wisun_br_stop (void )
Stop the Border Router.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
SL_STATUS_OK if successful, an error code otherwise
sl_wisun_br_trigger_global_repair#
sl_status_t sl_wisun_br_trigger_global_repair (void )
Trigger a global repair process from the Border Router.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
SL_STATUS_OK if successful SL_STATUS_NOT_READY if the Border Router is not started SL_STATUS_FAIL if the DODAG Version is not incremented
Increments the RPL DODAG Version to allow nodes in the network to choose a new position whose rank is not constrained by their rank within the old DODAG Version. The new DODAG Version is propagated through DIOs in the entire network and will cause all nodes to re-run a parent selection within the new DODAG Version, effectively temporarily disconnecting them from the network.
Note
This operation will disrupt network communications as the repair process is carried out. It is not recommended to trigger a global repair more often than once every 24 hours.