BR advanced connection parameters for sl_wisun_br_set_advanced_parameters.
Public Attributes#
PAN advertisement trickle timer parameters.
PAN configuration trickle timer parameters.
uint32_t
Version of sl_wisun_br_advanced_parameters_t.
Public Attribute Documentation#
trickle_pa#
sl_wisun_trickle_params_t sl_wisun_br_advanced_parameters_t::trickle_pa
PAN advertisement trickle timer parameters.
trickle_pc#
sl_wisun_trickle_params_t sl_wisun_br_advanced_parameters_t::trickle_pc
PAN configuration trickle timer parameters.
version#
uint32_t sl_wisun_br_advanced_parameters_t::version
Version of sl_wisun_br_advanced_parameters_t.
Set to SL_WISUN_BR_ADVANCED_PARAMS_API_VERSION.
Used to identify the layout of the structure when applying advanced BR connection parameters. Older supported versions may be accepted and updated internally to the current format, while unsupported versions are rejected.