Advanced RPL parameters for sl_wisun_set_ffn_advanced_parameters.
Public Attributes#
RFC8415 TX algorithm parameters for DAO transmission rand specification range [0.0, 1.0] irt_s specification range [1, 60] mrt_s specification range [0, 600] mrd_s specification range [0, 3600] mrc specification range [0, 15].
Maximum delay before sending an ETX probe (seconds).
Maximum delay before sending the first RPL DIS (unicast/multicast) packet following transition to Join State 4 - Preferred Parent Selection (seconds)
Public Attribute Documentation#
dao_txalg#
sl_wisun_rfc8415_txalg_params_t sl_wisun_ffn_advanced_rpl_params_t::dao_txalg
RFC8415 TX algorithm parameters for DAO transmission rand specification range [0.0, 1.0] irt_s specification range [1, 60] mrt_s specification range [0, 600] mrd_s specification range [0, 3600] mrc specification range [0, 15].
etx_probe_max_delay_s#
uint16_t sl_wisun_ffn_advanced_rpl_params_t::etx_probe_max_delay_s
Maximum delay before sending an ETX probe (seconds).
first_dis_max_delay_s#
uint16_t sl_wisun_ffn_advanced_rpl_params_t::first_dis_max_delay_s
Maximum delay before sending the first RPL DIS (unicast/multicast) packet following transition to Join State 4 - Preferred Parent Selection (seconds)