LFN connection parameters.

Public Attributes#

uint8_t

Duration of LFN PAN Advertisement (LPA) listening slot (millisecond) Specification range [15, 255].

uint8_t

Number of LPA slots for which an LFN shall listen for LPA frames Specification range [1, 255].

uint16_t

Delay between two LFN PAN Advertistement Solicit messages.

Public Attribute Documentation#

discovery_slot_time_ms#

uint8_t sl_wisun_lfn_params_connection_t::discovery_slot_time_ms

Duration of LFN PAN Advertisement (LPA) listening slot (millisecond) Specification range [15, 255].


discovery_slots#

uint8_t sl_wisun_lfn_params_connection_t::discovery_slots

Number of LPA slots for which an LFN shall listen for LPA frames Specification range [1, 255].


lpas_interval_s#

uint16_t sl_wisun_lfn_params_connection_t::lpas_interval_s

Delay between two LFN PAN Advertistement Solicit messages.

The delay is applied between the end of the response period and the next LPAS. Range [1, 65535]