You are viewing documentation for version:2.13.0 (latest)PDFRequest message body. Public Attributes#uint32_tidOption identifier. uint8_tvalValue. uint16_tval_lenSize of the value in bytes. Public Attribute Documentation#id#uint32_t sl_wisun_msg_set_option_req_body_t::idOption identifier. val#uint8_t sl_wisun_msg_set_option_req_body_t::val[]Value. val_len#uint16_t sl_wisun_msg_set_option_req_body_t::val_lenSize of the value in bytes.