You are viewing documentation for version:2.13.1 (latest)Request message body. Public Attributes#int32_tlevelSocket protocol level. uint16_toption_lengthSocket option length. int32_toption_nameSocket option to get. int32_tsocket_idID of the socket. Public Attribute Documentation#level#int32_t sl_wisun_msg_get_socket_option_req_body_t::levelSocket protocol level. option_length#uint16_t sl_wisun_msg_get_socket_option_req_body_t::option_lengthSocket option length. option_name#int32_t sl_wisun_msg_get_socket_option_req_body_t::option_nameSocket option to get. socket_id#int32_t sl_wisun_msg_get_socket_option_req_body_t::socket_idID of the socket.