Wi-SUN API events#
Modules#
sl_wisun_msg_network_update_ind
sl_wisun_msg_socket_data_available_ind
sl_wisun_msg_socket_connected_ind
sl_wisun_msg_socket_connection_available_ind
sl_wisun_msg_socket_closing_ind
sl_wisun_msg_connection_lost_ind
sl_wisun_msg_socket_data_sent_ind
sl_wisun_msg_regulation_tx_level_ind
sl_wisun_mode_switch_fallback_level_ind
sl_wisun_msg_lfn_multicast_reg_ind
sl_wisun_msg_dhcp_vendor_data_ind
Enumerations#
Wi-SUN Message API indication IDs.
Enumeration Documentation#
sl_wisun_msg_ind_id_t#
sl_wisun_msg_ind_id_t
Wi-SUN Message API indication IDs.
Enumerator | |
---|---|
SL_WISUN_MSG_CONNECTED_IND_ID | This indication is sent when a connection request has been completed. |
SL_WISUN_MSG_SOCKET_DATA_IND_ID | This indication is sent when data has been received on a socket. |
SL_WISUN_MSG_SOCKET_DATA_AVAILABLE_IND_ID | This indication is sent when there is buffered data available on a socket. |
SL_WISUN_MSG_SOCKET_CONNECTED_IND_ID | This indication is sent when a socket connect request has been completed. |
SL_WISUN_MSG_SOCKET_CONNECTION_AVAILABLE_IND_ID | This indication is sent when there is a socket connection request waiting. |
SL_WISUN_MSG_SOCKET_CLOSING_IND_ID | This event is sent when a socket is waiting to be closed. |
SL_WISUN_MSG_DISCONNECTED_IND_ID | This event is sent when a disconnection request has been completed. |
SL_WISUN_MSG_CONNECTION_LOST_IND_ID | This event is sent when a connection to Wi-SUN network has been lost and the device is trying to regain the connection. |
SL_WISUN_MSG_SOCKET_DATA_SENT_IND_ID | This event is sent when part of the buffered socket data has been sent. |
SL_WISUN_MSG_ERROR_IND_ID | This event is sent when an internal stack error has occurred. |
SL_WISUN_MSG_JOIN_STATE_IND_ID | This event is sent when the join state changes. |
SL_WISUN_MSG_NETWORK_UPDATE_IND_ID | This event is sent when the network has been updated. |
SL_WISUN_MSG_REGULATION_TX_LEVEL_IND_ID | This event is sent when regional regulation transmission level changes. |
SL_WISUN_MSG_MODE_SWITCH_FALLBACK_IND_ID | This event is sent when the mode switch is disabled. |
SL_WISUN_MSG_RX_FRAME_IND_ID | This event is sent on frame reception. |
SL_WISUN_MSG_LFN_WAKE_UP_IND_ID | This event is sent on LFN wake up. |
SL_WISUN_MSG_LFN_MULTICAST_REG_IND_ID | This event is sent when an LFN multicast group registration finishes. |
SL_WISUN_MSG_DHCP_VENDOR_DATA_IND_ID | This event is sent when DHCPv6 vendor-specific information is received. |
43
of file /mnt/raid/workspaces/ws.wIWINzxl8/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_events.h